Getting Started with S32Z280-594EVB

Last Modified: Apr 20, 2025Supports S32Z280-594EVB Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Build, Run

1. Out of the Box

1.1 Out of the Box

  • NXP S32Z280-594EVB evaluation board
  • 12 V power supply with universal adapters
  • Board standoffs

1.2 Get to Know the Hardware

The S32Z280-594EVB provides a platform for evaluation and development of S32Z2 high-performance real-time automotive processors, facilitating hardware and software development and providing robust debug capabilities. NXP provides Real Time Drivers (RTD) to be installed on top of the S32 Design Studio IDE, which the RTD consists of example software applications for various features and peripherals of the EVB.

S32Z280-594EVB Callout

S32Z280-594EVB Callout

1.3 Block Diagram Features

S32Z280-594EVB Evaluation Board

S32Z280-594EVB Evaluation Board.

1.4 Board Features

  • USB to UART interface
  • 2 x RCON Controller for custom boot settings
  • 1Kb EEPROM
  • JTAG debug connector
  • Quad flash
  • 1 x 5Mbit/S CAN-FD and 2 x 8Mbit/S CAN-FD interfaces
  • 1 x Micro-SD card socket
  • 512Mb + 64Mb flash
  • LPDDR4 flash
  • BMS, Aurora Trace, Zipwire connectors
  • Automotive ethernet and LIN
  • User LEDs
  • Option to connect to the S32X-MB motherboard to extend I/O capabilities

2. Get Software

2.1 Download S32 Design Studio

Download and install the S32 Design Studio for S32 Platform.

Download S32 Design Studio IDE

2.2 Install the Real Time Drivers (RTD)

Download the S32ZE Real Time Drivers Version 2.x.x updatesite.zip. Open the S32 Design Studio. Go to Help→S32DS Extensions and Updates→Add Update Sites, and choose the downloaded updatesite.zip.

GS-S32Z280-594EVB-IMG3_2_1

GS-S32Z280-594EVB-IMG3_2_1

Find and select the two S32ZE Real-Time Drivers options from the list on the S32DS Extensions and Updates window, and click Install/Update.

GS-S32Z280-594EVB-IMG3_2_2

GS-S32Z280-594EVB-IMG3_2_2

3. Build, Run

3.1 Running an Example Application

  1. Open the S32 Design Studio 3.6.x or above
  2. Go to File→New→S32DS Project from Example
  3. GS-S32Z280-594EVB-IMG4_2
  4. Select from Dio Examples the Dio_Example_S32Z2XX_SMU
  5. GS-S32Z280-594EVB-IMG4_3
  6. Double click the example_Dio.mex file from the Project Explorer, click Update Code→OK
  7. GS-S32Z280-594EVB-IMG4_4
  8. Click on the S32DS C/C++ icon, select the project and click the Build icon
  9. GS-S32Z280-594EVB-IMG4_5
  10. Connect the EVB to the 12 V power supply. Connect the S32 Debug Probe to the PC via USB, and connect the JTAG cable between the EVB and the S32 Debug Probe. Turn on the EVB using SW1
  11. Click on the Run→Debug Configurations
  12. GS-S32Z280-594EVB-IMG4_7
  13. Choose the Dio_Example_S32Z2XX_SMU project and click Debug
  14. GS-S32Z280-594EVB-IMG4_8
  15. Resume the code and watch D12 on the EVB to start blinking. By default the main.c is configured to let D12 blink for 10 times
  16. GS-S32Z280-594EVB-IMG4_9_1 GS-S32Z280-400EVB-IMG4_10_2

Support

Forums

Connect with other engineers and get expert advice on designing with the S32Z280-594EVB evaluation board using our community sites.