Getting Started with the i.MX RT1170 Evaluation Kit

Last Modified: 2020-11-30 15:00:00Supports i.MX RT1170 Evaluation Kit

1. Plug It In

Let's take your MIMXRT1170-EVK for a test drive. You have the choice of watching the sequence in a short video or following the detailed actions listed below.

1.1 Get Familiar with the Board

Get Started with the i.MX RT1170 - 1.1

Get Started with the i.MX RT1170 - 1.1

1.2 Attach the Power Adapter Cable

Plug the power adapter wire into the MIMXRT1170-EVK board 5 V DC IN header (J43) and switch on 5 V DC IN (SW5).

Get Started with the i.MX RT1170 - 1.2

Get Started with the i.MX RT1170 - 1.2

1.3 Run the Out-of-Box Demo

The MIMXRT1170-EVK board comes preprogrammed with a demo that will initiate the LED on the board to flash when plugged in.

When the board is tilted, the green LED gradually illuminates based on the degree of tilt on the X-axis.

Get Started with the i.MX RT1170 - 1.3

Get Started with the i.MX RT1170 - 1.3

2. Get Software

2.1 Installing Software for MIMXRT1170-EVK

2.2 Jump Start Your Design with the MCUXpresso SDK

Want to learn more about the SDK? The MCUXpresso software development kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

Click below to download the recent SDK release for the MIMXRT1170-EVK, make sure you select Host OS, Toolchain and desired components.

MCUXPRESSO-SDK-TN Get MCUXpresso SDK

2.3 Get Your Toolchain

MCUXpresso IDE is a development platform ecosystem from NXP. It provides an end-to-end solution enabling engineers to develop embedded applications from initial evaluation to final production.

MCUXpresso IDE

Get MCUXpresso IDE

Want to use a different toolchain? Need help choosing?

GS Tool Logos

2.4 MCUXpresso Config Tools

The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated into MCUXpresso or you can download it as a separate tool.

MCUXpresso Config Tools Get MCUXpresso Config Tools

2.5 PC Configuration

Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged into your PC.

Download driver

2.6 Serial Terminal

Install and configure your preferred terminal software to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the MIMXRT1170-EVK’s virtual COM port, open the device manager and look under the "Ports" group.”.

Not sure how to use a terminal application? Try one of these tutorials: MCUXpresso IDE Terminal Tutorial, Tera Term Tutorial, PuTTY Tutorial.

3. Build, Run

3.1 Build and Run an SDK Multicore Demo on the MIMXRT1170-EVK

3.2 Explore the MCUXpresso SDK Example Code

The MCUXpresso SDK comes with a long list of example application code. To see what's available, browse to the SDK boards folder of your SDK installation and select MIMXRT1170-EVK.

<SDK_Install_Directory>/boards/evkmimxrt1170 

To learn more about specific example code, open the readme.txt file in an example's directory.

3.3 Building and debugging MCUXpresso SDK Examples

If one or more of the demo application or driver examples sounds interesting, you probably want to know how you can build and debug it yourself. The Getting Started with SDK guide provides easy, step-by-step instructions on how to configure, build and debug demos for all toolchains supported by the SDK.

Use the guide below to learn how to open, build and debug an example application in MCUXpresso IDE, IAR Embedded Workbench IDE, Keil MDK or Arm GCC.

Boot Options

The i.MX RT family supports a number of different boot sources, and includes the option for memory to be copied to an on-chip or external destination memory as well as Execute in Place (XIP) for some interfaces. Learn more about your choices and which one is the adequate for your design.

Boot Options for i.MX RT Crossover MCUs

Documents and Videos Description
AN12108 How to Enable Boot from QSPI Flash This document describes how to use Flashloader step by step to program a bootable image into the external storage device either by using OpenSDA or MfgTool.
AN12107 How to Enable Boot from Octal SPI Flash and SD card This document describes how to program a bootable image into the external storage device.

Tools and References

MCUXpresso Secure Provisioning Tool  A GUI-based application provided to simply the generation and provisioning of bootable executables on NXP i.MX RT.

Community Resources for Booting  Look for answers to your boot questions or submit new questions in our Community.

External Memory

Documents and Videos Description
AN12437 i.MX RT Series Performance Optimization How to optimize the system performance running on different memory devices.
AN12108 How to Enable Boot from QSPI Flash This document describes how to use Flashloader step by step to program a bootable image into the external storage device either by using OpenSDA or MfgTool.
AN12107 How to Enable Boot from Octal SPI Flash and SD card This document describes how to program a bootable image into the external storage device.
Developing Code Using the Adesto EcoXip Memory Learn about the hardware and software requirements for configuring the NXP i.MX RT1050 EVKB board with an Adesto EcoXiP Flash device.
AN12564 Implement Read While Write (RWW) on i.MX RT Series How to implement the RWW requirement on the i.MX RT series.
AN12239 How to Enable HyperRAM with i.MX RT How to use the HyperRAM with the i.MX RT MCU, including hardware connections, HyperRAM protocol, source code and performance.
AN13028 Advanced HyperRAM/PSRAM Usage on i.MX RT This application note describes the advanced usage of HyperRAM/PSRAM when used with FlexSPI on i.MX RT MCU, including FlexSPI prefetch function, HyperRAM/PSRAM refresh interval and HyperRAM devices supported.
AN13204 i.MX RT1170 ECC Application This document discusses the ECC application on memory, including TCM, Cache, OCRAM and external memory.
AN12255 How to Use Flash Remapping Function The i.MX RT1170 supports the flash remapping function, which allows users to remap flash address to the FlexSPI interface.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples for external memory are listed below.

FlexSPI Nor Polling Example

How to use the FlexSPI driver with polling.

Path:

<SDK_PATH>/boards/evkbimxrt1170/driver_examples/flexspi/nor/polling_transfer 

EDMA Transfer Example

Multiple data transfer examples using EDMA.

Path:

<SDK_PATH>/boards/evkbimxrt1170/driver examples/flexspi/nor/edma_transfer 

SDRAMC Example

How to use the SEMC controller driver to initialize the external SDRAM chip.

Path:

<SDK_PATH>/boards/evkbimxrt1170/driver_examples/semc/sdram 

XECC Examples

How to use the external ECC controller (XECC) with FlexSPI or SDRAM

Path:

<SDK_PATH>/boards/evkbimxrt1170/driver examples/xecc 

Tools and References

MCUXpresso Secure Provisioning Tool  A GUI-based application provided to simply the generation and provisioning of bootable executables on NXP i.MX RT.

Security and Integrity

The i.MX RT1170 is secure-by-design and supported by secure software driving the secure System-on-a-Chip (SoC).

Documents and Videos Description
Secure Boot Webinar and demo Using the recent NXP software and tools, you can integrate boot authentication and encrypted execution into your design based on i.MX RT10xx MCUs. Learn more about secure boot features and how the MCUXpresso Secure Provisioning Tool allows you to configure them.
Realizing Today's Security Requirements: Achieving End-To-End Security with a Crossover Processor Learn about common shared security goals that IoT end and edge nodes should meet, as well as the steps, tools and procedures needed to achieve root of trust in end devices.
AN13250 i.MX RT1170 Secure Boot Modes Provides an overview of the secure boot modes available on the i.MX RT1170 family and how to enable them.
AN13133 Secure JTAG for i.MX RT1170 Describes the three JTAG security modes that are available on the i.MX RT series and how to use them on the i.MX RT1170 MCU.
AN13078 How to Use the Tamper Function Tamper detection is a special mechanism to trigger violation and zeroize key information when the device encounters unauthorized opening or tampering. This application note explains how to use the tamper function on i.MXRT1173.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to security and integrity are listed below.

Mbedtls Examples

Program performs cryptographic algorithm benchmarking and testing. (Requires optional mbedTLS middleware package).

Path:

<SDK_PATH>/boards/evkbimxrt1170/mbedtls_examples/

PUF Examples

Performs PUF enroll, start, generate key, set key and get key functions.

Path:

<SDK_PATH>/boards/evkbimxrt1170/driver_examples/puf 

Tools and References

One-stop secure boot tool: NXP-MCUBootUtility  A GUI tool specially designed for NXP MCU secure boot. It includes all the features of NXP's official security enablement toolset with support for full graphical user interface operation.

MCUXpresso Secure Provisioning Tool  A GUI-based application provided to simply the generation and provisioning of bootable executables on NXP i.MX RT.

RT1170 Security Reference Manual.

Wired Communications

Documents and Videos Description
Wired Communications Middleware for NXP Microcontrollers Learn about wired communications libraries and examples provided through the MCUXpresso SDK.
CANopen in NXP's MCUXpresso SDK A demo combining different middleware components of the NXP MCUXpresso SDK using the i.MX RT1064 and LPC55S16 demo boards.
CANopen and Embedded Wizard Demo featuring the i.MX RT 1064 and LPC55 A demo combining different middleware components of the NXP MCUXpresso SDK using the i.MX RT1064 and LPC55S16 demo boards.
AN12822 Emulating 8080 Bus with the FlexIO on RT1050 How to use the FlexIO module to emulate the 8080 parallel bus and to drive a graphic TFT LCD with the 8080 bus interface.
AN12679 Implement High-Speed RS-485 Application with i.MX RT Based on NXP SDK How to implement RS-485 communication with NXP i.MX RT series EVK, and how to design software based on NXP MCUXpresso SDK.
AN12103 Developing a Simple UVC Device Based on i.MX RT1050 UVC is widely used for applications including desktop video cameras (webcams), digital camcorders and still-image cameras. This document describes how to develop a simple UVC device and introduces the hardware and software platforms of the demo application
MCU Tech Minutes | Getting Started with CANopen and MCUXpresso Learn how to download an SDK that includes EmSA's CANopen stacks and set up one manager and one device CANopen network.
Employing TSN Over Ethernet to Enable Precision Motor Control through Operator Gesture This demo shows the i.MX 8M Plus processor, i.MX RT1170 MCU and Layerscape LS1028A using different protocols as well as custom motor control messages over TSN Ethernet in a complex industrial system.
AN13114 Enable More USB Examples on M4 Core for RT1170 RT1170 works with M7 and M4, on which all USB examples can run. However, all USB examples in the release package are enabled on M7. This document describes how to migrate USB examples from M7 to M4 with different toolchains

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to wired communications are listed below.

CANopen Examples

Implements a minimal CANopen Manager and CiA 401 generic I/O device. (Requires optional CANopen middleware package).

Path:

<SDK_PATH>/boards/evkbimxrt1170/canopen_examples/

lwIP Examples

Various demos and examples for the lwIP TCP/IP stack, which uses the ICMP protocol. (rRquires optional lwIP middleware package).

Path:

<SDK_PATH>/boards/evkbimxrt1170/lwip_examples/

USB Examples

A number of USB examples for host and device operation exist within the SDK. (Requires optional USB Host, Device, OTG stack middleware package).

Path:

<SDK_PATH>/boards/evkbimxrt1170/usb_examples/

Tools and References

Accelerate Development of Robust Network Communications with CANopen and CANopen FD  NXP has partnered with EmSA to offer CANopen as an enabling software technology. Fully integrated CANopen Libraries based on MicroCANopen Plus v7.0 are available in the MCUXpresso SDK.

EmSA CANopen Libraries for NXP SDK User Manual.

Wireless Connectivity

Documents and Videos Description
NXP Wireless Connectivity Our portfolio of low-power, cost-effective wireless solutions address many monitoring and control applications for the Internet of Things.
Cloud Connectivity on NXP Microcontrollers Integrated support for cloud services including Amazon Web Services, Microsoft Azure and Google Cloud IoT.
Getting Started with NXP Wi-Fi modules using i.MX RT platform Let's take your Wi-Fi module for a test drive. This guide uses the Wi-Fi modules and i.MX RT platforms!
AN12257 IoT Device Secure Connection with LoRa This document explains how to establish IoT secure connection with LoRa between gateway and end devices.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to wired communications are listed below.

AWS Examples

Amazon FreeRTOS Qualification (AFQ), device configuration, AWS Greengrass discovery, remote control by Android mobile application and shadow lightbulb demos.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/aws_examples 

ThreadX Example

A small demo of the high-performance ThreadX kernel.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/azure_rtos_examples/threadx_demo 

Wi-Fi Examples

CLI support usage example, iPerf network performance measurement, Wi-Fi test mode example and Wi-Fi configuration utility demos.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/wifi_examples/ 

Tools and References

HOMEKIT-SDK  The HomeKit Software Development Kit (SDK) from NXP offers support for home automation applications using Apple HomeKit technology, delivering great performance, advanced security and supporting all connectivity options; Bluetooth Smart® (Bluetooth Low Energy), Wi-Fi, Ethernet and remote access over iCloud.

Multicore and Hardware Acceleration

Documents and Videos Description
AN13264 i.MX RT1170 Dual Core Application Introduces the dual-core application on i.MX RT1170, including boot, MU/SEMA4/RDC/XRDC2/Shared memory and dual-core debug in a different tool chain.
How to use JLINK to debug RT1170 dual core The dual core i.MX RT117x devices have one Cortex-M7 core and one Cortex-M4 core that can be debugged simultaneously via JLINK if some additional setting changes are made.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. A common example related to power management is listed below.

FlexSPI Nor Polling Example

How to use the FlexSPI driver with polling.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/multicore_examples 

Power Mode Switch Demos

Demonstrates the use of power modes in the KSDK for bare metal or RTOS.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/demo_apps/power_mode_switch 

Power Management

Power management includes device-specific techniques and information on power management and low-power optimization.

Documents and Videos Description
AN13116 Entering STBY mode on a single-core RT1170 This application note outline steps to enter the STBY mode on a single core RT1170 and simulate a single-core state on RT1170 EVK.
AN13104 Debug and Application for RT1170 Clock and Low Power Feature This application note introduces not only clock and low-power features in RT1170, but also some debug and application skills when developing a low-power use case.
AN13148 i.MX RT1170 Low-Power Modes This document describes the i.MX RT1170 power architecture design, clock architecture, and how the low-power modes can be used and configured.

MCUXpresso SDK Example

Several examples, demos and drivers are available within the SDK to help you get started. A common example related to power management is listed below.

Power Mode Switch Demos

Demonstrates the use of power modes in the KSDK for bare metal or RTOS.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/demo_apps/power_mode_switch 

Audio

Documents and Videos Description
Audio Software on NXP Microcontrollers Middleware, example applications, MCUXpresso Config tools and partner solutions for advanced audio applications.
AN12090 Using Multi-Channel Feature of SAI This document introduces the technology of a 7.1 surround sound system, including SAI and FLAC, and provides guidance on how to use the multi-channel SAI feature to develop applications running in a correct high-performance way.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to motor control are listed below.

SAI Demo

Demonstrates complicated digital audio playback and record case.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/demo_apps/sai 

ASRC Demos

Demonstrates how to use the asynchronous sample rate converter module.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/driver_examples/asrc 

SPDIF Demos

Demonstrates how to use the spdif driver with EDMA and interrupt.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/driver_examples/spdif 

PDM Microphone Demos

Multiple EDMA and interrupt examples.

Path:

 <SDK_PATH>/boards/evkbimxrt1170/driver_examples/pdm 

Display and Graphics

The LCD panel that works with the IMIXRT1170EVK and is used in the MCUXpresso SDK graphics examples is the RK055HDMIPI4M.

Documents and Videos Description
Graphics for NXP Microcontrollers Graphics libraries and tools from multiple partners for developing embedded GUIs of all levels of complexity.
Cost-Effective Embedded HMI Solutions with i.MX RT1170 Drive down your costs while combining safety and modern UX by developing with the i.MX RT1170 crossover MCU and "Qt for MCUs".
Design Your Next Graphical UI for Industrial HMI Applications Using NXP's i.MX RT1170 MCU, GUI Guider and LVGL Learn more about the i.MX RT1170 MCU and see how LVGL and GUI Guider make it easy to design your next embedded GUI.
Implementing Graphics in Real-time Industrial HMI Systems with NXP MCUs and Embedded Wizard NXP has partnered with TARA Systems to offer Embedded Wizard as an Enabling Software Technology.
Getting Started with Embedded Wizard and MCUXpresso Learn how to download an SDK that includes Embedded Wizard and get an example project up and running on your device.
Creating Graphics on the i.MX RT1060 Learn how to develop graphics on the i.MX RT, which supports product designs with advanced multimedia for GUI and enhanced human machine interface (HMI) experience.
Implementing Graphics in Real Time Industrial HMI Systems with i.MX RT10xx MCUs and Crank Storyboard NXP has partnered with Crank Software to offer Storyboard as an Enabling Software Technology.
Simplifying the Creation of Stunning GUIs Introducing Embedded Wizard in the MCUXpresso SDK.
AN12302 i.MX RT eLCDIF RGB Mode Use Case An example using the enhanced Liquid Crystal Display Interface (eLCDIF) on the MIMXRT1050-EVKB board.
AN13075 i.MX RT1170 Heterogeneous Graphics Pipeline A brief overview of the graphics engines on the i.MX RT1170 as well as how to use them independently and in unison.
AN12940 Use Case of RT1170 LCD Display System based on MIPI DSI How to use the MIPI DSI Host Controller and LCDIFv2 Controller to drive a DSI-compliant LCD panel on i.MX RT1170.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to display and graphics are listed below.

EmWin Examples

Demonstrate how to use the emWin library to render text and graphical widgets. (Requires optional emWin middleware package).

Path:

 <SDK_PATH>/boards/boards/evkbimxrt1170/emwin_examples 

JPEG Examples

Reads the JPEG pictures from the SD card, decodes them, and shows them in the LCD panel one by one (Requires optional JPEG library middleware package).

Path:

 <SDK_PATH>/boards/evkbimxrt1170/jpeg_examples 

LittleVGL Examples

Demonstrates littlevgl widgets (Requires optional LVGL middleware package).

Path:

 <SDK_PATH>/boards/evkbimxrt1170/vlittlevgl_examples 

OpenVG Examples

Demonstrates OpenVG graphics library (Requires optional openvg middleware package).

Path:

 <SDK_PATH>/boards/evkbimxrt1170/openvg_examples 

VGlite Examples

Demonstrates VGlite graphics library (Requires optional vglite middleware package).

Path:

 <SDK_PATH>/boards/evkbimxrt1170/vglite_examples 

Tools and References

LVGL Open-Source Graphics Library  LVGL is a free and open-source embedded graphic library with features that enable you to create embedded GUIs with intuitive graphical elements, beautiful visual effects and a low memory footprint.

GUI Guider  A user-friendly graphical user interface development tool from NXP that enables the rapid development of high-quality displays with the open-source LVGL graphics library.

Camera Interfaces

The LCD panel that works with the IMIXRT1170EVK and is used in the MCUXpresso SDK graphics examples is the RK043FN01H-CT.

Documents and Videos Description
AN12110 Developing a Camera Application with i.MX RT Series How to develop an HD camera application with the NXP i.MX RT1050 processor.
AN13205 Development of H.264 Video Encode on RT Series How to develop an H264 video encoder application with the i.MX RT1170 processor.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to camera interfaces are listed below.

MIPI_RGB

This project shows how to receive the camera data using CSI driver for RGB data.

Path:

 <SDK_PATH>/boards/evkbimx1170/driver_examples/csi/mipi_rgb 

CSI YUV

This project shows how to receive the camera data using CSI driver with YUV format data.

Path:

 <SDK_PATH>/boards/evkbimx1170/driver_examples/csi/mipi_yuv 

Voice

Voice Resources

Documents and Videos Description
AN13065 Gender Voice Recognition with TensorFlow Lite Inference This document describes the steps to train the TensorFlow model on Gender voice audio samples and classification.
Clarinox Democratization of BT/BLE/Wi-Fi Technologies on NXP i.MX RT1170 MCUs for IoT Gateways The i.MX RT1170 MCU is a good platform to run complex Bluetooth and Wi-Fi use cases such as the IoT gateway.

Machine Learning

Machine learning (ML) typically encompasses applications where classification, recognition and prediction of man-made abstractions are desired. Examples include Image Recognition, Gesture Recognition, Anomaly Detection, Speech-to-Text, Text-to-Speech, ASR, Scene Recognition and many more.

Documents and Videos Description
eIQ® ML Software Development Environment Enables the use of ML algorithms on NXP MCUs, i.MX RT crossover MCUs and i.MX family SoCs. eIQ software includes inference engines, neural network compilers and optimized libraries.
Getting Started with eIQ on i.MX RT How to download eIQ Machine Learning software enablement and run it with MCUXpresso IDE, VS Code, IAR or Keil MDK.
eIQ Fact Sheet Machine learning software for NXP i.MX and MCUs - libraries, example applications and inference engines.
eIQ Glow Lab for i.MX RT Learn how to use the Glow neural network compiler tool by running a handwritten digit recognition model example. A step-by-step video covering this lab is also available below.
eIQ Toolkit and DeepViewRT Labs for i.MX RT Learn how to use eIQ Toolkit to generate your own image classification and object detection models and deploy them onto i.MX RT devices. Also learn about the eIQ DeepViewRT inference engine.
eIQ TensorFlow Lite for Microcontrollers Lab for i.MX RT Learn how to run your own TFLite model on i.MX RT microcontrollers using the TensorFlow Lite for Microcontrollers (TFLM) inference engine.
Application Software Pack: ML-Based System State Monitor This ML application software pack is designed to show how to create a fan vibration state monitoring solution and can also be used for other time-series anomaly detection use cases.
AN13001 Glow Memory Analysis How to understand the Glow memory information generated by the Glow compiler and calculate the memory required for a particular model. This compiler can then be used to determine the minimum memory size that is needed to run the model.
AN12766 Anomaly Detection with eIQ using K-Means clustering in Tensor Flow Lite Step by step instruction to enable a machine condition monitoring application using anomaly detection.
AN12781 Caffe Model Development on MNIST Dataset with CMSIS-NN Library Describes the process to train a Caffe model on the MNIST dataset for digit classification. The trained Caffe model is converted to a source file that can run on i.MX RT platforms.
MCU Tech Minute: Multistage ML with the Coral Development Board To enable truly battery operated ML, Coral introduces a two part "wake-to-run" ML workflow that takes advantage of the capabilities offered by NXP's i.MX RT1176 MCU, and pairs them with the Coral Edge TPU.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to machine learning are listed below.

eIQ Example

Several examples demonstrating machine learning applications using TensorFlow Lite for Microcontrollers, DeepViewRT and Glow (Requires optional eIQ middleware package).

Path:

 <SDK_PATH>/boards/evkbimxrt1170/eiq_examples 

Motor Control

Motor control is a complicated and advanced topic, with a wide range of intricacies and pitfalls that depend on the number of motors, motor type and sensored or sensorless motor drivers.

NXP has a number of ready-to-use motor control algorithms (middleware), and the best way to get started is with the FreeMASTER examples included in the MCUXpresso SDK. These examples utilize the FreeMASTER Run-Time Debugging Tool, a user-friendly real-time debug monitor and data visualization tool that enables runtime configuration and tuning of embedded software applications.

FreeMASTER supports non-intrusive monitoring of variables on a running system and can display multiple variables on oscilloscope-like displays as standard widgets (gauges, sliders and more) or as data in text form, offering simple-to-use data recorders. It can link with HTML, MATLAB® or Excel to other scriptable frameworks or even popular visual programming tools like Node-RED.

Documents and Videos Description
Get Your Motor Spinning with i.MX RT This presentation covers the MCU requirements, motor control basics and framework to spin a BLDC, PMSM or ACIM motor and how to implement motor control on the i.MX RT.
Employing TSN Over Ethernet to Enable Precision Motor Control through Operator Gesture This demo shows the i.MX 8M Plus processor, i.MX RT1170 MCU and Layerscape LS1028A using different protocols as well as custom motor control messages over TSN Ethernet in a complex industrial system.
AN12214 PMSM Field-Oriented Control on MIMXRT10xx EVK Describes the implementation of the sensor and sensorless speed and position motor control software for 3-phase Permanent Magnet Synchronous Motors (PMSM).
PMSM Field-Oriented Control on MIMXRT10xx EVK User's Guide Step-by-step guide on how to open, compile, debug and run Permanent Magnet Synchronous Motor (PMSM) projects in most common IDEs, as well as how to turn the NXP Freedom PMSM power stage and the i.MX RT10xx evaluation kit into a complete motor control reference design.
AN12659 NXP quad motor-control development platform HW Describes the NXP quad motor-control development platform modular architecture and provides a detailed hardware description of the different components.
AN12200 Dual FOC Servo Motor Control on i.MX RT Describes the dual servo demo with the NXP i.MX RT1020 processor. You can use it as a reference for motor control application developing based on other i.MX RT products.
FreeMASTER How To A starting guide for engineers using FreeMASTER tool.
FreeMASTER 3.0 Installation Guide This article will walk you through the installation process of FreeMASTER 3.0.
FreeMASTER Four-Part Webinar Series On-demand training provides an overview of the FreeMASTER software, its features, capabilities, available examples, application use cases and how to easily get started.

MCUXpresso SDK Examples

Several examples, demos and drivers are available within the SDK to help you get started. Some common examples related to motor control are listed below. Note that all examples require the optional motor control middleware package.

ACIM

AC induction motor middleware.

Path:

 <SDK_PATH>/middleware /motor_control/acim 

BLDC

Brushless DC electric motor middleware.

Path:

 <SDK_PATH>/middleware/motor_control/bldc 

FreeMASTER

FreeMASTER middleware for motor control examples.

Path:

 <SDK_PATH>/middleware/motor_control/freemaster 

PMSM

Permanent magnet synchronous motor middleware.

Path:

 <SDK_PATH>/middleware/motor_control/pmsm 

MCUXpresso IDE Terminal Tutorial

MCUXpresso IDE Terminal Tutorial

The most recent versions of MCUXpresso IDE count with a terminal emulation application. This tool can be used to display information sent from your NXP development platform's virtual serial port.

  1. Open the MCUXpresso IDE
  2. FRDM-K32L2B3-OPEN-MCU IDE-S2
  3. Launch the MCUXpresso IDE terminal by clicking the "Open a Terminal" button on the top of the IDE or press "Ctrl + Alt + Shift + T."
  4. FRDM-K32L2B3-MCU-IDE-TERMINAL-S2
  5. Select Serial Terminal
  6. FRDM-K32L2B3-SELECT-TYPE-S2
  7. Configure the serial port settings (using the LPC-Link2 COM port number) to 115200 baud rate, 8 data bits, no parity and 1 stop bit, then press “OK” button
  8. FRDM-K32L2B3-SERIAL-PORT-S2
  9. Verify that the connection is open. If connected, the MCUXpresso IDE will look like the figure below at the Terminal view
  10. FRDM-K32L2B3-VERIFY-S2
  11. You're ready to go

Tera Term Tutorial

Tera Term Tutorial

Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

Download
  1. Download Tera Term from SourceForge. After the download, run the installer and then return to this webpage to continue
  2. Launch Tera Term. The first time it launches, it will show you the following dialog. Select the serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
  3. TERA-TERM-TURORIAL-1
  4. Configure the serial port settings (using the COM port number identified earlier) to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
  5. Verify that the connection is open. If connected, Tera Term will show something like below in its title bar
  6. TERA-TERM-TURORIAL-2
  7. You're ready to go

PuTTY Tutorial

PuTTY Tutorial

PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

Download
  1. Download PuTTY using the button below. After the download, run the installer and then return to this webpage to continue
  2. Launch PuTTY by either double clicking on the *.exe file you downloaded or from the Start menu, depending on the type of download you selected
  3. Configure In the window that launches, select the Serial radio button and enter the COM port number that you determined earlier. Also enter the baud rate, in this case 115200
  4. FRDM-K32L2B3-PUTTY-S2
  5. Click Open to open the serial connection. Assuming the board is connected and you entered the correct COM port, the terminal window will open. If the configuration is not correct, PuTTY will alert you
  6. FRDM-K32L2B3-PUTTY-CERIFYCONN
  7. You're ready to go

Support

To learn what to do next, find your issue below. If you still need help, contact NXP Support.

Training

Basic Application Development Using MCUXpresso IDE and MCUXpresso Config Tools - This three-part video series covers the basic interactions between the MCUXpresso IDE and Config Tools when working with either an imported SDK example project or creating a new one.

MCU Tech Minutes- Key Features and Benefits of the i.MX RT series - Short video presentations introduce some of the key features and benefits of the i.MX RT series.

MCU Minutes: Introducing the i.MX RT1170 Crossover MCU - NXP offers breakthrough performance with the 1GHz i.MX RT1170.

Architecture and Features of the i.MX RT1170 MCU family - The i.MX RT1170 family is the most powerful of the Crossover microcontrollers, designed for Machine Learning, IoT, industrial automation, multimedia and audio applications.

Graphics Applications with the i.MX RT1170 Family of MCUs - Learn about hardware resources for graphic applications, middleware libraries for the i.MX RT1170 and watch an Embedded Wizard demo.

i.MX RT1170 Training - Full list of on-demand training, how-to videos and webinars from NXP about this product.

Forums

Connect with other engineers and get expert advice on designing with the i.MX RT1170 on one of our community sites.

Product Forums

Software Forums