Getting Started with the KW45B41Z Evaluation Kit

Last Modified: Mar 15, 2023Supports KW45B41Z Evaluation Kit with Bluetooth® Low Energy

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Modify an SDK Example

1. Plug It In

Let's take your KW45B41Z board for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions listed below.

1.1 Get Familiar with the Board

The KW45B41Z board is pre-programmed with a diagnostic demo, which tests various features of the board. This program utilizes the MCU-LINK VCOM output, which is connected to the debug probe(J14), which acts a serial to USB bridge to a host computer, as well as providing the CMSIS-DAP debug interface.

1.2 Serial Terminal

Most of the MCUXpresso SDK examples and this out-of-box demo set up for MCUXpresso IDE, IAR and Keil tools use the MCU UART for print output. If you are not sure how to use a terminal application try one of these: MCUXpresso Terminal Tutorial, Tera Term Tutorial, PuTTY Tutorial.

1.3 Plug In the Board

Connect a micro USB cable from connector J14 to a host computer or power supply to power up the board and run the demo program. The demo can be tested with any Bluetooth® Smart Ready products available on the market. The IoT Toolbox can also be used to showcase the profile functionality. For the out-of-the box experience please download the IoT Toolbox on your smartphone from your device's APP store.

1.4 Run the Out-of-Box Demo

Get familiar with the beacons by selecting the 'Beacons' icon once you have opened the IoT Toolbox App.

The beacons are non-connectable advertising packets that are sent on the three advertising channels. The latter contains the following fields.

  • Company Identifier (2 bytes): 0x0025 (NXP ID as defined by the Bluetooth SIG)
  • Beacon Identifier (1 byte): 0xBC (Allows identifying an NXP Beacon alongside with Company Identifier)
  • UUID (16 bytes): Beacon sensor unique identifier
  • A (2 bytes): Beacon application data
  • B (2 bytes): Beacon application data
  • C (2 bytes): Beacon application data
  • RSSI at 1m (1 byte): Allows distance-based applications

2. Get Software

2.1 Install Your Toolchain

NXP offers a complimentary toolchain called MCUXpresso IDE. Please download MCUXpresso v11.6.0 or above.

MCUXpresso IDE

Get MCUXpresso IDE

Want to use a different toolchain?

Need help choosing?

No problem! The MCUXpresso SDK includes support for other tools such as IAR .

IAR

2.2 Jump Start Your Design with the MCUXpresso SDK

Want to learn about SDK

The MCUXpresso SDK is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

You may install the MCUXpresso SDK directly form the MCUXpresso SDK website at mcuxpresso.nxp.com. Click on “Select Development Board” to search for the evaluation board.

GS-K32W148EVK2-2-STEP1

In the Search for Hardware search box, type in the selected board “KW45B41Z-EVK”. Click on the board to select it.

Getting Started with the KW45B41Z Evaluation Kit

On the right hand side you will see the option to build the SDK for the KW45B41Z-EVK. Click on this button to add the middleware needed.

Getting Started with the KW45B41Z Evaluation Kit

To build the SDK, let's “Select All” for the middleware available. Then scroll down and press “Download SDK”. The Software Terms and Conditions will appear, select “I Agree” in order to begin the download.

GS-K32W148EVK2-2-STEP4

Once the SDK package has been downloaded, drag and drop to the “Installed SDKs” window in the MCUXpresso IDE.

Getting Started with the KW45B41Z Evaluation Kit

If you are using another toolchain, you can download the SDK release for the KW45B41Z-EVK using the link below.

MCUXPRESSO-SDK-TN

Get MCUXpresso SDK

2.3 MCUXpresso Config Tools

The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated as a part of MCUXpresso IDE and also as a separate tool if using a different IDE.

Click the Get MCUXpresso Config Tools below to get the Config Tools installer.

MCUXpresso Config Tools

Get MCUXpresso Config Tools

2.4 Install Drivers

MCU-Link is supported on host computers running on Windows 10, MacOS X, and Ubuntu Linux operating systems (OSs). For each OS, an MCU-Link firmware package is available that includes the host device drivers, MCU-Link firmware, and scripts to program CMSIS-DAP and J-Link firmware options.

To download and install the host device drivers and update the MCU-Link firmware, follow these steps:

  1. Go to the MCU-Link page on the NXP website
  2. Click Design Resources. Then, click the SOFTWARE category. The latest version installation packages are displayed at the top for all three compatible OSs
  3. Download the package for your host OS and install it (Linux/MacOS) or execute the installer program (Windows). The package is installed/unzipped to the MCU-LINK_installer_Vx_xxx directory
  4. Switch MCU-Link to (USB) ISP mode by shorting jumper JP20
  5. Connect the J14 connector on the board to the USB port of the host computer through a USB micro-B cable. MCU-Link gets powered up in (USB) ISP mode. The board gets enumerated as a human interface device (HID) class device
  6. Program the MCU-Link firmware into the MCU-Link internal flash using the instructions provided in the "Firmware Installation Guide" section of the "Readme.txt" file. This file can be found in the MCU-LINK_installer_Vx_xxx_directory. Use the scripts provided to program the CMSIS-DAP or J-Link firmware option
  7. Disconnect the board from the host computer, remove jumper JP20 and reconnect the board

2.5 Secure Provisioning Command Line Tool (SPSDK)

Secure Provisioning SDK (SPSDK) is a unified, reliable and easy-to-use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment.

GS-K32W148EVK-SPSDK

To install the SPSDK, you may follow the instructions below, for more details or if you are using a different OS, please visit the installation guide provided in the Secure Provisioning SDK (SPSDK)

Requirements

Make sure to have Python 3.7+ installed (old version 2.x is not supported)

For Windows users:

  1. Create a folder in which the SPSDK repository will be located. In this example, I use the C:\spsdk
  2. Clone the repository to this folder
    1. git clone MCUXpresso Github
    2. Getting Started with the K32W148 Development Platform
  3. In the same folder, you may create and activate your virtual environment.

    Create the python virtual environment.

    1. python -m venv venv

      Activate the virtual environment

    2. venv\Scripts\activate

      When the virtual environment is active you will see the virtual environment's name in parenthesis next to your current working path. Getting Started with the K32W148 Development Platform

      Anytime you use the SPSDK, it is necessary to activate the virtual environment. You do not need to create a new environment each time. Repeat step 3.b only. Getting Started with the K32W148 Development Platform

  4. Install dependencies
    1. python -m pip install --upgrade pip
    2. c.pip install spsdk
  5. Ensure that you spsdk installation has been successful. You will see the output of the complete menu by running the following command.
    1. spsdk -help
    Getting Started with the K32W148 Development Platform

3. Build, Run

The KW45B41Z Wireless Connectivity software comes with a list of demo applications and driver examples ready to be compiled and run for each connectivity stack.

A short video is provided to walk you through this process or you can follow along the steps below.

3.1 Explore the MCUXpresso SDK Example Code

The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select KW45B41Z ( <SDK_Install_Directory>/boards/KW45B41Z ).

To learn more about specific example code, open the readme.txt file in an example's directory.

3.2 Building and Debugging MCUXpresso SDK Examples

If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with MCUXpresso SDK guide provides easy, step-by-step instructions on how to configure, build and debug demos for all toolchains supported by the SDK.

Use the guide below to learn how to open, build and debug an example application using the MCUXpresso IDE.

Using a different toolchain?

This demo is also available for IAR.

3.3 Updating NBU for Wireless Examples

Alert code:

Here you will find two type of images for the NBU FW:

  1. SB3 File Type
    1. This is for EVK users only. The EVK's come programmed with set keys for ease of use in development
  2. XIP File Type
    1. This is for samples that are not programmed with any keys. For these devices, you can create your custom keys, then create an SB3 file based on this XIP image
Getting Started with the KW45B41Z Evaluation Kit

To update the NBU, you may use the SPSDK command line tool.

  1. Open the path to your SPSDK folder and activate the virtual environment
    1. >> venv\Scripts\activate
  2. Place your device in ISP mode. For this example we will use the UART peripheral by connecting a USB cable to J14. On the EVK you can enter ISP by the following method
    1. Make sure a jumper is on JP25
    2. Press and hold SW4, press and release Reset, and then release SW4
  3. Once the device is connected you may check your devices available using SPSDK to find the COM port it is connected to.
    1. >> nxpdevscan
  4. Then you may run the 'receive-sb-file' command to load the sb3 file.
    1. >> blhost -p COM27 receive-sb-file path_to_SDK\kw45b41_nbu_ble_hosted_a1.sb3

4. Modify an SDK Example

A short video is provided to walk you through this process, or you can follow along the steps below.

4.1 Clone an Example Project from MCUXpresso SDK

Option A: Use the MCUXpresso IDE to import an example project.

Option B: Use the MCUXpresso Config Tool to clone an existing MCUXpresso SDK example for use with third party IDEs.

4.2 Use the Pin Tool

Now, let's use the Pins tool that is part of the MCUXpresso Config Tool to show how to add a new GPIO pin to your project to blink an LED.

MCUXpresso Terminal Tutorial

MCUXpresso Terminal Tutorial

The most recent versions of MCUXpresso IDE count with a terminal emulation application. This tool can be used to display information sent from your NXP development platform's virtual serial port.

  1. Open the MCUXpresso IDE LPC845-BRK-GS-MCUIDETT-
  2. Launch the MCUXpresso IDE terminal by clicking on the "Open a Terminal" button on the top of the IDE or press "Ctrl + Alt + Shift + T" LPC845-BRK-GS-MCUIDETT-
  3. Select Serial Terminal LPC845-BRK-GS-MCUIDETT-
  4. Configure the serial port settings (using the LPCXpresso COM port number) to 115200 baud rate, 8 data bits, no parity and 1 stop bit, then press "OK" button LPC845-BRK-GS-MCUIDETT-
  5. Verify that the connection is open. If connected, MCUXpresso IDE will look like the figure below at the Terminal view LPC845-BRK-GS-MCUIDETT-
  6. You're ready to go

Tera Term Tutorial

Tera Term Tutorial

Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  1. Download Tera Term from SourceForge. After the download, run the installer and then return to this webpage to continue
  2. Download

  3. Launch Tera Term. The first time it launches, it will show you the following dialog. Select the serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
  4. LPC845-BRK-GS-
  5. Configure the serial port settings (using the COM port number identified earlier) to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
  6. Verify that the connection is open. If connected, Tera Term will show something like below in its title bar
  7. LPC845-BRK-GS-
  8. You're ready to go

PuTTY Tutorial

PuTTY Tutorial

PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  1. Download PuTTY using the button below. After the download, run the installer and then return to this webpage to continue
  2. Download

  3. Launch PuTTY by either double clicking on the *.exe file you downloaded or from the Start menu, depending on the type of download you selected
  4. Configure In the window that launches, select the Serial radio button and enter the COM port number that you determined earlier. Also enter the baud rate, in this case 115200
  5. LPC55S69-GS-PUTY-3
  6. Click Open to open the serial connection. Assuming the board is connected and you entered the correct COM port, the terminal window will open. If the configuration is not correct, PuTTY will alert you
  7. LPC845-BRK-GS-
  8. You're ready to go