Getting Started with the TAA6065AT Programming Board

Last Modified: Jun 1, 2026Supports TAA6065AT Programming Board and Development Samples

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits (ICs) and system-in-package (SiP) devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the TAA6065DK1012 programming board.

1.1 Kit Contents and Packing List

The contents of the TAA6065DK1012 kit are:

  • TAA6065DK1012 programming board
  • 20 ICs TAA6065AT development board
TEA2017DK1002-GS-IMG

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

2. Get Hardware

2.1 Board Features

This board can be used for programming small series of TEA2226 samples. Place the jumper on the board in the TEA2017 position prior to programming TEA2226 samples. By connecting both the 3-pin and 6-pin connector to the USB-to-inter‑integrated circuit adapter/interface programming interface, regular production samples and development samples can be programmed after selecting the correct channel with the switch on the USB-I²C interface.

2.2 Board Description

The TEA2226 digital architecture is based on a high-speed configurable hardware state machine ensuring very reliable real-time performance.

Several parameters can easily be configured during evaluation with use of the graphical user interface (GUI):

  • Operating frequencies to be outside the audible area at all operating modes
  • Soft start and soft stop in burst mode, reducing the audible noise
  • Accurate transition levels between operation modes: high-power, low-power or burst
  • Enabling or disabling the lower power mode

TEA2226 samples can be easily programmed using the TEA20xx_SOCKET_DB1586 board in connection with the TEA2016DB1514v2 demo kit and the GUI.

2.3 Board Components

TEA2226 Programming board (SO16 socket)

TAA6065AT Programming Board Top View

TAA6065AT Programming Board Top View

3. Configure Hardware

3.1 Board Components

Both TEA2226AT and TAA6065AT development samples can be programmed by means of the TEA20xx_Socket_DB1586 board + inter‑integrated circuit (I²C) interface (RDK01DB1563). The selector switch on the I²C interface must be set in the TEA2017 position prior to programming TEA2226AT or TAA6065AT development samples.

TAA6065AT Programming Board Angle View

TAA6065AT Programming Board Angle View

Support

Forums

Connect with other engineers and get expert advice on designing with the TAA6065DK1012 on one of our community sites.