1
Out of the Box2
Get Software3
Plug It In4
BuildSign in to save your progress. Don't have an account? Create one.

Figure 1.S32K344EVB-Q257 Evaluation Board
Figure 2.S32K344EVB-Q257 Hero Specs
Something went wrong! Please try again.
You can watch the video or follow the step-by-step guide below to set up your S32K3X4EVB-Q257 evaluation board.
Download and Install S32 Design Studio IDE for S32 Platform.
Note: Check the S32 Design Studio page for the latest version, you will receive activation code through email.
Note: The images displayed on these pages correspond to the software versions available at the time of documentation. For the most up-to-date version, always verify directly through the official download links.
DOWNLOAD S32 DESIGN STUDIO IDE
Something went wrong! Please try again.
Go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates. Navigate to the S32K3xx development package and install it.
Note: In case of installation issues, please ensure that the latest version of S32 Design Studio Platform package and S32 Design Studio Platform Tools package is installed.
Continue with the installation of the Real-Time Drivers for S32K3xx:
Something went wrong! Please try again.
Download and install Elektrobit Tresos Studio / AUTOSAR Configuration Tool from S32K3 Standard Software Package.
Download and install the .exe file of the S32K3 Real-Time Drivers for Cortex-M from the S32K3 Standard Software Package.
The installer will ask for the EB Tresos installation directory on your disk, saving time in configuration.
Note: You will receive an activation code via email. If you installed RTD prior EB Tresos, create a SW32K3_RTD_4.4_x.y.z.link file in: C:\EB\tresos\links folder with the content: "path=C:/NXP/SW32K3_RTD_4.4_x.y.z", where x,y,z refers to installed RTD version.
Something went wrong! Please try again.
S32K3X4EVB-Q172 performs better when using the FreeMASTER Run-Time Debugging Tool.
Note: Check the FreeMASTER page for the latest version.
The FreeMASTER communication driver for S32K3 microcontrollers is also needed; download it from the Automotive SW - S32K3 - S32 FreeMASTER link in the S32K3 Standard Software Package.
Something went wrong! Please try again.
| Default Power-Supply Jumper settings | ||
|---|---|---|
| Jumper | State | Notes |
J13 |
CLOSED | 5 V from FS26 SBC |
J16 |
CLOSED | 3.3 V from FS26 SBC |
J23 |
2-3 | 3.3 V for the VDD_HV_A domain |
J24 |
2-3 | 3.3 V for the VDD_HV_A domain |
J25 |
CLOSED | Shunts for A current measurement bypassed |
J29 |
2-3 | 1 Ohm shunt for B current measurement |
J30 |
5-6 | VDD_HV_A_MCU is routed to VDD_HV_B domain |
J31 |
CLOSED | Shunts for B current measurement bypassed |
J321 |
1-2 | IOREF and AREF at Arduino routed to VDD_HV_A domain |
J360 |
5-6 | V15 domain powered from external NPN ballast transistor |
J37 |
2-3 | V15 NPN ballast transistor powered from VDD_HV_B domain |
J374 |
CLOSED | External circuits powered from VDD_HV_A domain |
J375 |
CLOSED | External circuits powered from VDD_HV_B domain |
J410 |
1-2 | The ADC reference is routed to the VDD_HV_A domain. |
J685 |
1-2 | Select voltage level for FS26 DEBUG pin |
J686 |
CLOSED | Disabled FS26 watchdog after power-up |
| Default Peripherals Jumper settings | ||
|---|---|---|
| Jumper | State | Notes |
J57 |
1-2 | USB to Serial IC powered from 5 V |
J60 |
2-3 | USB to Serial IC Reset pin routed to voltage divider |
J61 |
CLOSED | Ethernet connected to VDD_HV_B_PERF domain |
J62 |
CLOSED | Ethernet Connected to 3.3 V |
J65 |
CLOSED | QSPI flash powered from 3.3 V |
J402 |
CLOSED | QSPI signals level refers to VDD_HV_B_PERF domain |
J390 |
CLOSED | LIN1 Transceiver enabled |
J674 |
2-3 | LIN1 Controller mode via INH pin |
J678 |
CLOSED | LIN2 Transceiver enabled |
J679 |
2-3 | LIN2 Controller mode via INH pin |
J413 |
CLOSED | CAN0 Transceiver enabled |
J672 |
CLOSED | CAN1 Transceiver enabled |
Something went wrong! Please try again.
Switch SW10 to the OFF position (fully to the right).
Connect the 12 V power supply adapter and then switch
SW10 to the ON position (fully to the left).
This power-up procedure manage that SBC starts with the disabled watchdog. Four orange LEDs indicate active 12 V, 5 V, 3.3 V and 1.5V power supply domains.
Something went wrong! Please try again.
Connect a micro-USB cable to the J55 connector to debug via the on-board S32K3 debugger.
Or use one of the available JTAG connectors to debug via the external S32K3 debugger.
Something went wrong! Please try again.
Let's take your S32K3X4EVB-Q257 Evaluation Board for a test drive.
Open S32DS and from the menu, go to: File → New → S32DS Project from Example. Select one of RTD example codes. You may choose between examples with high-level API or with low-level API. For example: Port_example_K344.
Something went wrong! Please try again.
Double-click on the .mex project file.
Please unsure that you configure appropriate project and click on "Update Code" button for generating configuration files.
Something went wrong! Please try again.
Return back to the C/C++ perspective.
Use Debug Configuration menu and select one of predefined debug configurations for building and uploading software into MCU.
Note: If you don't use the default on-board debugger, edit the Debugger tab for your setup.
The S32DS will switch into Debug perspective where you may let the code run.
The red LED will now blink for approximately 10 seconds.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the S32K3X4EVB-Q257 evaluation board using our community sites.
Get the Integrated Development Environment (IDE)
Install the S32K3xx Development Package
Download and Install Elektrobit Tresos Studio and Real-Time Drivers (Only AUTOSAR® Users)
Get the Run-Time Debugging Tool