Accelerate Real-Time System Development | NXP Semiconductors

Last Modified: 2022-03-01 10:30:00Supports Real-Time Drivers (RTD)

Contents of this document

  • 1

    Configure Software
  • 2

    Support Package Installation

1. Installation

The following process is how to set up the S32DS, S32K3 and RTD SDK software.

1.1 S32DS and S32K3 RTD SDK Installation

  1. Get into the S32K3 Standard Software offerings using your NXP account.
  2. K3-STANDARD-SW
  3. Download the latest version of the RTD SDK, S32DS and S32K3 Support Package.
  4. K3-STANDARD

    K3-STANDARD-SW2

2. Support Package Installation

2.1 S32DS and S32K3 RTD SDK Installation

  1. Run the S32 Design Studio v3.4 Windows installer using using the S32DS.3.4_b201217_win32.x86_64.exe and License Keys → Activation Code
  2. Install the S32 Design Studio 3.4 development packages for offline use, support for S32K3 family in S32DS 3.4 using the SW32K3_S32DS_3.4.1_D2018.zip

    K3-STANDARD-SW-INSTALL

    K3-STANDARD-SW-INSTALL

    The S32K3XX_RTD_4_4_EAR_0_8_0_DS_updatesite_2008.zip is already included in the S32K3 support package

    For the latest S32K3xx RTD 0.9.0, you should download and install SW32K3_RTD_4.4_0.9.0_DS_updatesite_D2103.zip

    K3-STANDARD-SW-INSTALL2

    K3-STANDARD-SW-INSTALL2

    K3-STANDARD-SW-INSTALL3

    K3-STANDARD-SW-INSTALL3
  3. Install and update the RTD SDK:
  4. K3-STANDARD-SW-INSTALL4

    K3-STANDARD-SW-INSTALL4

    K3-STANDARD-SW-INSTALL5

    K3-STANDARD-SW-INSTALL5
  5. Find the RTD SDK files in the following path, after installation:

    C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_03
  6. K3-STANDARD-SW-INSTALL6

    K3-STANDARD-SW-INSTALL6

Support

Forums

Connect with other engineers and get expert advice on designing with the S32K144EVB on one of our community sites.