Battery Management Low Cost Dev Board

Last Modified: 2020-06-04 06:51:53Supports MPC5775B/E low-cost BMS and Inverter Development Board

Contents of this document

  • 1

    Get Software
  • 2

    Plug It In
  • 3

    Load and Run

1. Get Software

Let's take your MPC5775B/E-EVB highly-integrated low-cost development boards for Battery Management and Inverter applications for a test drive!

Check the AN12875: Getting started with the MPC5775B-EVB and MPC5775E-EVB

1.1 Get the OpenSDA Serial Driver

Install the OpenSDA serial driver if necessary, in order to make the COM port available as an OpenSDA port. It can be checked under "COM and LPT Ports" as "OpenSDA – CDC Serial Port" in the Device Manager.

Get the Open SDA serial driver

1.2 Get Your Integrated Development Environment (IDE)

MPC5775B/E-EVB performs better when using S32 Design Studio for Power Architecture® IDE

Download S32 Design Studio for Power Architecture

2. Plug It In

2.1 Plug the USB Serial Cable

Connect the micro USB cable to J116 micro USB port.

If the driver is available:
You will be able to see the OpenSDA – CDC Serial Port

If the driver is not available:
Go to the Device Manager and right-click the COM port detected and select Update Driver Software.
Select Browse > My Computer for driver software and select the downloaded OpenSDA driver.

2.2 Setup Tera Term Console

Open Tera Term on Windows® PC.
Select the serial port to which the micro USB of the development board is connected and click OK. Go to Setup > Serial Port and select 19200 as the baud rate.

Let's take your MPC5775B/E-EVB highly-integrated 2.2

2.3 Connect the MPC5775B/E Low-cost Development Board

Connect power supply to power socket and micro USB cable to micro USB port on the development board.
Make sure the status LEDs D14, D15, D16, and D32 for voltage levels 3.3V, 5V, 1.25V and 12V supply respectively are glowing green on the board.

2.4 Reset the MPC5775B/E Low-cost Development Board

After resetting the board by pressing the "Reset" button (SW1)

Let's take your MPC5775B/E-EVB highly-integrated 2.4a

Let's take your MPC5775B/E-EVB highly-integrated 2.4a

You will be able to see the welcome message on the terminal:

Let's take your MPC5775B/E-EVB highly-integrated 2.4b

3. Load and Run

3.1 Load Example in S32 Design Studio for Power Architecture® IDE

Open S32 Design Studio IDE and make or select a workspace, then click OK

Let's take your MPC5775B/E-EVB highly-integrated 3.1a

Go to New > S32DS Design Project from Example from the File menu

Let's take your MPC5775B/E-EVB highly-integrated 3.1b

Scroll down to the SDK PARTM v3.0.0 Example Projects and select MPC5777C
Then select Hello_world_mpc5777c and click Finish

Let's take your MPC5775B/E-EVB highly-integrated 3.1c

3.2 Generate Code Using Processor Expert

Click on the Generate Processor Expert Code icon:

Let's take your MPC5775B/E-EVB highly-integrated 3.2

3.3 Debug the Code by Using the Debug Configuration Wizard

Click on Run > Debug Configuration…
Select the Debugger tab and then select the OpenSDA Embedded Debug – USB Port interface

Let's take your MPC5775B/E-EVB highly-integrated 3.3a

The "Port" should automatically be selected if the EVB is connected to the computer.
Click Apply, then click Debug, and finally click Yes.

Let's take your MPC5775B/E-EVB highly-integrated 3.3b

3.4 Load the Code

Click the Resume icon to observe the blinking LED D20.

Let's take your MPC5775B/E-EVB highly-integrated 3.4b

Click the Terminate icon to end the program execution.

Let's take your MPC5775B/E-EVB highly-integrated 3.4b