1
Out of the Box2
Get Software3
Plug It In4
Create, Build and LoadSign in to save your progress. Don't have an account? Create one.

Applies for the DEVKIT-MPC5744P development board REV E.
Note: For additional information, check the DEVKIT-MPC5744P REV B – Quick Start Guide .
DEVKIT-MPC5744P development board REV E:
DEVKIT-MPC5744P development board REV B:
Differences between REV E and REV B:
Interface:
LIN0 (LIN1 on REV B)LIN1 using the PowerSBC physical layer (LIN0 on REV B using MC33662BLEF driver)CAN0 using the PowerSBC physical layer (CAN0 on REV B using MC33901WEF driver)REV B)Power:
REV B)Something went wrong! Please try again.
Something went wrong! Please try again.
Note: For high power/current consuming applications (like using external shield boards) use “External 12 V Supply” only.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
DEVKIT-MPC5744P performs better when using S32 Design Studio for Power Architecture®.
Note: Check the S32 Design Studio page for the latest version.
Download S32 DESIGN STUDIO IDE
Something went wrong! Please try again.
Some application examples output data over the MCU UART. Make sure you have installed the driver for the board’s virtual COM port.
Note: You must plug the board into your PC before you run the driver installer.
When the serial port driver is installed, run any terminal application to view the serial output from the MCU UART. Configure the terminal to 57,600 baud rate, 8 data bits, no parity and 1 stop bit.
Note: To determine the port number of the DEVKIT-MPC5744P's virtual COM port, open the device manager and look under the "Ports" group.
Learn more about Using a Terminal Application at Projects and Tutorials.
Something went wrong! Please try again.
Watch the video to set up your development board. You can also use the step-by-step guide.
Connect one end of the USB cable to the PC and the other end to the micro-B connector on your board.
Allow the PC to automatically configure the USB drivers.
Something went wrong! Please try again.
Your DEVKIT-MPC5744P comes pre-loaded with a demo using the potentiometer and the user LEDs.
Once the board is plugged in, the ADC in the DEVKIT-MPC5744P will scan the RV1 potentiometer result. Different combinations of the RGB LEDs
power on as you turn it.
Note: The clock is configured so the PLL runs at 160 MHz.
Something went wrong! Please try again.
Watch the video to create a new project and load a code example. You can also use the step-by-step guide.
Note: Uncheck the box "Use this as default and do not ask again".
Elf S32DS Project for this one
Something went wrong! Please try again.
Use one of these two paths to create a project:
icon to build the project, then click the
icon to build all projectsThe following message will be displayed on the console once you successfully build a project:
Something went wrong! Please try again.
Note: For DEVKIT-MPC5744P, OpenSDA works as a debug adapter, so no standalone debugger is required.
Select a Project, Interface and Port, then click Debug
(Example: "FirstProject_Debug" and "OpenSDA for DEVKIT-MPC5744P")
Something went wrong! Please try again.
Follow one of these paths to debug from RAM:
Note: Repeat for all related projects and follow the steps in 4.2 Build a New Project in IDE.
Finally, to debug from RAM, select the RAM-related session while debugging.
Note: Follow the steps in 4.3 Debug a Project in IDE.
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Launch Tera Term and select Serial
Note: The COM port will be automatically populated in the list if your board is already plugged in.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Note: Baud rate of 57,600 is recommended.
Note: The terminal window will open if your board is already plugged in. PuTTY will alert you if the configuration is not correct.
Note: These tutorials are generic, so specific values like baud rates and data bit configurations may not apply to DEVKIT-MPC5744P code examples. Check the comments in each example project for specific instructions for each code example.
When the installer wizard window is displayed, click Next
Selecting the S32 Design Studio only installs this software. To install more softwares, select "Additionally Install" option
Choose either the default or new installation location, then click Next
Note:Use a path without spaces for the installation location.
At some point during the installation, you will be prompted for the software activation code
To get your activation code, go to the Product Download page and select the License Keys tab
OpenSDA is an open-standard serial and debug adapter. It bridges serial and debug communications between a USB host and an embedded target processor.
The DEVKIT-MPC5744P comes with the OpenSDA Application preinstalled.
Follow these instructions to run the OpenSDA Bootloader and update or change the installed OpenSDA application.
SW4 Bootloader EntrySDA)SW4 Bootloader EntryA removable drive should now be visible in the host file system with a volume label of BOOTLOADER.
You are now in OpenSDA Bootloader mode.
SDA_INFO.HTML in the BOOTLOADER drive. A web browser will open the OpenSDA homepage containing the name and version of the installed application. This information can also be read as text directly from
SDA_INFO.HTML
The new OpenSDA Application should now be running and check the latest version by repeating first step.
Use the same procedure to load other OpenSDA applications.
Determine the symbolic name assigned to the DEVKIT-MPC5744P virtual serial port
In Windows, open Device Manager and look for the COM port named OpenSDA-CDC Serial Port
Open the serial terminal emulation program of your choice
For Windows you can use Tera Term , PuTTY or HyperTerminal
SW1 Reset button at any time to restart the example application. Resetting the embedded application will not affect the connection of the virtual serial port to the terminal program
Note: Refer to the OpenSDA User's Guide for a description of a known Windows issue when disconnecting a virtual serial port while the COM port is in use.
Connect with other engineers and get expert advice on designing with the DEVKIT-MPC5744P Application Processor on one of our community sites.
Get to Know Your Evaluation Board
Understanding the Header/Pinout
Understanding the Power Supply Settings
Understand the User Peripherals
Understanding Programming Interfaces
Understanding Communication Interfaces
Understanding Indication LEDs
Understanding Test Points
Understanding Safety Functionalities
Understanding the MPC574xP Family Phantom Feature Differences
Understanding the MPC5744P Package Level Pinout Diagram
Download the DEVKIT-MPC5744P Development Board – Quick Start Package
Get your Integrated Development Environment (IDE)
Get your PC Configuration Driver