1
Out of the Box2
Get Software3
Plug It In4
Build, LoadSign in to save your progress. Don't have an account? Create one.

The electrification X-in-1 platform consolidates multiple vehicle electrification applications into a single electronic control unit (ECU). By combining functions that traditionally require separate ECUs, this platform helps reduce hardware complexity, system cost and weight while supporting efficient safety and security management.
This getting started guide walks you through how to set up, build and run the 2-in-1 DC-DC converter and traction inverter using the S32K396 microcontroller (MCU) to control both applications on a shared platform.
In addition to the kit contents, the following hardware is recommended when working with this kit:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is recommended when working with this kit:
Something went wrong! Please try again.
For evaluation, you will need a PC running Windows or Linux that also meets the minimum system requirements for NXP FreeMASTER.
Something went wrong! Please try again.
In this step, you will confirm that the required software libraries are installed and compatible with the other software components in this project. You may have some of these libraries already installed on your PC.
After successfully downloading the .exe file, during the installation, you will change the default path to:
C:/<local_path>/S32DS.3.6.0/S32DS/software/http://www.nxp.com/lgfiles/updates/Eclipse/AMMCLIB/S32DS_3.5Something went wrong! Please try again.
In this step, you will install the updatesite for the IPCF in S32DS.
To configure IPCF for use with EB tresos Studio, follow these steps:
SW32K396_IPCF_1.1.0_D2502.exe to install the application<proj_path>/ X-in-1/eenvs/S32K396/2-in-1_DC-DC_Inverter/M7_2_MSC/S32K396_SSM_core2/util/SW32K396_IPCF_1.1.0_D2502/eclipse/plugins/Ipcf_TS_T40D34 M11I0R0plugin.xml fileSomething went wrong! Please try again.
After installing S32 DS and FreeMASTER, you will link the source files to the master safety core, built using Tresos Studio.
Once the project is open in Tresos Studio, follow these steps:
<proj_path>/ X-in-1/eenvs/S32K396/2-in-1_DC-DC_Inverter/M7_2_MSC/S32K396_SSM_core2/util/common.makThen locate the following line:
Figure 1: Adding the path to FreeMASTER.
S32DS.3.6.0/S32DS/software/FreeMASTER_S32K3_v3.0/srcSomething went wrong! Please try again.
Once you have installed the SW32K3_SAF_1.0.5_EVAL_D2502 driver using the .exe file, proceed through these steps:
C:/EB/tresos/plugins/:
Bist_TS_T40D34M10I5R0eMcem_TS_T40D34M10I5R0mSel_TS_T40D34M10I5R0Safetybase_TS_T40D34M10I5R0sBoot_TS_T40D34M10I5R0sCheck_TS_T40D34M10I5R0sReco_TS_T40D34M10I5R0cd C:/<project_location>/build/export S32K39X_EB_ACP_DIR=C:/EB/tresos/export S32K3_SAF_DIR=C:/NXP/SW32K3_SAF_1.0.5_EVAL_D2503/eclipse/pluginspython build_instance.py -c ../X-in-1/build.json --patch allSomething went wrong! Please try again.
In this step, you will prepare to run the prebuilt binaries or build an electrification X-in-1 project from source.
To run an electrification X-in-1 project using the provided prebuilt binaries, install the required debugging tools and sign in to the NXP software catalog. You do not need to install the build dependencies unless you plan to build the project from source.
To build an electrification X-in-1 project from source:
Note: If your account does not have access to one or more premium software releases, you can still run the projects by flashing the provided prebuilt binaries. This option does not require you to build the projects from source, but the required debugging tools must be installed.
Something went wrong! Please try again.
To give you an idea of how to set up your lab bench, Figure 2 below provides an example.
Figure 2. 2-in-1 Inverter Lab Bench Hardware Layout.
Each numbered label in the image above corresponds to the matching item details in the list below:
Something went wrong! Please try again.
In addition to the X-IN-1 Modular Platform Design page, visit the related hardware and software pages.