1
Out of the Box2
Get to Know the Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the EVBMLC2HOST and EVBMLC2PER evaluation boards.
The kit contents include:
D-Sub 9 connectors. The red/black cable is terminated with banana jacksSomething went wrong! Please try again.
In addition to the kit contents, the following hardware can be either beneficial or even necessary when working with the kit:
The board is useful for individually powering up to six LED boards with a DC voltage of up to 60 V, while respecting a desired maximum current limit.
Something went wrong! Please try again.
This evaluation board requires a laptop running Windows 10 or Windows 11 with at least one of these operating systems installed.
Something went wrong! Please try again.
Installing the software—NXP MLC GUI or, as an alternative, CANoe based GUI—is essential for being able to work with the evaluation kit.
Something went wrong! Please try again.
The EVBMLC2HOST offers the possibility to modify the least significant part of the CAN address by positioning five switches. Furthermore, it integrates a 5 V low dropout regulator (LDO) and a CAN transceiver embedded in the UJA1163ATK system-basis chip (SBC).
Built into the ASL6112SHN, the EVBMLC2HOST additionally has the following features:
The EVBMLC2PER has the following features built into the ASL6112SHN:
The EVBMLC2PER offers the possibility to modify the least significant part of the CAN address by positioning five switches.
However, as the EVBMLC2PER has no UJA1163ATK SBC, it misses the 5 V low dropout regulator (LDO) and the CAN transceiver. The reason being that for the EVBMLC2PER to work, it must be connected to the EVBMLC2HOST. The connection allows the EVBMLC2PER to access the 5 V low drop out (LDO) and the CAN transceiver present on the host board, which are shared hardware resources.
Something went wrong! Please try again.
The EVBMLC2HOST, whose appearance is shown in Figure 5 and whose schematic is given in Figure 7, includes the following components:
J1 female DB9 sub-connector – Supplies the board with 12 V and communication via the
CAN cableJ2 female connector – Connects to EVBMLC2PER(Plug the six-pin J1 male connector belonging to the EVBMLC2PER board into this connector)
J3 male connector – Connects to LED boardJ4 jumper – Controls supply to the board(Add a short to this jumper, otherwise the board remains unsupplied, thus when the board is supplied, a red LED emits light)
DB9 sub-connector and the J4
jumper has been
provided with a shortS1 five-switch block – Sets the board physical addressThe initial address is 0b11111 and is equivalent to decimal 32. The switch at position 5 corresponds to
the
least
significant bit, while position 1 corresponds to the most significant bit. It is highly recommended to change the
switch positions to get a small address. For instance, 0b00000 = 0 decimal. To get this address value,
move
all five switches shown in Figure 5 to the opposite position.
Notice that the ID resistor and the NTC have not been populated. This is because they belong to the domain of the LED board.
The EVBMLC2PER, whose appearance is shown in Figure 6 and whose schematic is given in Figure 8, includes the following components:
J1 male connector – Connects to EVBMLC2HOSTPlug the six-socket J2 female connector belonging to the EVBMLC2HOST board onto this connector.
J2 female connector – Plugs onto the six pins J1 male connector belonging to the
adjacent boardJ3 male connector – Connects to LED boardS1 five-switch block – Sets the physical address of the ASL6112SHNThe initial address is 0b11111, equivalent to decimal 32. The switch at position 5 corresponds to the
least
significant bit, while position 1 corresponds to the most significant bit. It is highly recommended to change the
switch positions to get a small address (for instance 0b00001 = 1 decimal). To get this address value,
the four
switches labeled 1 to 4, shown in Figure 6, must be moved to the opposite position. For a peripheral board,
it is good practice to use a higher address than the host card address. If more peripherals needed, continue
incrementing the address by one unit.
Notice that the ID resistor and the NTC have not been populated. This is because they belong to the domain of the LED board.
Something went wrong! Please try again.
The schematics of the boards follow. For board layout and routing information, see reference 1 in Section 3.2.
Something went wrong! Please try again.
NXP Semiconductors provides online resources for this evaluation board and its supported devices on NXP.
An alternative evaluation GUI—usable under the CANoe environment—can be downloaded by logging in to your secured NXP account. Once in the secured area, type the following string in the search bar: "ASL6112SHN CANoe project". You will be redirected to the download. The Vector CANoe project is intended for those who have a Vector CAN interface, such as the VN1630A.
Something went wrong! Please try again.
In addition to our ASL61XXYHZ, you may also want to visit: Automotive Advanced Exterior Lighting.