1
Out of the Box2
Get to Know the Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KIT6X02AF2T1 board.
The kit contents include:
Something went wrong! Please try again.
The purpose of the KIT6402AF2T1 is to build and interface from CAN to transport protocol link (TPL). The KIT6402AF2T1 can be used in any regular CAN environment. It can also be used with NXP PC software (that is, scripting GUI) to communicate via TPL to attached NXP devices (that is, BMA7118, BMA7418, BMA8420 or similar). To use the KIT with the NXP PC software, extra hardware is required.
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KIT6x02AF2T1 or from the provided link.
Something went wrong! Please try again.
The main features of the KIT6X02AF2T1 are:
The main features of the KIT6X02AF2T1 are:
The KIT6X02AF2T1 serves as a hardware tool-supporting evaluation of ETPL devices via a CAN interface. Control of the CAN bus can be done with any CAN environment. If no specific environment is available, there is also a software solution from NXP available that allows the evaluation of a BMS system.
Something went wrong! Please try again.
The KIT6X02AF2T1 serves as a hardware tool-supporting evaluation of ETPL devices via a CAN interface. Control of the CAN bus can be done with any CAN environment. If no specific environment is available, there is also a software solution from NXP available that allows the evaluation of a BMS system.
Something went wrong! Please try again.
Connector J6 connects the KIT6402AF2T1 to the supply and CAN cable.
Table 1. Interface - J5.
| Pin number | Connection | Description |
|---|---|---|
| 1 | VBAT | Battery supply Apply a voltage from 6 V to 18 V for normal operation of the board. |
| 2 | CANH | CAN high-line |
| 3 | CANL | CAN low-line |
| 4 | GND | Supply ground |
Connectors J1 and J2 connects to the KIT6402AF2T1 TPL ports 0 and 1.
Table 2. TPL port 0 - J1.
| Pin Number | Connection | Description |
|---|---|---|
| 1 | TPL0_P | TPL port 0 (positive) |
| 2 | TPL0_N | TPL port 0 (negative) |
Table 3. TPL port 1 - J2.
| Pin Number | Connection | Description |
|---|---|---|
| 1 | TPL1_P | TPL port 1 (positive) |
| 2 | TPL1_N | TPL port 1 (negative) |
The KIT6X02AF2T1 offers access to various debugging points to allow a fast evaluation of the product. The debugging points are shown in Figure 2.
The CAN traffic can be monitored either on the CAN physical layer (J9), or on the digital pins (J14). See Table 4
for details of the settings.
Table 4. CAN signals - J14.
| Header number | Function | Description |
|---|---|---|
| 1 | GND | Ground as reference |
| 2 | CAN_TXD | CAN transmitt |
| 3 | CAN_RXD | CAN receive |
The BMA6X02C can route various status and sideband signals to the GPIO pins. These status signals can be useful for traffic monitoring and debugging. See the data sheet of the BMA6X02C for further details.
Table 5. GPIO pins -J13.
Something went wrong! Please try again.
The KIT6X02AF2T1 has several configuration options. The most important ones are the CAN speed and CAN ID configuration of the BMA6X02C. This configuration can be changed with the switches on the board (See Figure 3).
The reset button initiates a reset of the BMA6X02C on the board. The DIP switches (SW2) configure the CAN
communication speed and the CAN-ID used for communication. See for details of the settings in Table 6.
Note: Putting a switch in ON position means that the pin reads as LOW. Putting the switch downwards means that the pin reads as HIGH.
Table 6. DIP switches -J5.
Something went wrong! Please try again.
In addition to our KIT6X02AF2T1: Product description page, you may also want to visit: Product pages: S32K358BMU, S32K344BMU.