1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. This incorporates monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component count, lower cost and improved performance in powering state-of-the-art systems.
This page guides you through the process of setting up and using the MR-BMS771 board.
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Note: The MR-BMS771 board is designed to open the charge circuit when the battery is overcharging. Therefore, the charger does not need to have a battery management system Battery Management System (BMS) connector.
Something went wrong! Please try again.
Installing software is necessary to work with this reference design. All listed software is available on the reference design information page at MR-BMS771.
Something went wrong! Please try again.
Something went wrong! Please try again.
The MR-BMS771 is a standalone BMS reference design suitable for mobile robotics, such as drones and rovers that supports 7-cell to 14-cell batteries.
The device performs analog-to-digital conversion on the differential cell voltages and currents. It is capable of accurate battery charge coulomb counting and battery temperature measurements. It can also communicate with a flight management unit (FMU) through DroneCAN/CyphalCAN and/or a System Management Bus (SMBus).
Something went wrong! Please try again.
As the MR-BMS771 board aims to be adaptable for every battery setup, power and battery cell-terminal connectors are not pre-mounted on the Printed Circuit Board (PCB). This allows the user to configure the board with the connector.
The power-connector footprints on the design correspond to the DFRobot FIT0588 connector. These footprints also support soldering typical insulated heavy-gauge power wires. TE Connectivity provides a line unmanned power (UMP) connectors, specifically for professional high‑power mobile systems.
Something went wrong! Please try again.
The MR-BMS771 board can be configured to fit 7S to 14S battery packs.
Depending on the desired configuration, some adjustments must be made on the board:
Something went wrong! Please try again.
The shunt resistor (R1) can be disconnected from the overcurrent protection circuit and the Battery Control Circuit (BCC) by opening the
SJ13 and SJ14 jumpers. Both jumpers are closed by default.
Something went wrong! Please try again.
The external antenna is selected by default.
The onboard NTAG 5 chip is designed to provide active antenna matching and amplification, giving enhanced performance when the battery is present and providing power. However, for extended-range operation, an external NFC antenna can replace the PCB antenna.
To use the PCB antenna, the user must reconfigure the board using the following steps:
The NTAG 5 chip is not installed for the first batch.
Something went wrong! Please try again.
Depending on the application, the user can add an optional heat sink onto the MR-BMS771 board. The recommended part to use as a heat sink is the HSB30-373710.
It is recommended that you use an electrically isolated yet quality thermally conducive layer (for example, a special adhesive tape) between the BMS771 and the heat sink. This will improves the thermal conductivity.
Something went wrong! Please try again.
In addition to our MR-BMS771 page, you may also want to visit: