Getting Started with the KITPF9455FRDME Evaluation Board

Last Modified: Jul 23, 2026Supports KITPF9455FRDME

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Plug It In
  • 4

    Configure the Board

1. Out of the Box

The KITPF9455FRDME board kit allows you to evaluate, design, implement and validate the PF9455 power management integrated circuit (PMIC) for high-performance applications.

This getting started guide will walk you through the process of setting up and using the KITPF9455FRDME board.

1.1 Kit Contents and Packing List

The kit's contents include:

  • Assembled and tested KITPF9455FRDME evaluation board with preprogrammed KL25Z microcontroller (MCU) in an antistatic bag
  • Quick Start Guide
  • 3.0 ft USB-STD A to USB-C-micro cable
  • Six Phoenix connectors, two positions, straight, 10 mm
  • Jumpers mounted on board

1.2 Additional Hardware

In addition to the kit's contents, the following hardware provides further support when using this board.

  • Power supply capable of providing 5 V

1.3 Minimum System Requirements

You will need a Windows PC workstation to evaluate the board. For best results, please use the following equipment:

  • USB-enabled computer with Windows 7 or Windows 10
  • FTDI USB serial port driver for the FT230X basic universal asynchronous receiver-transmitter (UART) device

1.4 Software

Before working with the board, you will need to install software. You can find the software at the PF9455 evaluation board's page or from the NXP PMIC GUI.

2. Get Software

This section covers the board components and features.

2.1 Board Features

The KITPF9455FRDME evaluation board includes the following features:

  • Phoenix 10 mm male connector or jack connector for power supply input
  • Phoenix 10 mm male connectors for PMIC switcher outputs
  • Header connectors for input/output (I/O) configuration
  • Selectable power input for programming
  • Access pin connectors for monitoring inputs and outputs
  • Red and green LEDs to indicate signal or regulator status
  • Blue LED to indicate that the one-time programmable (OTP)8 V burning voltage is set
  • Advanced system monitoring via the KL25Z MCU
  • Embedded USB-to-inter-integrated circuit (I²C) protocol for connecting to the software GUI through the KL25Z MCU

2.2 Board Description

The KITPF9455FRDME evaluation board integrates a KL25Z MCU to support communication between the board and the PC-based GUI to control and monitor of the PF9455 device.

2.3 Board Components

The diagram below shows you the communication paths between the components.

Figure 1. Overview Diagram of Communication Between PF9455 and NXP

Figure 1. Overview Diagram of Communication Between PF9455 and NXP

Figure 2 below shows the placement of connectors, configuration headers, and LED indicators on the KITPF9455FRDME evaluation board For the default jumper and switch configuration, refer to the KITPF9455FRDME product page.

Figure 2. KITPF9455FRDME – Location of Key Components

3. Plug It In

3.1 Plug It In

Follow the steps below to set up the KITPF9455FRDME board:

  1. Verify that the jumpers and switches are configured in their default positions
  2. Connect the power supply to VIN-J47 (the 10 mm Phoenix connector)
  3. Connect the USB cable between the board and the PC

To launch the PF9455 NXP Graphical User Interface (GUI):

  1. Click the Windows icon
  2. Locate NXPGUI in the Windows All apps bar
  3. Click the NXPGUI icon to launch the GUI

4. Configure the Board

4.1 Configure the Board

This section will walk you through the KITPF9455FRDME evaluation board configuration. You will get an explanation of the features associated with each jumper and switch details on enabling features through hardware configuration and advice on the LED signaling and test points available on the board.

The default debug configuration enables the board to be fully controlled by the KL25Z MCU (via I2C) and the GUI. Figure 2 below shows the default jumper and switch configuration for PF9455.

Reference Description Settings for configuration External configuration
J1 Power-on (PWRON) pullup voltage selection. Pins: 1 to 2 VIN Open
Pins: 2 to 3 VAON Open
J2 One-time programmable supply voltage (VDDOTP) connection. Pins: 1 to 2 VDIG Open
Pins: 2 to 3 VDDOTP_BST Connected
J9 Fault collection and control unit 0 (FCCU0) input level connection. Pins: 1 to 2 VDDIO -
Pins: 2 to 3 GND -
J10 Fault collection and control unit 1 (FCCU1) input level connection. Pins: 1 to 2 VDDIO -
Pins: 2 to 3 GND -
J20 Power on connection to interface system. Pins: 1 to 2 Connected Connected
J24 Selection of external VDDIO voltage (1 to 2: 1.8 V <–> “2 to 3”:3.3 V). Pins: 1 to 2 1.8V -
Pins: 2 to 3 3.3V Connected
J29 RSTB pullup to VDDIO, connect for operation. Pins: 1 to 2 Connected Connected
J36 External input/output supply voltage (VDDIO) power Input selection. Pins: 1 to 2 External Connected
Pins: 2 to 3 SW1 -
J48 Low-dropout regulator 1 (LDO1) input voltage. Pins: 1 to 2 VSW_IN Connected
Pins: 2 to 3 SW1_OUT -
J49 Low-dropout regulator 2 (LDO2) input voltage. Pins: 1 to 2 VSW_IN Connected
Pins:2 to 3 SW1_OUT -
J50 Low-dropout regulator 3 (LDO3) input voltage. Pins: 1 to 2 VSW_IN Connected
Pins: 2 to 3 SW1_OUT -
J54 USB jumper. Used to connect to USB power. Open for using external power supply (VIN). Connect external power for correct operation. Pins: 1 to 2 Used- USB power Open - external power supply Open
Reference Function Description
J39 Switcher 2 (SW2) output PMIC switcher 2 output voltage direct connection to PMIC pin.
J40 Switcher 3 (SW3) output PMIC switcher 3 output voltage direct connection to PMIC pin.
J41 Switcher 4 (SW4) output PMIC switcher 4 output voltage direct connection to PMIC pin.
J42 SW5 output PMIC switcher 5 output voltage. Direct connection to PMIC pin.
J43 Switcher 5 (SW5) output PMIC switcher 5 output voltage direct connection to PMIC pin.
J47 Switcher 1 (SW1) output PMIC switcher 1 output voltage direct connection to PMIC pin.
Reference Function Description Color
BH1 Ground (GND) Board grounds direct connection through four access points Black
BH2
BH3
BH4
TP119 Low-dropout regulator 1 input (LDO1IN) Monitoring point for the LDO1 input voltage. Red
TP120 Low-dropout regulator 2 input (LDO2IN) Monitoring point for the LDO2 input voltage. Red
TP121 Low-dropout regulator 3 input (LDO3IN) Monitoring point for the LDO3 input voltage. Red
TP61 Low-dropout regulator 1 output voltage (VLDO1) Monitoring point for the LDO1 output. Red
TP60 Low-dropout regulator 2 output voltage (VLDO2) Monitoring point for the LDO2 output. Red
TP59 Low-dropout regulator 3 output voltage (VLDO3) Monitoring point for the LDO3 output. Red
TP15 Always-on voltage output (VAON) Monitoring point for the VAON output. White
TP90 Switcher 1 feedback (SW1 FB) Monitoring point for the SW1 feedback. White
TP86 Switcher 2 feedback (SW2 FB) Monitoring point for the SW2 feedback. White
TP87 Switcher 3 feedback (SW3 FB) Monitoring point for the SW3 feedback. White
TP91 Switcher 4 feedback (SW4 FB) Monitoring point for the SW4 feedback. White
TP92 Switcher 5 feedback (SW5 FB) Monitoring point for the SW5 feedback. White
TP78 Voltage monitor 1 (VMON1) Monitoring point for the external monitor VMON1. Orange
TP79 Voltage monitor 2 (VMON2) Monitoring point for the external monitor VMON2. Orange
TP65 XFAILB XFAILB PMIC access point, bidirectional pin. White
TP57 General-purpose input/output 1 (GPIO1) GPIO1 access point, bidirectional pin. White
TP20 General-purpose input/output 2 (GPIO2) GPIO2 access point, bidirectional pin. White
TP56 General-purpose input/output 3 (GPIO3) GPIO3 access point, bidirectional pin. White
TP8 General-purpose input/output 4 (GPIO4) GPIO4 access point, bidirectional pin. White
TP4 Inter-integrated circuit serial data (I²C-SDA) I²C SDA access point, bidirectional pin. White
TP5 Inter-integrated circuit serial clock (I²C-SCL) I²C SCL access point, bidirectional pin. White
TP9 Frequency synchronization (FSYNC) FSYNC access point, bidirectional pin. White
TP55 Analog multiplexer output (AMUX) Analog multiplexer output monitoring point. White
TP12 Reset signal output (RSTB) Systems set signal output monitoring point. White
TP3 Fail-safe output 0 (FS0B) Fail-safe output monitoring point. White
TP10 Interrupt output (INTB) INTB output monitoring point. White
TP52 Fault collection and control unit 0 (FCCU0) FCCU0 fault monitoring input pin access point. White
TP53 Fault collection and control unit 1 (FCCU1) FCCU1 fault monitoring input pin access point. White
TP6 Standby input (STBY) STBY input pin access point. White
TP2 Standby input (STBY) PGOOD input pin access point. White
TP7 PWRON Power on input pin access point. White

Design Resources

Additional References

In addition to the PF9455 page, reference the PF09 or PF0300 pages and KITPF9455FRDME, KITPF9455FRDMPGM or I.MX94 hardware pages.