Enablesengineers with flexibility to design high performance applications with freedom
Embedded World 2016 – Nuremberg, Germany, February 23, 2016 –NXPSemiconductors N.V. (NASDAQ: NXPI) today introduced the AXP family of logictranslators, designed for low-power and high-performance applications. Thefamily of AXP translators is the lowest power voltage translator solution inthe market while also offering the widest range of voltage translation from 0.7volts to 5.5 volts. The AXP translators (AXPnT) are ideal for high performanceapplications with Microprocessors/Microcontrollers/SOCs operating at ultra-lowvoltages below 1.8 volts that still need to interface with I/O peripheralsolutions typically operating at 2.5 V, 3.3 V, or even 5.5 V.
In 2014, NXP introduced the AXPfamily of logic devices, offering the lowest power logic functions in theindustry. With today’s introduction of the AXPnT, NXP now offers solutions to interfacingMicroprocessors/Microcontrollers/ASICs operating as low as 0.7 V to peripheraldevices operating as high as 5.5 V.
The AXPnT includes standard buffers,as well as gates and configurable functions. They are available in both leaded and leadless package options, including NXP’s 5-and 6-pin GX packages. These packages arethe smallest leadless logic packages in the industry. By providing the lowestpower voltage translator products, NXP Semiconductors continues to support themigration of applications to lower voltages. The result is greater powersavings for battery powered applications, while at the same time facilitatingthe interfacing of lower-voltage ASICs, microprocessors, microcontrollers, orSOC chips with legacy higher-voltage peripheral devices in the market place.
Features of AXPnT devices
· Dualsupply voltage level translation
o VCCI= 0.7 V to 2.75 V
o VCCO= 1.2 V to 5.5 V
· Verylow dynamic power dissipation (CPD)
· Schmitt-triggeraction on all inputs
· 12mAbalanced output drive
· Over-voltagetolerant inputs and outputs
· Leaded and Leadless Package Options
· Fully specified(-40 to +85 °C)
· Pb-free,RoHS compliant and Dark Green
Availability
The AXPtranslator family of devices are expected to sample in February 2016.
Links
Productinformation: www.nxp.com/logic
50 Years of Logic: Leading volume supplier of Logic worldwide
NXPSemiconductors is committed to the logic market and continually invests in newprocess and package technologies, as well as packaging facilities, to offer aleading-edge portfolio. Over the last 50 years, the NXP logic business—startingas Philips Semiconductors—has supported growing global demand for logic. As theNo. 1 volume supplier in the world, NXP can support the highest volume logicrequirements, while offering a broad variety of industry-leading packagesolutions.
– End –
About NXP Semiconductors
NXP SemiconductorsN.V. (NASDAQ: NXPI) enables secure connections and infrastructure for a smarterworld, advancing solutions that make lives easier, better and safer. As theworld leader in secure connectivity solutions for embedded applications, NXP isdriving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years ofcombined experience and expertise, the company has 45,000 employees in morethan 35 countries.
Forward-looking Statements
This document includesforward-looking statements which include statements regarding NXP’s businessstrategy, financial condition, results of operations and market data, as wellas other statements that are not historical facts. By their nature,forward-looking statements are subject to numerous factors, risks anduncertainties that could cause actual outcomes and results to be materiallydifferent from those projected. Readers are cautioned not to place unduereliance on these forward-looking statements. Except for any ongoing obligationto disclose material information as required by the United States federalsecurities laws, NXP does not have any intention or obligation to publiclyupdate or revise any forward-looking statements after NXP distributes thisdocument, whether to reflect any future events or circumstances or otherwise.For a discussion of potential risks and uncertainties, please refer to the riskfactors listed in NXP’s SEC filings. Copies of NXP’s SEC filings are availablefrom the SEC website, www.sec.gov.
NXP and the NXP logo are trademarks of NXPB.V. All other product or service names are the property of their respectiveowners. © 2016 NXP B.V.
For more information, please contact:
NXP Global Technology PR | NXP Global Technology PR | | | |
Tate Tran | Jack Taylor | | | |
Tel: +1 408-802-0602 | Tel: +1 512-560-7143 | | | |
Email: tate.tran@nxp.com | Email: j.taylor@nxp.com | | | |
Tags: Automotive, Industrial