Complete solution combines mobile payment and ticketing with GSMA-compliant remote SIM activation for consumers to quickly add mobile subscriptions and cellular networks to their smartphones for better coverage and when traveling abroadSHANGHAI, China, June 26, 2017 (GLOBE NEWSWIRE) -- MWC SHANGHAI -- NXP Semiconductors N.V. (NASDAQ:NXPI) collaborates with Shanghai Unicom, one of the first pilot units in “consumer networking” of China Unicom, and roam2free to develop a secure eSIM solution that makes it easy for consumers to add mobile plans and cellular networks to their smartphone. For the ultimate consumer experience, the solution provides convenient mobile payment and ticketing while bringing a new level of connectivity to smartphones and other mobile devices. Consumers will have convenience to use a mobile application to add and manage multiple mobile subscriptions for better coverage or when traveling abroad to minimize roaming fees.
China Unicom, one of the world’s largest telecom companies, will provide the necessary eSIM Subscription Manager Data Preparation (SM-DP+) infrastructure and commercialization support for the ‘one-stop-shop’ solution. The offering will include NXP’s embedded secure element (eSE) hardware with eSIM features, plus roam2free’s eSIM system integration (Sim2Free), application development and system support. As the backbone to NXP’s mobile subscription solution, Sim2Free seamlessly connects eSE-enabled smartphones and wearables to existing and future SM-DP+ services in China through a streamlined implementation that accelerates time to market for developers. The eSIM offering is also compliant with the GSMA consumer specification (SGP22) to enable fast, seamless deployment and connectivity for OEMs and mobile network operators (MNOs).
“roam2free is an established brand for solutions that enables connected cars and connected devices in China,” said Mark Shi, CEO of roam2free. “This collaboration now addresses the growing demands for enhanced smartphone connectivity by providing a complete eSIM solution to manage connectivity and remove the need of a physical SIM card, which also saves costs across the board.”
This initiative builds on NXP’s leadership in mobile payment and ticketing in China, following a number of NXP’s strategic collaborations to deploy its mobile solutions and eSE that increase consumer engagement and support an increasingly mobile lifestyle. NXP technology supports a rapidly growing number of OEMs, popular manufacturers of smartphones and Chinese public transport operators seeking to integrate secure mobile applications, with its mobile payment solution and eSE being among the first to support Shenzhen’s public transportation e-payment system. The Company’s technology is also used for ticketing at China’s popular metro stations and public bus lines across the country, and NXP has several mobile ticketing and payment deployments in Shenzhen, Guangdong, Guangzhou province, Beijing and other major Chinese cities.
“As a market leader for secure applications using state-of-the-art embedded secure element, NXP’s proven technology and success in China brings a brand new level of convenience and features to consumers and the telecom industry as a whole, while also making the solution easy to integrate for OEMs,” said Mochen Tian, Vice President of Sales and Marketing S&C BU – Greater China, at NXP. “The collaboration with Shanghai Unicom and roam2free is the first of its kind to provide integrated eSIM capabilities that offers both a generational leap in connectivity and accessibility plus delivers a complete solution for popular consumer use cases like payment and ticketing.”
See NXP Technology in Action at Mobile World Congress Shanghai 2017 from June 28-July 1
Visit China Unicom and NXP at Mobile World Congress at the Shanghai New International Expo Centre, China Unicom Booth W4.B20 for more information.
About roam2free
Shanghai Gotell Communication Technology Holdings Co., Ltd ("roam2free"), founded in 2013, is a leading cellular connectivity solution and service provider. Our solution is a full software stack with cloud platform for delivering and managing eSIM (embedded SIM). We work closely with MNOs, IoT device manufacturers and smartphone manufacturers, providing a complete and secure “cloud – network – device” cellular connectivity service and solution. Our major clients are IoT/smartphone and car manufacturers. Find out more at www.roam2free.com.
About China Unicom and Shanghai Unicom
China United Network Communications Group Co., Ltd. ("China Unicom") was established on January 6, 2009 on the basis of the former China Unicom and China Netcom. The company offers a wide array of services, including mobile communications services, domestic and international fixed telephony networks and facilities (including Wireless Local Loops); voice, data, image and multimedia communications and information services, value-added telecom services, IP telephony service, system integration service related to communications and information services as well as other services approved by the government. Shanghai Unicom, one of the first pilot units in "consumer networking" of China Unicom, provides eSIM business operation across the country. Find out more at www.chinaunicom.com.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security & privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 44,000 employees in more than 35 countries and posted revenue of $6.1 billion in 2015. Find out more at www.nxp.com.
NXP and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.
For more information, please contact:AmericasTate TranTel: +1 408 802 0602Email: tate.tran@nxp.comGreater China/AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chang@nxp.comEuropeMartijn van der LindenPhone: +31 6 1091 4896Email: martijn.van.der.linden@nxp.com
![Primary Logo](https://resource.globenewswire.com/Resource/Download/15138703-6ac6-4e52-9366-3215f59f8599?size=1)
NXP Semiconductors Netherlands B.V.