Whereas 61% of the global mobile payment users are from China, China’s
penetration of eLocks is still under 3% (Source:
Mobile Payment Conference 2018; SM Home 2017). This is partly due to a
difficult lock configuration for end users, no
remote key distribution and insufficient security. Nevertheless, smart eLocks
have now been identified as a starter-product of smart homes to build up the
basis of security. Due to China’s rapid growth in housing, a growing
demand for secure and convenient products came up and the requests for digital
door locks have finally taken off.
RocketXS: Increased Security at Complete Ease-of-use
Laurent Dardé presenting NXPs eLock solution ‘RocketXS’ in China
With the recently launched
RocketXS
platform, NXP presents an all-in-one residential eLock solution that addresses
the standards of the Chinese market. Bringing together NXP’s
expertise in NFC, Bluetooth® Low Energy and access
control, RocketXS offers a turn-key solution for residential eLocks. This
solution includes all the necessary components for a swift time to market: A
selection of state-of-the-art material, schematics and production ready
firmware. To help ensure smooth design-in, design-in support is provided by an
experienced design house, eliminating road blocks to mass-production. This
enables manufacturers of mechanical locks to extend their offering to smart
locks with little effort.
Various Use Cases
NXP’s all-in-one eLock solution is ideal for various applications, for example,
granting cleaning personal or guests temporary access without the need of
being present or to provide children with tokens if they are too young to
handle keys.
Benefits at a Glance
The
RocketXS solution allows a quick and reliable unlocking via fingerprint,
Bluetooth® Low Energy and NFC. It also takes convenience and security to
the next level as all NFC cards in a user’s wallet (phone) can be set
as a door key. This means that the real key is hidden and only the user
himself knows which one is right and therefore increases the difficulty of
break-ins and hacking. Support of MIFARE® DESFire® based cards is
built into the firmware, further increasing the security. The 9.6mm x 9.6mm
wide fingerprint sensor enables a faster fingerprint registration as well as a
reliable detection due to a higher resolution. The WeChat mini App allows to
configure the lock via smartphone without installing an app. It helps to
remove the display screen from the lock, brings the purity to the next level
and allows a secure remote key sharing. Furthermore, the RocketXS has more
than two years of battery life thanks to a very low power consumption down to
25 uA, which is half of the sleep power of typical existing solutions.
The Future of the Access Market
With RocketXS, NXP presents an integrated solution allowing companies, small
or large, to bring multi-functional and secure eLocks to market at fast speed.
All in all, RocketXS is an advanced, cost-effective smart lock solution which
we are sure to hear more about in the future!