At no less than five festivity locations – including the Valkhof and Plein ’44
– visitors will be able to pay wirelessly for their food and drink. The special Four-Day pass contains an NXP
MIFARE DESFire chip. By facilitating cashless payment the Four-Day Event follows “the new way to pay”
trend.
NXP has been a partner of the Nijmegen Four-Day Event for many years. After a small-scale pilot last year at the
Valkhof Festival, Cashless Payment will be used on a large scale this year during the Four-Day festivities between
July 18 and 24.
If you have credit left on a Valkhof pass from last year, you can exchange this free of charge at the exchange point
on the Valkhof.
The ‘Vierdaagsefeesten’ was first held in 1970 takes place every summer. The festival coincides with
the Four- Day Marches in Nijmegen, which is the largest multiple day walking event in the world with 45,000
participants. During the Four-Day Marches numerous activities are organized in the town center as part of the
‘Vierdaagsefeesten’, including performances by various artists. The Marches and the
‘Vierdaagsefeesten’ collectively attract over 2.35 million visitors to the city each year, which makes
it the perfect place for NXP to apply its ‘contactless’ chip technology.
New ways of paying
All bars and restaurants involved in the Valkhof Festival, Valkhof Park, Plein 1944, Hennis Latin Stage and café
van Ouds are (partly) going to switch from the traditional tokens that visitors were able to use to pay for their
food and drinks to a chip card enabling ‘cashless’ payments. It is expected that this new way of
paying is really going to take off and that soon visitors to the city center and the festival will be able to pay
for their food and drinks with the same card.
Chips/NFC
The chips that NXP has developed to enable contactless communication are part of the MIFARE-family. The first
generation of chips was launched onto the market around 20 years ago. Nowadays the term MIFARE covers a whole range
of chips: from simple chips without security to very advanced chips with a very high degree of security. The chip
that can be used at the festivity locations to make ‘cashless’ payments is a MIFARE chip (type
DESFire) that uses the NFC technology. This is a very secure chip that was developed at the beginning of this
century and enables visitors to make secure payments. Today the MIFARE DESFire chip is not only used in cards but is
also increasingly being used in Smartphones. Expectations are that consumers will be able to pay using their
Smartphone with DESFire chip in the near future.
Role of the banks
The banks are also making great progress with the introduction and promotion of NFC. There will be a huge noncontact
terminal in the Molenstraat. Visitors of the Four-Day festivities who make a contactless payment in one of the
participating shops will earn a coupon that could win them great prizes, such as a tablet, smart watch or mobile
telephone. To make all this possible, several shops in Nijmegen are having noncontact terminals installed in time
for the Four-Day week. In addition, visitors can use their bank cards to make contactless payments in a number of
cafes and bars on the Faberplein.
NXP
For NXP this is a good example of innovation in practice, in our own city and during the largest walking event in
the Netherlands.