Spotlight on Wireless Connectivity

Seven Wireless Trends That Will Shape 2025

Seven Wireless Trends That Will Shape 2025

Discover how wireless technologies are revolutionizing connectivity and enabling smarter homes in 2025.

Spotlight on We Are NXP


Trending Topics


Recent Articles

FRDM-IMX93 Development Board Launches with On-Board IW612 Wi-Fi 6 Tri-Radio Module

NXP expands its FRDM ecosystem with the launch of the new FRDM-IMX93, the first FRDM board with a built-in Wi-Fi module based on the IW612 Wi-Fi 6 Tri-Radio solution.

Boosting In-Vehicle Connectivity Experience: NXP's AW693 and Smart Link Management

The AW693 chip incorporates advanced Wi-Fi features to create a robust in-vehicle wireless infrastructure.

S32J Ethernet Switches Bring Safe, Secure Networking to NXP CoreRide Platform

NXP has introduced the new S32J family of high-performance Ethernet switches, providing OEMs with more efficient and re-configurable networking choices.

Speed Up Compact Design of Fully Software Configurable Analog Input Modules Using NAFE13388-UIM

The NAFE13388-UIM 8-channel universal input AFE Arduino shield board is designed for the evaluation of the NAFExx388, which is a highly configurable, industrial-grade multichannel analog input analog front-end (AFE).

CES 2025: Brighter Lives Driven by Wireless Connectivity

The RW61x Tri-Radio wireless MCU provides a unique solution for smart HMI with high-performance connectivity and an integrated display driver, bringing rich HMI to a wireless system.

FRDM to Innovate: Expanding the FRDM Ecosystem with i.MX Applications Processors

Learn more about the first FRDM development board to feature an i.MX applications processor.

NXP and geo Showcase Smart Energy Management at CES 2025

NXP and geo are partnering to bring revolutionary, Matter-based smart home energy management to consumers. geo's SeeZero home energy management system will make homes more efficient, reduce their carbon footprint, and come closer to net-zero.

Looking Forward to the Lower Power Future with MCX L Series

MCX L Series Cortex®-M33 MCUs operate at up to 96 MHz with ultra-low-power levels even in harsh industrial conditions.

Seven Wireless Trends That Will Shape 2025

2025 is poised to bring innovations to IoT for smart homes and buildings, driven by advancements in wireless technologies, enhanced connectivity, and the evolution of industry standards.


NXP Smarter World Podcast

NXP Smarter World Podcast

Join us as we dive deep into the issues behind today's connected world and explore our scalable solutions for our digitally-enhanced environment.