Spotlight on Smart Home

Bringing Brighter Lives to CES 2025

Bringing Brighter Lives to CES 2025

Discover breakthrough technologies, shaping smarter, more connected and sustainable autonomous homes.

Spotlight on We Are NXP


Trending Topics


Recent Articles

NXP’s Unified Wi-Fi Driver

The MXM driver is NXP's unified Wi-Fi driver solution supporting Multi-Chip Multi-Interface capability.

MCUXpresso SDK 24.12.00 on GitHub: Advancing Wireless Development

The latest MCUXpresso SDK accelerates wireless development through improved GitHub integration.

 Bringing Brighter Lives to CES 2025

The Consumer Electronics Show (CES) in Las Vegas is always an exciting time for NXP and our partners, since it lets us...

Streamline Linux Development with GoPoint for i.MX Application Processors

Discover GoPoint for Applications Processors, an all-in-one interface that connects developers to application-specific demos for i.MX processors..

FRDM-IMX93 Development Board Launches with On-Board IW612 Wi-Fi 6 Tri-Radio Module

NXP expands its FRDM ecosystem with the launch of the new FRDM-IMX93, the first FRDM board with a built-in Wi-Fi module based on the IW612 Wi-Fi 6 Tri-Radio solution.

Boosting In-Vehicle Connectivity Experience: NXP's AW693 and Smart Link Management

The AW693 chip incorporates advanced Wi-Fi features to create a robust in-vehicle wireless infrastructure.

S32J Ethernet Switches Bring Safe, Secure Networking to NXP CoreRide Platform

NXP has introduced the new S32J family of high-performance Ethernet switches, providing OEMs with more efficient and re-configurable networking choices.

Speed Up Compact Design of Fully Software Configurable Analog Input Modules Using NAFE13388-UIM

The NAFE13388-UIM 8-channel universal input AFE Arduino shield board is designed for the evaluation of the NAFExx388, which is a highly configurable, industrial-grade multichannel analog input analog front-end (AFE).

CES 2025: Brighter Lives Driven by Wireless Connectivity

The RW61x Tri-Radio wireless MCU provides a unique solution for smart HMI with high-performance connectivity and an integrated display driver, bringing rich HMI to a wireless system.


NXP Smarter World Podcast

NXP Smarter World Podcast

Join us as we dive deep into the issues behind today's connected world and explore our scalable solutions for our digitally-enhanced environment.