The Power of Transformation: NXP in Embedded Systems Education
This year was the 15th anniversary of FIT and my task was to lead the Autonomous Vehicle Challenge (AVC).
Jan 28, 2025
Discover breakthrough technologies, shaping smarter, more connected and sustainable autonomous homes.
Nov 27, 2024
This year was the 15th anniversary of FIT and my task was to lead the Autonomous Vehicle Challenge (AVC).
By Eli Hughes
Tags: We Are NXP
Aug 5, 2024
Processing thousands of wafers per week, Chandler Fab boosts the local economy and global availability of the most advanced automotive-grade semiconductors.
Tags: We Are NXP
Nov 20, 2023
NXP and Advantest have collaborated with Arizona State University (ASU) to develop a pioneering engineering curriculum - The EEE 522 Radio Frequency Test.
Tags: We Are NXP
Nov 20, 2024
The mobile robotics industry is advancing rapidly thanks to technological improvements in sensors and electronics.
By Neal Kondel
Nov 7 2024
Join us at the SPS show or electronica in Munich to see our wall of partner evaluation boards, as well as the release of the NXP i.MX 91 processor
Tags: Industrial
Sep 26, 2024
Get an in-depth look at the role of ultra-wideband (UWB) in enhancing location-based services and increasing autonomy in various environments
How to build a complete Matter Ecosystem with NXP's FRDM Wireless MCU development boards.
Feb 5, 2025
The MXM driver is NXP's unified Wi-Fi driver solution supporting Multi-Chip Multi-Interface capability.
The latest MCUXpresso SDK accelerates wireless development through improved GitHub integration.
By Kyle Dando
Jan 28, 2025
The Consumer Electronics Show (CES) in Las Vegas is always an exciting time for NXP and our partners, since it lets us...
By Ron Martino
Tags: Consumer, Home Appliance
Discover GoPoint for Applications Processors, an all-in-one interface that connects developers to application-specific demos for i.MX processors..
Tags: Technologies, Edge Computing
NXP expands its FRDM ecosystem with the launch of the new FRDM-IMX93, the first FRDM board with a built-in Wi-Fi module based on the IW612 Wi-Fi 6 Tri-Radio solution.
By Haley Vu
The AW693 chip incorporates advanced Wi-Fi features to create a robust in-vehicle wireless infrastructure.
By Wei Chang
NXP has introduced the new S32J family of high-performance Ethernet switches, providing OEMs with more efficient and re-configurable networking choices.
Tags: Automotive, Vehicle Networking
Jan 17, 2025
The NAFE13388-UIM 8-channel universal input AFE Arduino shield board is designed for the evaluation of the NAFExx388, which is a highly configurable, industrial-grade multichannel analog input analog front-end (AFE).
Tags: Industrial , Factory Automation
Join us as we dive deep into the issues behind today's connected world and explore our scalable solutions for our digitally-enhanced environment.
Subscribe to receive NXP Smarter World Blog articles and exclusive announcements.
GET THE NEWSLETTER