The Power of Transformation: NXP in Embedded Systems Education
This year was the 15th anniversary of FIT and my task was to lead the Autonomous Vehicle Challenge (AVC).
Nov 22, 2024
Explore how NXP’s i.MX RT crossover MCUs empower the next generation of robotic vacuums with real-time performance, power efficiency, and advanced connectivity.
Nov 27, 2024
This year was the 15th anniversary of FIT and my task was to lead the Autonomous Vehicle Challenge (AVC).
By Eli Hughes
Tags: We Are NXP
Aug 5, 2024
Processing thousands of wafers per week, Chandler Fab boosts the local economy and global availability of the most advanced automotive-grade semiconductors.
Tags: We Are NXP
Nov 20, 2023
NXP and Advantest have collaborated with Arizona State University (ASU) to develop a pioneering engineering curriculum - The EEE 522 Radio Frequency Test.
Tags: We Are NXP
Nov 20, 2024
The mobile robotics industry is advancing rapidly thanks to technological improvements in sensors and electronics.
By Neal Kondel
Nov 7 2024
Join us at the SPS show or electronica in Munich to see our wall of partner evaluation boards, as well as the release of the NXP i.MX 91 processor
Tags: Industrial
Sep 26, 2024
Get an in-depth look at the role of ultra-wideband (UWB) in enhancing location-based services and increasing autonomy in various environments
The AW693 chip incorporates advanced Wi-Fi features to create a robust in-vehicle wireless infrastructure.
By Wei Chang
NXP has introduced the new S32J family of high-performance Ethernet switches, providing OEMs with more efficient and re-configurable networking choices.
Tags: Automotive, Vehicle Networking
Jan 17, 2025
The NAFE13388-UIM 8-channel universal input AFE Arduino shield board is designed for the evaluation of the NAFExx388, which is a highly configurable, industrial-grade multichannel analog input analog front-end (AFE).
Tags: Industrial , Factory Automation
The RW61x Tri-Radio wireless MCU provides a unique solution for smart HMI with high-performance connectivity and an integrated display driver, bringing rich HMI to a wireless system.
Learn more about the first FRDM development board to feature an i.MX applications processor.
NXP and geo are partnering to bring revolutionary, Matter-based smart home energy management to consumers. geo's SeeZero home energy management system will make homes more efficient, reduce their carbon footprint, and come closer to net-zero.
By Charlie Ice
MCX L Series Cortex®-M33 MCUs operate at up to 96 MHz with ultra-low-power levels even in harsh industrial conditions.
By Eli Hughes
Tags: Industrial, Power and Energy
Jan 2, 2025
2025 is poised to bring innovations to IoT for smart homes and buildings, driven by advancements in wireless technologies, enhanced connectivity, and the evolution of industry standards.
By Charlie Ice
The RW61x Tri-Radio wireless MCU provides a unique solution for smart HMI with high-performance connectivity and an integrated display driver, bringing rich HMI to a wireless system.
By Haley Vu
Join us as we dive deep into the issues behind today's connected world and explore our scalable solutions for our digitally-enhanced environment.
Subscribe to receive NXP Smarter World Blog articles and exclusive announcements.
GET THE NEWSLETTER