Every 2 years in November, tens of thousands of people flock to Electronica for an immersive 4
days of groundbreaking electronics. This year was no different – it was an occasion to
share new ideas, and explore how they all connect. For NXP, it was an opportunity to show
what’s possible today with the secure connected car and glimpse into the future of the
completely autonomous vehicle.
Electronica’s ‘connected worlds – safe and secure’ theme is on
target with the industry’s focus. – Kurt Sievers, Head of NXP Automotive, opened electronica Monday evening to a
crowded auditorium in Munich.
Semiconductors are the foundation of all innovation for tomorrow’s connected worlds, from
the tiniest wearables to self-driving cars and smart cities. But, he added, if you only connect
the world and forget about security, it can lead to adverse, even disastrous, consequences.
He shared the recent attack that took down a big chunk of the Internet for most of the U.S.
Eastern seaboard using smart – but unsecured – toasters, surveillance cameras and
other unsecured things.
It was a natural segue into the electronics industry’s focus on security, which was on
the minds of many in the audience.
A live experience of secure connected mobility
The connected car, and ultimately the completely autonomous vehicle, isn’t so far away.
That’s what NXP set out to show on the streets of Munich.
Siemens, Honda, DAF trucks, Cohda Wireless, Marben and Chemtronics joined NXP to show
intelligent traffic management, where cars, trucks, and motorcycles talked to traffic lights, road
works and each other. Called V2X (vehicle-to-everything) communications, vehicles and even ships
and drones, can connect and communicate to the infrastructure and other vehicles based on wireless
communications (IEEE802.11p).
More than a dozen use cases were shown with the vehicle that “sees”
what’s ahead, around corners and over hills, detecting people and other vehicles. It syncs
with traffic signals to zip through green lights. It knows about an approaching ambulance,
pinpointing the location of the siren that would otherwise only be heard. It helps you avoid
accidents, reduces congestion and minimizes emissions. You can watch some of the use cases in this
video:
For more information, read about the connected vehicle experience in this blog,
Speed up autonomous cars.
Platooning system to bring 30 times faster reaction time A new platooning
system, developed in partnership with DAF Trucks, sets out to achieve
30 times faster reaction time
when compared to human-controlled vehicles by 2017.
In platooning, a radar system is an essential element next to V2X. Two or more trucks wirelessly
link to form a platoon to save fuel, increase road safety, and cut down on emissions.
The second truck, the follower, is in a semi-autonomous driving state, safely braking and
accelerating at high speeds in sync with the lead truck. If a car or another object cuts in front
of a truck, the radar detects it. Performance is critical to reliably and quickly detect objects,
allowing the vehicle to safely react.
New radar system detects and processes near-vehicle objects with higher accuracy and
safety The ability of a vehicle to make precise, safety-related decisions depends on its capacity
to accurately detect and classify objects. The new automotive S32 radar microcontroller offers four times the performance of its predecessor to safely detect and process any object in the vicinity of the car.
The higher performance of this MCU means higher accuracy and safety for applications such as
collision avoidance, lane change assist, autonomous emergency braking, radar cocooning with
360° perception or adaptive cruise control. In intelligent transport systems, vulnerable road
users (VRUs) like pedestrians, motorcycles and bicycles can be detected and tracked much faster.
Get faster, more secure V2X development with Cohda Wireless NXP now has full access to Cohda’s optimized algorithms for the rapid development
of V2X
standard enhancements and additional applications. This means that NXP can provide you with
enhanced firmware for the NXP RoadLink™ chipset.
The streamlined software licensing helps you speed up your V2X and Connected Autonomous
Vehicle (CAV) developments to meet the needs of shorter time to market and even more secure
solutions.
Automotive lighting is redefined with groundbreaking digital LED A new
digital LED concept for automotive applications with the first LED product was unveiled by Inova
Semiconductors. This next-generation LED platform was rolled out by the Open ISELED Alliance. The
product,
available from Dominant Opto Technologies in early 2017, is the first developed under the umbrella of ISELED, an open alliance formed to provide a full
ecosystem for the new digital LED right from its very inception. The alliance includes Inova
Semiconductors, Dominant Opto Technologies, NXP, TE Connectivity and Pforzheim University.
NXP engages in the debates NXP CEO Rick Clemmer joined renowned experts
from the semiconductor industry for the CEO Roundtable which focused on security (watch the replay).
“It’s not just about tech, it’s about applications and solutions that make
our lives more connected and safer.” -NXP CEO Rick Clemmer
#ele16pic.twitter.com/zeGxEz2Mqe
At the Automotive Conference, several automotive sessions were led by NXP and partners
and security was a key topic, starting with a panel discussion on the secure
connected (self-driving) car with Lars Reger. Other sessions included multicore SOCs for
automotive with Stefan Singer, Marc Osajda covered MEMS and automotive and Timo van
Roermund led a session on security.
Additionally, Lars Reger and Davide Santo joined a panel discussion on automotive technology
transfer (read about it).
NXP Auto CTO Lars Reger moderates
#ele16
auto tech transfer panel: How do self-flying robots deal with cyber
#security? — NXP Automotive (@NXP_Auto)
November 8, 2016
New auto tech acceptance traditionally moves slow. It needs move fast to compete with
non-traditional players. -NXP’s Davide Santo,
#ele16
— NXP Automotive (@NXP_Auto)
November 8, 2016
The story of the future of intelligent transportation doesn’t stop here. Keep up with
what’s shaping the industry by following NXP Automotive on Twitter
for the latest news and event updates.
VP of Global Marketing and Communications, NXP Semiconductors
Birgit is the VP of Global Marketing and Communications at NXP. Throughout her tenure at NXP, she has witnessed the significant impacts of NXP’s innovations and has driven strategic initiatives to share this with the world. She is a technology enthusiast and is passionate about connecting the dots on the latest breakthroughs and identifying the unique stories behind them.