(Photograph by Frederic Maligne) NXP and Easymile partner on an autonomous
shuttle demonstration featuring NXP’s V2X technology
To mark the 50th anniversary of our Toulouse site, we held round
tables on the theme of the Future of Mobility, one focused on self-driving
mobility: a society revolution, and the other on smart cities. 12 industry
experts from companies such as Renault, Airbus, Continental, EDF, Orange,
Valeo and NXP were split across the two panels, that were hosted by the tech
aficionado Anicet Mbida, journalist for Europe 1. What follows is a recap of
those discussions.
The discussion for the future of mobility centers around changing societal
values rather than the technology that will enable it. The need for more
autonomy is accentuated by the movement to make our roads safer and reduce
fatalities. Using the technology that we already have today to sense our
environment can be re-used to help prevent collisions, or other critical
situations where human drivers cannot react as fast. In fact, Guillaume
Devauchelle, Vice President of the Innovation group and Scientific Development
at Valeo, says that the technology needs to be transparent. Drivers
don’t want or need to know about what technology is there, they just
want to be connected and feel safe on the road. This means that the technology
has to be ultra-reliable.
Kurt Sievers, Executive Vice President and General Manager for Automotive at
NXP, says mobility is being redefined. To help society with this shift,
Sievers says we shouldn’t talk about only cars. Instead, we need to
talk about safe and secure mobility. Through industry collaboration, we can
replace the human driver with technology. It requires an array of different
sensors to achieve the same level of perception, but the upside is that the
technology will be more accurate than human beings – seeing
around corners, through fog or over a hill, for example. Furthermore, our cars
will transform into a learning system with artificial intelligence –
teaching the vehicle to learn from the environment in the same way that a
human driver is able to learn. The final piece to the story is
“actuation,” when the vehicle knows when and how much pressure
to brake, or to turn left or right without a cue from a human driver.
Actuation must be perfected – from the human brain into the physical
electronics world. That is what makes the whole system so powerful, according
to Sievers: being able to bridge back and forth between the real, physical
world and the digital.
The late Mark Rich, Vice President of Connected Fleet in the CTO office
at Airbus, agreed that sensing and processing is important, but interaction is
potentially more so. In the aviation world, there is much more interaction
between the pilot and the vehicle than in the transport vehicle world. So,
communications and the types of communication that exist today are clearly
going to be necessary to enhance this automation capability.
Network capabilities will make the prioritization of services to the
autonomous car a key point according to Julien Masson, head of connected car
at Orange. You want the vehicle to be able to prioritize and notify you of
critical issues, rather than giving bandwidth to infotainment for example. So,
what’s really needed is investment in the infrastructure and also
widescale collaboration to be able to beat cybersecurity threats. Being able
to protect the vehicle to different levels of cybersecurity is one point, but
how it is embedded into the infrastructure is equally as important says
Sievers.
Moving beyond the question of cybersecurity, is the question of
responsibility. Alexandre Corjon, Global Vice President of Electrics,
Electronics and Systems at Renault says that the grey area over who is
responsible is resolved by technology. Technology will make sure that we are
able to protect the driver continuously, that there is no risk of the driver
thinking that the vehicle is in control and taking the right decisions, when
suddenly it can’t do it. As Adrian Traskov, head of chassis and safety
IC solutions at Continental explains, being able to apply the same level of
testing to the autonomous car as traditional car platforms today, is just not
possible. For a vehicle to be released today, it is tested over millions of
miles to get the confidence that the systems function. These systems become
much more complex in the future and will require billions of miles to get the
same level of confidence. So, what will happen is real users will effectively
be the testers. Data will be aggregated from a whole fleet of cars, to be
processed together, to allow a function by function release over the air to
the entire fleet as each function is validated, so enhancing the experience
with each step. So, the whole network needs to be secured – this is a
huge infrastructure problem.
We can learn from the aerospace industry though, since one of the key
crossovers between automotive and aerospace industries is functional safety.
There is a major difference between what is in operation today between the
two, according to Masson. Planes have a much higher level of functional safety
with redundancy levels. In addition, air traffic controllers add a layer of
human operation, which will not exist in the fully autonomous car, since this
will rely on AI. Rich added that the autopilot function does involve a human
aspect, which is learning to let go of the controls. The human element is
really the hinging factor for Sievers; as the industry moves through the
gradual process of automation, we’ll get to a blocking point for most
people around level 3- because although the driver is off action because the
autopilot is activated, the driver still has to pay attention because
something may happen that requires their attention. Sievers believes that
drivers can’t function properly like this, they are either fully on or
fully off. Which is why he suggests this leapfrog movement, to move directly
to a level 5 system to tackle the mogoogre difficult end of the spectrum.
The question of autonomous vehicles and the required enabling infrastructure
has its importance within the smart cities of tomorrow, too. Traffic
congestion, pollution, parking facilities, building development and
transportation of goods and services are concerns shared by city planners. The
timeframe to move towards more connected and secure cities must be aggressive.
Solutions must be standardized. Christophe Fourtet, Founder and
Scientific Director at SigFox questions how do we get the right information
about the right infrastructure. The information that we collect today is not
nearly pertinent enough to build the infrastructure that we will need
tomorrow.
We need to have better connectivity and integration for the infrastructure to
be more developed – as the way that people live their lives is
changing. There are increasing numbers of people who no longer travel to an
office to work – instead opting to work from wherever they are able to
connect, from their home, the coffee shop and even the airport lounge says
Paul Hart, Senior Vice President and General Manager of RF Power at NXP. The
key challenge ahead of us is to be able to provide this level of connectivity
and provide the fast data rates everywhere as needed. This will give us the
ultimate flexibility in how we work, how to coordinate all the different
pieces of the smart city that need to be integrated.
One way that this could function is through collaborative platforms that puts
citizens at the heart of information sharing and overlays data analytics
capabilities to data that is collected by groups of individuals to create a
solution for a different type of usage. There are many examples of these
collaborative navigation applications already in use today, but likely we will
be seeing more and more of these civilian citizen systems, that will mesh
together to create a new smarter city dynamic, according to Stephane
Gervais-Ducouret, General Director at Neavia.
The challenge here, Hart said, is that anyone can look into the future and
dream about what it should be like. What’s really difficult is for us
to look into the future, dream and get it right. Getting it right means
creating an infrastructure that will enable self-, organic development from
both citizens and industries. In the end, innovation of our cars will inspire
amazing features that we haven’t yet conceived. These same innovations
will make our future smart cities secure, usable and interactive.
In late June, these key industry leaders gathered for a VIP event held at
NXP Toulouse to celebrate its 50 year anniversary. Back in 1966, the Mayor
of Toulouse announced the construction of the Toulouse site as one that
would spark huge development in the region and make Toulouse a technology
hub for the future. Fifty years later, the statement rings true: Toulouse is
a hotbed of start-ups and R&D centres for the automotive and aerospace
industries.