Like any emerging technology, the myths around UWB hit the headlines almost as
fast as the facts and sometimes linger on in our memories. We asked several
UWB ecosystem players to weigh in on the misconceptions concerning UWB now and
in the future as the technology becomes more accessible. Let’s demystify four
misunderstandings about UWB.
Myth One: UWB Only Operates at Short Distances
This misperception is both understandable and incorrect. Although UWB is
technically a short-range wireless technology (like Bluetooth, WiFi and NFC),
that’s really more of a category listing.
UWB can operate at frequencies between 6.5GHz and 10GHz compared with
Bluetooth’s fixed 2.4 GHz.
The general rule is indeed that the higher the frequency, the shorter the
range.
However under line-of-sight conditions, UWB’s operating range can stretch to
100 meters—the length of an international soccer pitch. Of course, the real
world range depends on many variables in the end-product design and the
environment it’s planned for. Antenna design, for instance, power levels,
channel frequency, complexity of the propagation environment and the kinds of
materials that the signal may have to pass through all have an influence.
UWB will not perform well in metal environments, but does pass through other
materials such as wood, plaster and even brick, while density of the material
impacts the range. So, although many current applications are using UWB for
its short-range benefits, it can stretch a lot further.
Myth Two: UWB Is Just Another Connectivity Technology
Sure, it started life as a means of high-rate data communication, and it was
up against WiFi, but that was then. UWB has undergone several transformations:
It has evolved from an OFDM-based data communication to an impulse radio
technology specified in IEEE 802.15.4a and the security extension being
specified in IEEE 802.15.4z (at the PHY/MAC level) today make it a unique
secure fine ranging technology.
Having undergone that transformation, today’s UWB has evolved from data
communication into something unique: a secure fine-ranging impulse radio
technology. As such it fits better into the category of sensing technologies
that can pinpoint objects more accurately than any other, down to +/- 10cm,
bringing a new dimension of spatial and contextual awareness to product
technology.
Myth Three: UWB’s ‘Precision’ Benefits Can Be Matched by Bluetooth
Since UWB broke cover and showed its incredibly accurate location sensing
capabilities, Bluetooth LE and WiFi’s positioning capabilities and accuracy
have been promoted and improved. Experiments under lab conditions, including a
very high infrastructure density and clear line of sight, have shown
improvements in the new Bluetooth 5.1 release and the WiFi Alliance has
announced updates on their localization capabilities for the coming release,
too. But the physics doesn’t compare. They still rely on a modulated sine wave
carried over a narrow frequency, whereas UWB has a unique pulse signal (2ns)
operating over 500MHz of frequency.
Bluetooth LE and WiFi use the receiver signal strength indication (RSSI)
technique which are known to be more susceptible to environmental factors,
including obstructions and interference from other radios, resulting in
reduced accuracy. An obstruction can result in severe attenuation of signal
power, leading to errors that can be off by multiple meters.
Bright minds. Bright futures. NXP team members create breakthrough technologies that advance our world.
The future starts here.
UWB in turn is based on time-of-flight measurements. Distance is determined by
the travel time of a pulse packet and multiplied by the speed of light.
According to the FiRa Consortium™ “UWB’s very fast transmission of steep and
narrow pulses makes it possible to mark signal timing with a higher degree of
certainty. The UWB pulse signal maintains its accuracy even as the distance
between the devices increases, and displays excellent resilience in non-Line
of Sight (non-LoS) scenarios.”
Simply put, UWB can do more, more accurately, more reliably and under more
conditions.
Myth Four: UWB Is a Niche Technology
Yes, it’s mainly three big companies, namely Apple, Samsung and BMW, that have
been making news about UWB’s powerful capabilities for mobile access and file
sharing. But the impact of their integration effort to the broader ecosystem
development can’t be underestimated.
When the automotive industry adopts a new technology it’s well embedded, since
decisions in automotive will be generational. The same is true for mobile. To
make the decision to add another RF or antenna to the platform is a big deal
and will not happen unless it’s adding big value for consumers. And once a new
technology makes it to the phone, it becomes a free resource and triggers
adoption to new use cases.
In fact, the FiRa Consortium has already listed
more than 35 use cases, and there will be more. Indoor GPS, credentials sharing, access control,
gesture-based control and VR gaming, presence-based device activation… these
are just the beginning. UWB can be stretched from phone to car to IoT sensors,
devices and objects of all form factors with mobile likely to be the seeding
platform for the broad adoption of UWB.
Click here
or image to see full UWB Infographic.
Send an email to
uwb.solution@nxp.com
if you would like us to tackle another myth about
UWB!