Getting Started with S32N5 Reference Design Board

Last Modified: Sep 7, 2026 new Supports S32N5 Real-Time Central Compute Reference Design Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Get Familiar with the Board
  • 4

    Plug It In
  • 5

    Build and Load

1. Out of the Box

The S32N5 Reference Design Board (RDB) is a robust and comprehensive design featuring the S32N5 vehicle super-integration processor. The S32N5 RDB is designed not only for evaluating the S32N5 processor, but also for complete end-to-end application development. Its wide range of integrated onboard components integrated makes the S32N5 RDB is well suited for a variety of automotive, robotics and transportation applications. For example, it provides a reference platform for central compute applications that support software-defined vehicle (SDVs).

This guide will walk you through the process of setting up your S32N5 RDB and running the included demo. The diagram below lays out the components of the RDB.

GS-S32N5-RDB Block Diagram

GS-S32N5-RDB Block Diagram

1.1 Kit Contents

The RDB contents include:

  • S32N5 RDB with acrylic plate
  • 12 V Power Supply
  • 32 GB SD card
  • Instructions for lid and socket mounting
  • Communication-port cable
  • Multifunction cable
  • 1 Gb Ethernet loopback cable
  • Custom RJ12-RJ12 cable
  • USB to USB-C cable
  • Power cord
  • Universal adapter
  • Cat 6A Ethernet cable
  • 10 jumper headings

1.2 Minimum System Requirements

You will need a Windows PC workstation to evaluate the board. For best results, please ensure your PC is equipped with the following:

  • A serial console application, such as:
  • Windows Hardware Quality Labs (WHQL)-certified FTDI Combined Driver Model (CDM) serial configuration through the FTDI chip: D2XX Drivers - FTDI
  • Install the driver only if Windows does not automatically configure the COM portS32 flash programmer available in the following directory: \S32DS.3.6\S32DS\tools\S32FlashTool\GUI\s32ft.exe

2. Get Software

2.1 Get Software

When working with this RDB, you will need to download software. All available software is available on the Automotive Software Package Manager page. You will need to install the GrayVIP executable, where upon its successful installation, there will be a prebuilt binary image needed to program the board and perform the initial boot of the S32N5 RDB. The image below shows where the GrayVIP for the S32N5 (1.0.26.0 or newer) download is located on the Automotive Software Package Manager.

GS-S32N5-RDB Out of the Box 1.2

Automotive Software Package Manager GrayVIP Selections

3. Get Familiar with the Board

This section outlines the RDB's features and components.

3.1 Board Features

Features of the S32N5 RDB include:

  • Central compute microprocessor (MPU)
  • Power management integrated circuits (PMICS): FS04, PF5300
  • Multiple boot configurations
  • Support for multiple Ethernet protocols
  • Support for multiple communication protocols
  • Support for ASIL D safety

3.2 Board Description

The S32N5 RDB features the S32N5 vehicle super integration processor. Designed to support both the processor and its integrated subsystems, the board provides a comprehensive platform for evaluation and development. Its onboard components (such as ICs), peripherals and external connectivity options allow users to efficiently evaluate device capabilities and accelerate target application development.

3.3 Board Components

The diagram below outlines the components of the S32N5 RDB. A complete and detailed diagram can also be found in the S32N5 RDB User Guide. The components highlighted in the image below are the ones most relevant to this Getting Started guide.

GS-S32N5-RDB Get Software 2.3

4. Plug It In

This section walks you through how to hook up and configure the board.

4.1 Connect Power Supply

Connect the power supply to the 12 V power jack, J43, on S32N5 RDB.

GS-S32N5-RDB Plug It In 3.1

4.2 Connect the USB Cable

Connect the RDB J1 port to the USB port of your Windows PC with a USB Type-C cable.

4.3 Configure the Boot Mode

Set switch S1[1:4] to 0b0000 to boot in serial mode.

4.4 Power on the Board

Turn on the power switch, SW1, on the RDB.

4.5 Program the GrayVIP Prebuilt Image

Follow the steps below to program the GrayVIP prebuilt image (GrayVIP_IVT_GrayVIPApp_Blob.bin) available in the directory <GrayVIP_install_directory>\prebuilt\gcc\binaries in XSPI flash:

  1. Open the S32 Flash Tool and select the following:
    • Target: S32N5X
    • Destination: FLASH
    • Algorithm: S32HS01GT
    • COM port: Third COM port
  2. Select "Test connection…" to verify that the COM port connection is good
  3. Select "Upload target and algorithm to hardware…" to load the flash algorithm
  4. Select "Upload file to device…" to program the image to the XSPI flash (When prompted, select the binary file referenced in step 4.5)

The image below references the configuration steps listed above corresponding to a, b, c and d respectively.

GS-S32N5-RDB Plug It In 3.2

4.6 Power Off the Board

Once the programming is complete, turn off the power switch (SW1) on the S32N5 RDB.

4.7 Configure XSPI Boot Mode

Set switch S1[1:4] to 0b0001 to boot from XSPI flash.

5. Build and Load

This section walks you through how to load and run the GrayVIP software on the S32N5 RDB. Follow the instructions below to run GrayVIP on the RDB.

5.1 Setup the Serial Consoles

  1. Open your preferred serial console (such as Tera Term or MobaXterm), and four COM ports should appear
  2. Open the third COM port and set the baud rate to 230400
  3. Additionally, open the lowest-numbered COM port and set the baud rate to 115200

5.2 Turn on the S32N5 RDB

Using the SW1 power switch, turn on the S32N5 RDB.

5.3 Running GrayVIP

After the XSPI boots, the GrayVIP software is executed. The serial console shows output logs of the GrayVIP software running on the RDB (see examples below).

GS-S32N5-RDB Build and Load 4 GS-S32N5-RDB Build and Load 4.2

Design Resources

Board Information

Information for the RDB can be found in the following documentation: