Getting Started with the PF9453UK-EVK

Last Modified: Dec 2, 2025Supports PF9453 WLCSP Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get to Know the Hardware
  • 3

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the PF9453UK-EVK board.

1.1 Kit Contents and Packing List

The kit contents include:

  • Assembled and tested evaluation board in an antistatic bag
  • Quick Start Guide
  • One PF9453UK-EVK evaluation board for evaluating board functions and features
  • One USB type C cable

1.2 Additional Hardware

In addition to the kit components, the following hardware is recommended when working with this kit:

  • Power supply with a range of 2.7 V to 5.0 V (set the current limit initially to 1.0 A; maximum power consumption at default voltages is up to 18 W)
  • Oscilloscope/multimeter
  • Electronic load (optional) - each power rail output can be connected to e-load for testing

1.3 Minimum System Requirements

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications supports proper operation of this evaluation board:

  • USB-enabled computer with Windows 7, Windows 8, or Windows 10

1.4 Software

Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at PF9453UK-EVK board or from the provided link.

  • Go to PF9453 EVB graphical user interface
  • Extract the Evaluation Kit GUI zip file, PF9453_EVB_GUI_1.25.2.21-x64, into the selected folder. No need to install. (If the password is requested to unzip, type “NXP”)
  • Install the FTDI D2XX direct drivers from ftdchip
  • Run the file PF9453.exe. The interface window is shown in Figure 1

Figure 1. Interface Window

Figure 1. Interface Window

2. Get to Know the Hardware

This evaluation board features the PF9453 PMIC. The kit integrates all hardware needed to fully evaluate the PMIC and a communication bridge based on Future Technology Devices International Ltd. (FTDI) to interface with the PF9453 GUI software interface to configure and control the PMIC.

2.1 Board Features

  • Four Buck regulators:
    • One 2.5 A BUCK regulator
    • One 1.5 A BUCK regulator with DVS
    • Two 1 A BUCK regulators
  • Two Linear regulators:
    • One 10 mA LDO
    • One 250 mA LDO
  • One 400 mA load switch with a built-in active discharge resistor
    • 32.768 kHz Crystal oscillator driver and buffer output
  • System features:
    • 2.7 V to 5.5 V operating input voltage range
    • Power ON/OFF control
    • Standby/run mode control
    • DVS control
    • Interrupt configuration
    • Fm+ 1 MHz I²C Interface (via FTDI USB to I²C cable)

2.2 Board Description

The figure helps to identify the different main sections on the board.

Figure 2. Evaluation Board Featured Component Locations

Figure 2. Evaluation Board Featured Component Locations
  1. PF9453 PMIC (WLCSP package)
  2. USB type C connector
  3. VPWR and GND input power connectors
  4. LDO1, LDO_SNVS, BUCK1 and BUCK2 sensing test points
  5. LDO1, LDO_SNVS, BUCK1 and BUCK2 power test points
  6. Digital signals jumper selectors
  7. ADC Jumpers
  8. BUCK3 and BUCK4 sensing test points, SDA and SCL PMIC, 32 kHz
  9. BUCK3 and BUCK4 power test points
  10. I²C headers and tests points
  11. FTDI (I²C to USB IC)

3. Configure Hardware

3.1 Configure Hardware

Figure 3 shows the default jumper configuration of the board.

Figure 3. Evaluation Board Default Jumper Configuration

Figure 3. Evaluation Board Default Jumper Configuration
Name Default Description
J401 1 to 2 Selects source voltage for VSYS and PSYS (PMIC input voltage): 1 to 2 → PMIC input voltage comes from the USB type C connector 2 to 4 → PMIC input voltage comes from external connector (J400) or test points TP400 and TP402 2 to 3 → PMIC input voltage comes from FRDM_VIN Connector J600-06.
J402 CLOSED Connects the external LDO to VIN voltage.
J403 1 to 3 Selects output voltage of the external LDO U400: 1 to 2 → External LDO output voltage = 1.8 V 2 to 3 → External LDO output voltage = 3.3 V.
J405 2 to 3 Selects PMIC I²C pullup voltage: 1 to 2 → I²C Voltage comes from BUCK4 Out 2 to 3 → I²C Voltage comes from External LDO U400.
J406 2 to 3 Selects PMIC pullup voltage for digital signals: 1 to 2 → VIO Voltage comes from LDO_SNVS 2 to 3 → VIO Voltage comes from External LDO U400.
J407 2 to 3 Selects if SCL_PMIC signal (PMIC I²C signal) passes through the level shifter U401 or not: 1 to 2 → SCL_PMIC signal passes through level shifter U401 2 to 3 → SCL_PMIC signal does not pass through level shifter U401.
J408 2 to 3 Selects if SDA_PMIC signal (PMIC I²C signal) passes through the level shifter U401 or not: 1 to 2 → SDA_PMIC signal passes through level shifter U401 2 to 3 → SDA_PMIC signal does not pass through level shifter U401.
J410 Closed Connects the green LED driver U405 to VIN voltage.
J500 Closed Connects load switch Input to BUCK4 out.
J501 Open Jumper for internal validation only.
J502 Closed Connects POR_B signal to VIO pullup voltage.
J503 Closed Connects IRQ_B signal to VIO pullup voltage.
J504 Closed Connects WDOG_B signal to SW500.
J505 2 to 3 Selects PMIC_STBY_REQ signal voltage level: 1 to 2 → PMIC_STBY_REQ connected to VIO 2 to 3 → PMIC_STBY_REQ connected to GND.
J506 2 to 3 Selects WDOG_B signal voltage level: 1 to 2 → WDOG_B connected to VIO 2 to 3 → WDOG_B connected to GND.
J507 2 to 3 Selects SD_VSEL signal voltage level: 1 to 2 → SD_VSEL connected to VIO 2 to 3 → SD_VSEL connected to GND.
J508 2 to 3 Selects PMIC_ON_REQ signal voltage level: 1 to 2 → PMIC_ON_REQ connected to VIO 2 to 3 → PMIC_ON_REQ connected to GND.
J509 2 to 3 Selects LSW_EN signal voltage level: 1 to 2 → LSW_EN connected to VIO 2 to 3 → LSW_EN connected to GND.
J604 Closed Connects BUCK1_OUT voltage to ADC0 channel.
J605 Closed Connects BUCK2_OUT voltage to ADC1 channel.
J606 Closed Connects BUCK3_OUT voltage to ADC2 channel.
J607 Closed Connects BUCK4_OUT voltage to ADC3 channel.
J608 Closed Connects LDO1_OUT voltage to ADC4 channel.
J609 Closed Connects LDO_SNVS voltage to ADC5 channel.
J610 Closed Connects VIN voltage to ADC6 channel.
Name Signal Description
SJ401 CLOSED Connects VIN to PSYS.
SJ402 CLOSED Connects VIN to VSYS.
R626 1 to 2 Selects SCL signal source: 1 to 2 → SCL signal comes from FTDI IC 2 to 3 → SCL signal comes from FRDM connector J601-10.
R627 1 to 2 Selects SDA signal source: 1 to 2 → SDA signal comes from FTDI IC 2 to 3 → SDA signal comes from FRDM connector J601-09.
R628 1 to 3 Selects PMIC_ON_REQ signal source: 1 to 2 → PMIC_ON_REQ signal comes from FTDI IC 1 to 3 → PMIC_ON_REQ signal comes from FRDM connector J602-01.
R629 1 to 3 Selects PMIC_STBY_REQ signal source: 1 to 2 → PMIC_STBY_REQ signal comes from FTDI IC 1 to 3 → PMIC_STBY_REQ signal comes from FRDM connector J602-02.
R630 1 to 3 Selects WDOG_B signal source: 1 to 2 → WDOG_B signal comes from FTDI IC 1 to 3 → WDOG_B signal comes from FRDM connector J602-03.
R632 1 to 3 Selects LSW_EN signal source: 1 to 2 → LSW_EN signal comes from FTDI IC 1 to 3 → LSW_EN signal comes from FRDM connector J602-05.
R633 1 to 3 Selects SD_VSEL signal source: 1 to 2 → SD_VSEL signal comes from FTDI IC 1 to 3 → SD_VSEL signal comes from FRDM connector J606-06.
R634 1 to 3 Selects IRQ_B signal source: 1 to 2 → IRQ_B signal comes from FTDI IC 1 to 3 → IRQ_B signal comes from FRDM connector J606-07.
R635 1 to 3 Selects POR_B signal source: 1 to 2 → POR_B signal comes from FTDI IC 1 to 3 → POR_B signal comes from FRDM connector J606-08.
R636 1 to 3 Selects ADC supply voltage source: 1 to 2 → ADC voltage comes from FTDI_3.3V 1 to 3 → ADC voltage comes from FRDM_3.3V connector J600-05.

Figure 4. PF9453 EVB Test Set Up

Figure 4. PF9453 EVB Test Set Up

See Figure 4 and follow the steps to test the PF9453UK-EVK board. Ensure that all jumpers are in their default positions before starting (see Figure 3).

  1. Connect the positive terminal of the multimeter to TP22 BUCK2_S test point and the negative terminal of the multimeter to TP34 GND test point, see Figure 4 where step 1 is represented with the circle with number 1
  2. Connect the USB -Type C to the PF9453 WLCSP-EVK. See that the green LED D401 is ON, see Figure 4 circle with number 2. Use the USB Type-C connector as the power supply with this configuration. Avoid connecting loads that may exceed its power capacity. For tests requiring higher current—such as efficiency measurements—use an external power supply. See Table 3 for setup instructions. If the USB Type-C supply is sufficient, proceed to the next step
  3. Move the J508 to position J508 (1 to 2), see Figure 4, circle with number 3 (this turns on the PMIC by setting the high state the PMIC_ON_REQ pin)
  4. Measure the default voltage of BUCK2 with the multimeter, it must be 0.85 V (default voltage)
  5. The default power configuration can be checked without doing any hardware (HW) or software (SW) modifications. Check the default voltage configuration using a multimeter on BUCK1, BUCK2, BUCK3, BUCK4, LDO1 and LDO SNVS test points
Regulator PF9453
BUCK1 1.1 V
BUCK2 0.85 V
BUCK3 1.8 V
BUCK4 3.3 V
LDO1 0.8 V
LDO SNVS 1.8 V

Design Resources

Additional References

In addition to our PF9453 Product description page, you may also want to visit: