Secure Automotive Network Design Guide

Last Modified: Jun 19, 2023Supports S32K324 Triple PMSM Control Reference Design Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Software
  • 3

    Plug It In

1. Out of the Box

1.1 Get to Know the MCTPTX1AK324 Reference Design Board

MCTPTX1AK324-GS-CALLOUTS MCTPTX1AK324_connectors

1.2 Block Diagram Features

MCTPTX1AK324 Reference Design Board

2. Get Software

You can watch the video or follow the below step-by-step guide to set up your MCTPTX1AK324 Evaluation Board:

2.1 Download the Development Kit - Application Software

The software package includes projects for most typical hardware configurations.

Download EVB Software

2.2 Get the Integrated Development Environment (IDE)

Download and install S32 Design Studio IDE for S32 Platform

Download S32 DESIGN STUDIO IDE

2.3 Get the Development Packages

All development packages are available from S32K3 Standard Software Package.

Download and install the latest version of S32K3xx Development Package.

Download and install the latest version of S32K3xx Development Package

Download and install S32K3xx Real-Time Drivers Version 2.0.0 package.

Download and install S32K3xx Real Time Drivers Version 2.0.0 package

Download and install IPCF package to support S32K324 dual-core communication.

Download and install IPCF package to support S32K324 dual-core communication

2.4 Get Automotive Math and Motor Control Library (AMMCLib)

We strongly recommend the latest version of the Automotive Math and Motor Control Library (AMMCLib)

DOWNLOAD AMMCLIB

2.5 Get the Run-Time Debugging Tool

MCTPTX1AK324 performs better when using the FreeMASTER Run-Time Debugging Tool.

Download FreeMASTER tool

The FreeMASTER communication driver for S32K3 microcontrollers is also needed. Download it from the Automotive SW - S32K3 - S32 FreeMASTER link in the S32K3 Standard Software Package.

Open S32DS Extensions and Updates dialog (menu -> Help -> S32DS Extensions and Updates), click on Add Update Sites link and navigate to FreeMASTER communication driver for S32K3 (zip file starting with "com.") on your disk.

Get Started with the MCSPTE1AK344

Install FreeMASTER communication driver for S32K3.

Get Started with the MCSPTE1AK344

3. Plug It In

3.1 Check the Default Jumper Positions In the MCTPTX1AK324 Evaluation Board

MCTPTX1AK324-JUMPERS1

Default Jumper settings
Jumper State Notes
J1 CLOSED 5 V for UART to USB
J8 CLOSED 5 V for CAN PHY
J9 CLOSED Enable FS26 debug mode
J10 CLOSED FS26 VCore 1.5 V for MCU VCore
J11 CLOSED FS26 LDO2 5.0 V for 5.0 V devices
J12 CLOSED MCU VDD_HV_A supply input
J13 CLOSED Enable FS26 debug mode
J19 CLOSED FS26 LDO1 5.0 V for 5 V devices
J21 CLOSED MCU VDD_HV_B supply input
J31 OPEN FS26 wake inputs

3.2 GD3000 Overcurrent Compare Setting

Make sure the potentiometer for overcurrent comparator is set in position (slightly to the left from the middle) for approximately 8 – 10 A.

3.3 Connect the Motor

Connect three permanent magnet motors in J34, J35, and J36 connectors. DC motor connected in J39. And if you are controlling valves, connect them in J33.

3.4 Plug in the Power Supply

Attach the 12 V power cable for powering your MCTPTX1AK324 development board, the LED D2, D3, and D6 would turn on green.

3.5 Plug In the Debugger

Attach your Arm-Cortex compatible JTAG/SWD debugger to the connector J22 or J23.

3.6 Plug In the Serial Interface

Attach J24 USB to serial interface for FreeMASTER communication. Please plug it in if you want to control and monitor motors though FreeMASTER.

3.7 Plug In the CAN Interface

Connector J37 is for CAN communication. Please plug it in if you want to control and monitor motors through CAN bus.

Run the MCTPTX1AK324 Reference Design Board

Import the Demo Project Using Your IDE

Import the installed application software project into the S32 Design Studio.

GS_S32K324_SW

Load Code Into the S32K324 MCU

In the S32 Design Studio menu click Run > Debug Configuration and select the predefined debug configuration and click on Debug to start loading built code into MCU.

GS_S32K324_SW

Let the Code Run on the MCU

After the code was loaded into MCU, the S32DS will switch into debug perspective where you may let the code run by clicking on Resume (or press F8) and use Disconnect to avoid interference between the S32DS IDE debugger and the FreeMASTER tool.

GS_MCTPTX1AK324_SW

Run the Motors

There are 3 ways to run the motors, FreeMASTER over UART, CAN and button SW3.

GS_MCTPTX1AK324_SW

Approach 1. Run the Motors With FreeMASTER

Open S32K_PMSM_Sensorless.pmpx file from MCTPTX1AK324_Triple_PMSM_RDB_M7_0 \FreeMASTER_control folder.

GS_S32K324_SW

Click the green GO! button in the FreeMASTER toolbar (or press <CTRL> + <G>) to enable the communication

Successful communication is signalized in the status bar at very bottom as:

RS232 UART Communication;COMn; speed = 115200

GS_S32K324_SW

In FreeMASTER, go to Control page tab, set required motor rpms and turn on the motor drive.

GS_S32K324_SW

Approach 2. Run the Motors With CAN bus

Use a CAN Interface to connect the board.

GS_MCTPTX1AK324_SW

Transmit a CAN standard frame using 0x01 ID to start motors. And the motors state will be feedbacked by ID 0x02 and 0x03 frames.

GS_MCTPTX1AK324_SW

CAN frame definition table.

GS_MCTPTX1AK324_SW