NXP Semiconductors today announced its lead partnership for the Arm® Ethos™-U55 microNPU (Neural Processing Unit), a machine learning (ML) processor targeted at resource-constrained industrial and Internet-of-Things (IoT) edge devices. As an industry-leading innovator of microcontrollers (MCUs), NXP intends to implement the Ethos-U55 in its Arm Cortex®-M based microcontrollers (MCUs), crossover MCUs and real-time sub-systems in applications processors.
The expansion builds on the company's growing ML offerings, including the recently announced i.MX 8M Plus applications processors with dedicated NPU.
The highly configurable Ethos-U55 works in concert with the Cortex-M core to achieve a small footprint while also delivering greater than 30x improvement in inference performance compared to Cortex-M alone, even in high performing MCUs. The Ethos-U55 is specifically designed to accelerate ML inference in area-constrained embedded and IoT devices. Its advanced compression techniques save power and reduce ML model sizes significantly to enable execution of neural networks that previously only ran on larger systems.
In addition, a unified toolchain with Cortex-M gives developers a simplified, seamless path to develop ML applications within the familiar Cortex-M development environment. The end-to-end enablement, from training to run-time inference deployment for Ethos-U55, will be accessible through NXP's eIQ® machine learning development environment.
NXP's comprehensive portfolio of ML compute elements (CPU, GPU, DSP and NPU) are enabled with its eIQ machine learning development environment, which provides choices of popular open-source inference engines that deliver the performance needed for the specific compute element. Using NXP's edge processors and eIQ tools, customers can easily build many ML applications, including, object detection, face and gesture recognition, natural language processing, and predictive maintenance.
NXP and the NXP logo are trademarks of NXP B.V. All other products or service names are the property of their respective owners. Arm and Cortex are trademarks or registered trademarks of Arm Ltd or its subsidiaries in the EU and/or elsewhere. All rights reserved. © 2020 NXP B.V.