EINDHOVEN,
The LPC18Sxx and LPC43Sxx microcontroller families are well suited for any 'connected' application, particularly hubs or gateways, tasked with relaying and/or bridging large volumes of high-speed data. These functions are common in products such as smart meter communications hubs, factory, building, and home automation devices, streaming audio products, automotive aftermarket and many more.
"The tremendous growth in 'connected things' has begun and will accelerate exponentially in the coming years," said
"The Internet of Things (IoT) must be built from the ground up with security in mind," said
A spectrum of solutions for secure connectivity
Both LPC18Sxx and LPC43Sxx families integrate an
The LPC43Sxx and LPC18Sxx microcontroller families anchor a spectrum of secure connectivity solutions from NXP. Both families are supported by software solutions from ecosystem partners for secure firmware updates, secure IoT connectivity, and secure networking stacks (SSL, TLS). In addition these new MCUs can be seamlessly paired with an NXP A-Series secure element for a turnkey solution to add tamper detection, secure authentication with hardware-accelerated PKI (RSA and ECC keys), secure certificate storage and more.
Like all LPC microcontrollers, the new LPC43Sxx and LPC18Sxx microcontroller families are fully supported by the LPC developers' ecosystem. This provides an extensive collection of tools, drivers and middleware, as well as popular forums in constant use by a highly engaged community of embedded developers. To enable developers to bring secure, connected products to market quickly, LPCXpresso evaluation boards are available for both families. Each includes an LPC MCU and NXP A7001CM secure element as well as numerous connectivity and development/debugging interfaces. Together with the LPCXpresso IDE or third-party tool-chain support, plus free LPCOpen drivers and example code, these boards provide a complete low-cost evaluation/development platform.
An LPC43S37-based development platform, available in Q2, will help designers implement a range of secure connectivity solutions for IoT, Industry 4.0, consumer and other applications. The platform combines the MCU, security software from ecosystem partners, an NXP A-Series secure element and supports connectivity features including Ethernet and WiFi.
Availability and demonstration
Parts in both MCU families will be available in multiple sizes of LQFP and BGA packages.
They are available now with pricing starting at USD
The LPC18Sxx and LPC43Sxx microcontroller families will be demonstrated in the NXP booth #5-378, in hall 5 at embedded world 2015 in Nuremberg,
Additional product information is available online:
About
Forward-looking Statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT: For further press information, please contact:NXP Semiconductors Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com