SAN JOSE, Calif.,
| |||||
A photo accompanying this release is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/bed4dc33-7740-4b9a-85c3-101f2223d468
Automakers face significant hurdles in the quest to bring self-driving applications to market efficiently. Solutions to problems — such as how to route multiple streams of automotive sensors data quickly and reliably, how to tackle complex software development in-house and how to create differentiation — are in high demand. These challenges were top-of-mind when long-time partners EB and NXP developed the combined hardware-software solution, which delivers unique benefits to carmakers.
About EB robinos
• EB robinos is the first comprehensive, hardware-agnostic software framework that enables carmakers and automotive suppliers to develop and bring to market increasingly automated driving features and manage the complexity of advanced in-car systems. It features:
About NXP BlueBox Automated Drive Development Platform
• NXP BlueBox
Quotes:
“Developing automated vehicle functions is very challenging for many reasons. One of the most challenging tasks for automated vehicle development is interfacing software components with your target platform. The availability of EB robinos for NXP’s BlueBox means that applications can be run on the hardware via the EB robinos open interface specification. This saves time and enables a proper buildup of functionality,” said Phil Magney, founder and principal advisor at
“Automakers working at the forefront of autonomous development are faced with increased complexity, greater competition and very challenging timelines,” said Martin Schleicher, executive vice president strategy and partnerships at EB. “Together, NXP and EB are providing automakers with a powerful, competitive advantage, allowing them to dramatically accelerate the development of highly automated driving features, with a critical emphasis on the highest levels of functional safety.”
“NXP’s safe compute engine, BlueBox, and EB robinos software framework are a perfect match,” said Davide Santo, Autonomous Platform Architect, NXP Automotive. “They combine two very powerful building blocks for enabling self-driving robots on wheels. This engagement is part of NXP’s strategy to deliver open platform support. We are very pleased to see this solution now being deployed, and look forward to distributing EB robinos in the near future as part of our NXP BlueBox.”
About NXP Semiconductors
About Elektrobit (EB)
Elektrobit (EB) is an award-winning and visionary global supplier of embedded and connected software solutions and services for the automotive industry. A leader in automotive software with over 25 years serving the industry, EB‘s software powers over 80 million vehicles and offers flexible, innovative solutions for connected car infrastructure, human machine interface (HMI) technologies, navigation, driver assistance, electronic control units (ECUs), and software engineering services. EB is a wholly owned subsidiary of Continental. For more information, visit us at www.elektrobit.com.
For more information, please contact: Europe / U.S.Jason DealTel: +44 771522841Email: jason.deal@nxp.comGreater China / AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chang@nxp.comElektrobitManuela PapadopolTel: +1 425 686 3100Email: Manuela.Papadopol@elektrobit.com
Tags: Automotive