NXP Supplies RoadLINK Chipsets for Secure Vehicle-To-X (V2X) Communications In Korea’s Next-Generation Intelligent Transportation System (C-ITS) ProjectSEOUL, South Korea, July 20, 2016 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI) and eSSys today announced that they will be technology partners in Korea’s next-generation Cooperative Intelligent Transportation System (C-ITS) project promoted by the Korean Ministry of Land, Infrastructure and Transport. NXP will supply eSSys with its RoadLINK V2X chipset, a vehicle-to-vehicle and vehicle-to-infrastructure (V2X) communication and security solution which will be test-operated on an 87.8 km route between Sejong City (city of government offices) and Daejon. The year-long pilot operation begins July 2016.
Currently, a variety of smart transport technologies are being installed on national highways, including the primary highway for access to the 2018 Winter Olympic Games in Pyeongchang. The fundamental differentiator that the newly adopted C-ITS with NXP will offer is secure information exchange in real time between vehicles (Vehicle-to-Vehicle, V2V) and between cars and the surrounding intelligent infrastructure (Vehicle-to-Infrastructure, V2I) including roadworks, traffic signs or traffic lights.
Rapid response times combined with the ability of V2X-capable cars to see around corners or through obstacles beyond the driver’s line of sight will prevent accidents, while significantly improving traffic flow and reducing CO2 emissions. According to the Korea National Police Agency, more than 5,000 people die in accidents each year, and more than 300,000 people incur injuries. Congestion currently costs 25 billion euros per year. The Korea Transport Institute estimates that 76 percent of all road accidents could be avoided with the full deployment of its C-ITS plans.
“As a Korea-based vehicle electronics systems provider, eSSys supplies communications modules to automobile manufacturers and tier one suppliers combining high efficiency and optimum performance,” said Yong-beom Kim, CEO of eSSys. “eSSys’ WAVE communications systems based on NXP’s proven RoadLINK V2X chipset are expected to play a key role in the national C-ITS project.”
NXP’s RoadLINK V2X communication and security technology is essential for the continued development and advancement of self-driving cars and macro-traffic management. It enables vehicles to wirelessly exchange information such as speed, position and direction with other automobiles in their vicinity, and allows vehicles and infrastructure to communicate traffic management data or notices such as localized speed limits, traffic signaling and road works warnings, hazardous conditions and more. RoadLINK’s secure element is an integral part of the chipset that protects the privacy of the driver and prevents hacking or manipulation.
“It is an honor that our proven RoadLINK V2X chipset was selected for the next-generation intelligent transport system by the Ministry of Land, Infrastructure and Transportation,” said Lars Reger, Chief Technology Officer (CTO) for NXP’s Automotive business unit. “Our advanced intelligent transport technologies will significantly contribute to saving lives on Korean roads, improving traffic flow and boosting the overall convenience of transport. Based on software-defined radio technology, our hardware platform is able to support the Korean V2X standard, as well as the vast majority of regional variants around the globe.”
The strength of NXP’s RoadLINK technology has been proven in more than one million test kilometers in various projects worldwide. In this year’s prestigious Smart City Challenge, NXP partnered with the U.S. Department of Transportation to provide intelligent transport technologies to the city of Columbus, Ohio, the selected winner in the national contest. In the European Truck Platooning Challenge in April of this year, NXP successfully demonstrated autonomous driving on public roads in a Europe-wide initiative by the Dutch Ministry of Infrastructure and the Environment. NXP V2X and radar technology was used in DAF trucks, as well as in four of the six truck OEM platoons. NXP RoadLINK technology will also be implemented in select production vehicles in the U.S. next year.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security and privacy, and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 44,000 employees in more than 35 countries and posted revenue of $6.1 billion in 2015. Find out more at www.nxp.com.
About eSSys
Specialized in automotive electronics systems, eSSys is devoted to developing, manufacturing major car electronic parts including Telematics, AVN, ETCS, Bluetooth, Wi-Fi and Next Generation WAVE (V2X), providing our customers with affordable communication modules that achieve optimum performance. As a pioneer in communication technology localization for automotive electronics including DSRC chips and many others, eSSys takes a step forward to focus on developing competitive new products, builds the next generation ITS (Intelligent Transport System) including WAVE, leads the high speed wireless communication technology like Wi-Fi, penetrates in and develops multimedia field including AVN/Multi Box, and continues investment to become a dedicated developer and manufacturer in the field of advanced Telematics designed to support driving safety and emergency rescue. Find out more at www.essys.co.kr.
For more information, please contact:AmericasJack TaylorTel: +1 512 560-7143Email: jack.taylor@nxp.comGreater China/AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chan@nxp.comEuropeMartijn van der LindenPhone: +31 6 1091 4896Email: martijn.van.der.linden@nxp.com

NXP Semiconductors Netherlands B.V.