EINDHOVEN,
As the market leader in MCUs and IoT processing, NXP introduced 25 product families to its successful line of S08 8-bit high performance MCUs over the past 12 years, with the S08QG, S08QD, S08SF, S08SH, S08AC, and S08FL MCU families being among the most popular. Together with the extension of these popular 8-bit MCU families and the S08 products to follow in 2017, NXP provides engineers the foundation to expand on today’s applications for the Internet of Tomorrow.
“The S08 microcontroller is NXP’s most successful 8-bit MCU, garnering wide adoption over the last decade. And as a trusted supplier, we understand that our ongoing investment and commitment to the longevity of key S08 products is critical, which is why we are extending longevity program of the six most popular S08 MCU products,” said Emmanuel Sambuis, vice president and general manager of the microcontroller product line at NXP.
“The S08 MCU portfolio contributes to NXP’s unique scale of microcontroller and microprocessor products – allowing us to deliver innovative products, from low cost 8-bit S08 MCUs to ultra-low power ARM® Cortex®-M-based MCUs, and high-performance Cortex-A microprocessors,” said
NXP’s 8-bit portfolio offers the reliability and robustness needed to withstand harsh working environments, making the S08 MCU portfolio ideal for automotive, industrial control and home appliance applications. Complete with both 3V and 5V options, the S08 MCU portfolio also comes packed with a rich set of features offering high performance paired with low power consumption.
Inspired by the passion to make the devices we interact with every day smarter, NXP drives to deliver a product to solution challenges faced by engineers, while also helping them adapt to future needs. With the more than 60 combinations of devices included as part of this product longevity extension*, NXP looks forward to what the future holds with respect to 8-bit powered devices.
For more information about NXP’s S08 8-bit portfolio, please visit: http://www.nxp.com/products/microcontrollers-and-processors/more-processors/8-16-bit-mcus/8-bit-s08:HCS08 and for additional details on longevity, visit: http://www.nxp.com/about/technology-leadership/product-longevity:PRDCT_LONGEVITY_HM.
* Please note, as a result of the move by many to much smaller form factors (like TSSOP, QFN, etc.) PDIP packages of the above six S08 products are not included in this longevity extension program.
About NXP
NXP and the NXP logo are trademarks of
For more information, please contact:
| Americas | Europe | Greater China / Asia | |||||||||||||||||||||||
| Tate Tran | Martijn van der Linden | Esther Chang | |||||||||||||||||||||||
| Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +886 2 8170 9990 | |||||||||||||||||||||||
| Email: tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: esther.chang@nxp.com |
Tags: Automotive, Industrial