News Highlights
The i.MX RT106F leverages the power of NXP’s OASIS face processing engine to provide a breakthrough in price and performance, using a neural network to perform face detection, recognition and anti-spoofing, without the need for cloud connectivity. OEMs now have the ability to take advantage of NXP’s proven hardware and software-based platform to offer advanced human machine interface (HMI) capabilities that can anticipate and personalize the end user’s experience with smart edge devices such as smart appliances, thermostats, lighting, alarms and power tools.
“Think about a toy that recognizes each member of the family and responds appropriately depending on their facial expressions or a smart appliance that can intuitively adjust its settings to a user’s preferences based on previous interaction,” said
The MCU-based face recognition solution bundles everything required to implement accurate, low latency face and expression recognition using an ultra-small form factor that fits into existing applications. The self-contained platform includes production ready pre-certified hardware and software tools, and NXP’s fully integrated OASIS face processing engine for face and expression recognition with camera and display drivers. In addition to creating the easiest path to adding these capabilities to MCU-based devices, the all-inclusive offering clears away any need for specialized expertise, supply chains or logistics.
With total system costs less than half that of microprocessor-based alternatives, the new offering has already been embraced by OEMs who are excited about the possibilities of delivering more advanced and unique user experiences.
NXP is now engaging with OEMs to provide early access to the evaluation and development kit for this solution, and broad market availability is expected to begin in Q1 2020.
See the MCU-based face recognition solution in action at IFA Berlin 2019
NXP is demonstrating the new solution during IFA in
About
NXP and the NXP logo are trademarks of
For more information, please contact:
Americas | Europe | Greater China / Asia | |||
Tate Tran | Martijn van der Linden | Ming Yue | |||
Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +86 21 2205 2690 | |||
Email: tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: ming.yue@nxp.com |
Source: NXP USA, Inc.