EINDHOVEN,
The solution features the ability to connect with 250 nodes allowing for it to be deployed in a wide range of uses in homes and industrial environments. ZigBee 3.0 and Thread ready, JN5169 also features a new toolchain for software development allows up to 15% code size reductions and features extensive debugging capabilities. Intuitive one-touch commissioning using NFC connectivity ensures that the devices can be easily yet securely paired without sending network details 'over-the-air', thus strongly reducing the threat of hacking.
To support JN5169, NXP is launching three new design references for white, tunable white and RGB(W) color lamps, which reduce the total build cost of smart lighting solutions up to 25%. With 512kB embedded flash memory, there is enough memory available on the product to enable Over-The-Air software upgrades, meaning that expensive external flash memory is no longer required, leading to additional cost savings. The lamp reference designs are complemented by wireless switches, remotes, wall panels, sensors, smart plugs and gateways as well as control by cloud services from NXP and its eco-system partners.
"Home automation is one of the leading sectors of the IoT market. As these devices come ever more prominently into the mainstream, our customers need lower cost, easier to use, more robust and more secure solutions," said
"What we have announced in response to this, is an all-encompassing solution for the smart lighting and home automation market, which will outstrip other competitors in convenience, reliability and cost. JN5169 demonstrates that we are not only at the forefront of the smart lighting and home automation industry, but also the leading innovators."
Other key features of JN5169 include:
The new JN5169 product is already being adopted by leading players in the smart lighting market, including
''NXP is our long term valued partner for connected lighting products. With NXP's new JN5169 wireless microcontroller based reference designs, TCP will be able to improve both the performance and ease of use of our connected lighting products and thus maintain our leadership in the US connected lighting market."
"Leedarson has been developing smart bulbs starting from NXP reference designs since 2011. The unique features of the new NXP JN5169 ZigBee chip allow Leedarson to improve range and efficiency and lower standby power consumption of our smart lighting product portfolio and thus to offer a more attractive and green solution to our customers.''
About
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT:NXP Semiconductors Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com