Delivering unmatched performance and quality, the new UCODE 8 is a universal RAIN RFID chip designed to ensure high inventory accuracy on all retail product categories through best-in-class read sensitivity. The new auto adjust feature ensures a consistently high performance read-rate across different product materials and global deployments. Additionally the unique brand identifier feature validates product authentication and helps identify fakes to combat grey market activities. The solution is particularly well-suited for retailers, brand owners, label manufacturers, system solution companies and others seeking to use top-notch RAIN RFID technology for supply chain management and brand protection.
“In the retail industry, there is an ever-increasing demand for optimized inventory visibility and improved process efficiencies to support their omnichannel strategies and create a better shopping experience for consumers, ensuring that they have the right product available at all times via all channels,” said Ralf Kodritsch, director segment manager of RFID Solutions at NXP. “UCODE 8 provides unparalleled performance, addressing exactly those dynamic needs of the retail market, where accuracy, speed and brand protection are crucial throughout all retail processes — from manufacturing and distribution to in-store inventory and the final customer sale.”
Saving Cost with the Innovative Auto Adjustment Feature
The RAIN RFID Chip platform features auto adjustment to deliver consistent readability when used on different materials across different frequency ranges. The feature lowers cost by reducing the need for dedicated regional antenna designs. The automated error correction for memory data also improves data accuracy and ensures that memory data content will remain unchanged over the entire product lifecycle. Its dual-axis glue spacer design and large area gold contact pads can reduce failure rates caused by mechanical stress at the antenna contacts and thereby eliminate performance degradation.
“The RFID inlay is the only element that touches every read point throughout the global supply chain. Our vision is to create inlay products that help the industry unlock new use cases while delivering consistent global performance across each read point,” said
“UCODE 8 pushes the envelope by creating a chipset that is optimized across many other use cases such as functions on conveyor systems in dense packages, handhelds on loading docks, overhead systems in warehouses or on retail floors, exit portals for loss prevention, or close-range readers for point-of-sale or parts verification,” said
For more information about UCODE 8, click here.
See NXP Technologies in Action at RFID Journal Live! from
Visit NXP during RFID Journal Live! at Booth 804. See the UCODE family of products in action and interact with other innovative demonstrations.
About
NXP and the NXP logo are trademarks of
For more information, please contact:
Americas | Europe | Greater China / Asia | |||
Tate Tran | Martijn van der Linden | Esther Chang | |||
Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +886 2 8170 9990 | |||
Email:tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: esther.chang@nxp.com |