EINDHOVEN, The Netherlands,
Photos accompanying this announcement are available at
http://www.globenewswire.com/NewsRoom/AttachmentNg/e9abcfff-cfaf-4349-a065-21a3d953c65c
http://www.globenewswire.com/NewsRoom/AttachmentNg/147b5abc-5695-4ebf-9585-a745cb1c386b
Bringing the NXP i.MX 6UL processor’s cost effective, feature-rich functionality to a broader group of developers, makers and OEMs can help expedite the rapid development of affordable, connected, Android-based IoT devices.
Analyst forecasts predict that by 2019, 70 percent of the connected smart home will be dominated by connected systems. This combination of NXP hardware and Android software will enable companies to develop connected devices without having to build from kernel to applications, significantly lowering the barriers of entry to the IoT market.
“For the past year, NXP has been an early hardware partner for Google’s IoT platform now called Android Things. We are now the only partner on the market to offer low cost certified, system on modules,” said Robert Thompson, i.MX ecosystem manager at NXP. “We believe that successful implementation of IoT depends on the whole ecosystem working together so we’re excited to be part of this Android Things launch.”
Android Things compatible boards can bring greater benefit to developers in various ways including Google-certified firmware that can run on devices to perform bug fixes, provide automatic updates, ease integration into the Android framework, and allow access for developers to deploy and test their code.
“Developers can take their products, and embed these Android IoT boards into them,” said Martyn Humphries, VP of consumer and industrial applications processors at NXP. “By building on the Android framework, makers and device manufacturers can focus on the details of their product, and leave the low level implementation details and security updates up to Google.”
i.MX Powered Boards
Powered by the i.MX 6UL processor, the PICO-iMX 6UL board from TechNexion and the Argon i.MX 6UL board from VVDN Technologies ease and advance features for developers. The boards display the ‘Android Things’ approved logo and are available today. In addition, the Murata IoT Development Platform from
For more information, please visit https://developer.android.com/things/index.html and www.nxp.com/AndroidThings.
About NXP Semiconductors
NXP and the NXP logo are trademarks of
For more information, please contact:AmericasTate TranTel: +1 408-802-0602Email: tate.tran@nxp.comEuropeMartijn van der LindenTel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China / AsiaEsther ChangTel: +886 2 8170 9990Email: esther.chang@nxp.com
Tags: Consumer, Industrial