EINDHOVEN,
“For the IoT to scale, developers must have solutions that enable them to efficiently develop and deploy connected products,” said
“These awards further validate how the Hexiwear IoT and Wearables Development Platform enables developers to quickly and easily bring IoT and wearable products to life. At NXP, we are changing the way new product development is done for IoT applications,” said
“Hexiwear enables designers and engineers to quickly move from idea to prototyping to volume production. Being selected to receive the ECN IMPACT Award in the rapid prototyping category as well as being a triple award winner at the ARM TechCon Innovation Challenge is a tremendous honor,” said Dr.
Hexiwear is a complete open-source platform that combines the style and usability of high-end consumer devices with the functionality and expandability of sophisticated engineering development platforms, making it the ideal form factor for IoT edge node and wearable markets. It is developed by MikroElektronika in partnership with NXP.
At the core of Hexiwear are the low power, high-performance Kinetis K6x microcontroller, the Kinetis KW4x multimode radio System on Chip (SoC) supporting BLE, six sensors, external flash memory, a color OLED display and a rechargeable battery. Hardware expansion is easy with more than 200 click boardsTM, including a wide variety of sensors, connectivity and HMI options.
The Kinetis K6x MCU can be programmed in a traditional way using FreeRTOS, the Kinetis software development kit (SDK) and the Kinetis Design Studio IDE or through the innovative ARM mbed™ platform. Android and iOS support is straight forward with open source, customizable applications. Hexiwear also enables sensor readings, alarms, reports and other data to be easily sent to the cloud. For more information visit nxp.com/hexiwear
For more information about the ECN Awards visit http://ecnawards.com/.
For more information about the ARM TechCon Innovation Challenge visit http://www.armtechcon.com/2016-innovation-challenge-winners-demonstrate-exceptional-arm-creativity/
For more information about MikroElektronika, visit: http://www.mikroe.com
About
About MikroElektronika
MikroElektronika is a renowned producer of a wide range of hardware and software development tools for various microcontroller architectures, including compilers for three languages: mikroC, mikroBasic and mikroPascal. The company is also known as the originator of mikroBUS™ — a well established standard for add-on boards compatible with their offering of hundreds of sensor and transceiver add-on boards called click boards™. MikroElektronika's goal is to provide software and hardware tools that are easy to use, save time and help get the job done quickly. This approach attracts both hobbyist and professionals. Learn more at: www.mikroe.com
About the ECN IMPACT Awards
NXP, the NXP logo and Kinetis are trademarks of
For more information, please contact:Americas Tate TranTel : +1 408-802-0602Email: tate.tran@nxp.comEurope Martijn van der Linden Tel: +31 6 10914896Email: martijn.van.der.linden@nxp.comGreater China /AsiaEsther Chang Tel: +886 2 8170 9990Email: esther.chang@nxp.com