Long-Range Bi-Directional Communication Opens Up Convenient Remote Control Access and Management Features for Future Car KeysEINDHOVEN, Netherlands, Sept. 15, 2015 (GLOBE NEWSWIRE) -- At the IAA international motor show today in Frankfurt, Germany, NXP Semiconductors N.V. (NASDAQ:NXPI), market leader for secure connected vehicles and car access solutions, announced the new Mantra RF portfolio – a family of high-performance transceivers and receivers for secure car access and vehicle management. The chip family offers a long-range, two-way RF link that enables robust bi-directional communication between key fob and car over a distance of several hundred meters. Car keys with Mantra enable users to conveniently check the fuel, battery levels, and latest maintenance data from a distance. Car owners can also verify if the doors and windows are locked, remotely operate the locks, start the car and pre-set the car's temperature.
Jens Hinrichsen, senior vice president secure car access and networking, NXP Semiconductors, commented, "The car key is an important differentiator for every car brand. NXP aims to continuously raise the bar in car access functionality, performance and security. The new Mantra RF solution is the new industry benchmark for secure bi-directional long-range communication."
Designed for the mid-to-high-end car access market, the Mantra family offers very high sensitivity and blocking performance for improved robustness against radio jamming and undisturbed signal reception. Furthermore it incorporates new innovative concepts: the Mantra family is currently the only chip family on the automotive market that offers a triple-receiver for simultaneous reception of up to three channels. This multi-channel reception ensures that no signals are missed, offering very high system robustness at very low power consumption. Furthermore, this new concept enables the integration of different receiver units, such as tire-pressure monitoring, car diagnostics and car management, into the car-access module to reduce the overall system costs. The Mantra family provides strong security and authentication features to prevent unauthorized access.
Key Features
- Multi-channel transceiver and receiver solutions
- Single IC for bands (315, 345, 426, 434, 447, 868, 915, 950 MHz)
- Simultaneous reception of up to three channels in parallel
- Two RF inputs allowing sequential antenna diversity
- Low receiver power consumption
- Flexible customization at ultra-low power with the programmable µC core
- High-performance, low-noise front end
The Mantra family is available. For more information about the Mantra chip family visit us at IAA in Frankfurt, September 17-27, New Mobility World, Hall 3.1, booth# A31.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) creates solutions that enable Secure Connections for a Smarter World. Building on its expertise in High Performance Mixed Signal electronics, NXP is driving innovation in the application areas Connected Car, Security, Portable & Wearable and Internet of Things. NXP has operations in more than 25 countries, and posted revenue of $5.65 billion in 2014. Find out more at nxp.com.
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by the United States federal securities laws, NXP does not have any intention or obligation to publicly update or revise any forward-looking statements after NXP distributes this document, whether to reflect any future events or circumstances or otherwise. For a discussion of potential risks and uncertainties, please refer to the risk factors listed in NXP's SEC filings. Copies of NXP's SEC filings are available from the SEC website, www.sec.gov.
CONTACT: For further press information, please contact: Europe: Birgit Ahlborn +49 170 57 46 124 birgit.ahlborn@nxp.com Greater China / Asia: Esther Chang +886 2 8170 9990 esther.chang@nxp.com Americas: Hillary Cain +1 408 518 5227 hillary.cain@nxp.com
NXP Semiconductors