Layerscape® Platform Demonstration Showcases xDSL CPE use case in Broadband World ForumBERLIN, Oct. 24, 2017 (GLOBE NEWSWIRE) -- (BROADBAND WORLD FORUM 2017) -- NXP Semiconductors N.V. (NASDAQ:NXPI) and Metanoia Communications, today announced that Metanoia’s proven ADSL2/2+, VDSL2 and G.fast (referred to collectively as “xDSL”) technology will be demonstrated with NXP’s innovative Layerscape portfolio. The technology collaboration will deliver next generation broadband access solutions for home and carrier gateways, xDSL Central Office systems and standalone xDSL termination such as SFP modules.
Major consumer trends driving the need for this technology are the continued growth of internet traffic driven by video, virtual reality (VR), cloud, and more; going wireless - content increasingly delivered wirelessly to smart devices around the home; and IP/OTT delivery of content on-demand taking over from linear broadcasting.
Recently Metanoia’s MT-G5321 based G.fast CPE and DPU technology was certified by the Broadband Forum and the University of New Hampshire Interoperability Laboratory.
“Showcasing Metanoia’s industry-leading xDSL expertise with NXP’s Arm® 64-bit Layerscape roadmap will enable us to deliver highly integrated broadband access solutions in the future which can be upgraded in the field as standards and requirements evolve,” commented Noy Kucuk, vice president, digital networking at NXP. “Working with Metanoia enables us to expand the addressable market for our broadband home router solutions which already enjoy a strong position in fiber gateways.”
“We are pleased to work with NXP to expand our market offering and leverage their broad multicore portfolio and domain knowledge to provide the next generation of xDSL solutions to the market,” commented Didier Boivin, vice president at Metanoia. “Our combined product offering will allow customers to address all xDSL market segments, going from a single PHY to very high-end home gateway, with the same xDSL technology”.
NXP and Metanoia will demonstrate the programmable platform to invited customers during the Broadband World Forum event in Berlin, 24-26 October. Please contact pr@nxp.com or visit NXP at Pod 1 in the Pod Zone - FA13C to schedule a private demonstration.
About Metanoia Communications, Inc.
Metanoia Communications, a subsidiary of Elan Microelectronics, was established in Hsinchu Science Park, Taiwan. Since its inception, Metanoia has been contributing to the development of several generations of semiconductor and software solutions for the wireline Broadband and the in-home networking markets, delivering to broadband manufacturers very high-speed PHY devices with reliable and superior performances.
For more information about Metanoia, please visit our website at www.metanoia-comm.com.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) enables secure connections and infrastructure for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the secure connected vehicle, end-to-end security and privacy and smart connected solutions markets. Built on more than 60 years of combined experience and expertise, the company has 31,000 employees in more than 33 countries and posted revenue of $9.5 billion in 2016. Find out more at www.nxp.com.
The NXP logo and Layerscape are trademarks of NXP B.V. ARM is a trademark or registered trademark of ARM Ltd or its subsidiaries in the EU and/or elsewhere.All other product or service names are the property of their respective owners. All rights reserved. © 2017 NXP B.V.
For more information, please contact:
NXP Americas
Jacey Zuniga
Phone: +1 512-895-7398
Email:
jacey.zuniga@nxp.com

NXP USA, Inc.