Offering an improved operating range and security support from NXP’s latest platform, MIFARE DESFire EV1, up to Common Criteria level EAL5+ MIFARE DESFire EV2 is an ideal platform to enable the smart infrastructures of tomorrow. With DESFire EV2 multiple applications, such as public transport ticketing, bike rental, access management, closed-loop payments, membership, loyalty programs and much more, can now be integrated on a single smart card.
The new MIFARE DESFire EV2 platform is fully backwards compatible with existing MIFARE DESFire installations, offering a fast replacement and migration for established providers wanting to upgrade their systems. The new platform will be demonstrated at the
One of the differentiating features of NXP‘s new MIFARE DESFire EV2 is the ability to seamlessly incorporate and add different applications onto the smart cards once they have been issued and are being used by consumers. In the past, adding new applications to a smart card already in circulation was cumbersome – updates typically required access to the master security key and so cards had to be recalled from the field. Different operating environments also limited the types of applications that could be loaded onto the card resulting in additional complexity when creating apps. Now, with the innovative MIsmartApp and an enhanced key management system developed for MIFARE DESFire EV2, independent system integrators can create a single application for different environments or card systems without the card provider sharing the master security key
“The second evolution of our industry-leading MIFARE DESFire open architecture platform for smart cards offers exceptional performance, state-of-the-art security and privacy as well as enhanced multi- application support to make new business models possible,” said Ulrich Huewels, general manager and senior vice president, secure identification solutions,
“NXP’s MIFARE DESFire EV2 allows cities to easily integrate additional services like our bike-sharing service to existing city cards,” said
“We have been using MIFARE DESFire and MIFARE DESFire EV1 for more than 10 years and appreciate the continuous evolution of this NXP product family,” said
The new MIFARE DESFire EV2 development platform also includes the Transaction MAC (TMAC), a verification feature for card transactions. Ideal for contactless systems with multiple operators and /or merchants, the TMAC ensures that all payment claims to the merchant clearing houses are valid and can be processed. The TMAC allows the backend systems to detect forged transactions, a repeat of a valid transaction and unreported transactions.
For more information on MIFARE DESFire EV2 please visit the following websites:
About MIFARE
MIFARE is NXP´s well-known brand for a wide range of contactless IC products used in more than 40 different applications worldwide. With more than 260 million reader core components and more than 10 billion contactless and dual interface ICs sold, MIFARE products are one of the most proven and reliable interface technologies in the market. MIFARE products comply with the international standard ISO/IEC 14443 and are backward-compatible within the product families. This ensures that the existing infrastructure can be smoothly upgraded to higher security and feature levels, such as payment systems, ticketing solutions, loyalty programs, access management, and parking. To further extend the reach of MIFARE products, the
About
For more information, please contact:NXP Global Technology PRTate TranTel : +1 408-802-0602Email: tate.tran@nxp.comNXP Global Technology PRJack Taylor Tel: +1 512-560-7143Email: j.taylor@nxp.com
Tags: Industrial