EINDHOVEN,
Convenience for customers at the self-service check-out kiosk is also brought to the next level by the SLIX 2. The RFID chip is now capable of scanning more tags in one go – situations that required two checkout cycles in the past, work now with only one cycle. The SLIX 2 is fully compatible with existing ICODE library systems, ensuring that over 5000 public and university libraries already using ICODE SLIX and ICODE SLI based labels can migrate and benefit from the latest technology without difficulties.
In addition to improved scanning and reading capabilities the new SLIX 2 introduces near field communication (NFC) technology to enhance library services. The new chips offer additional memory space to store dedicated URLs without compromising the library management memory areas. The URLs will point to internet spaces that contain additional information related to the book or media. Sophisticated content, such as movie trailers, author bios, book reviews, and much more, becomes automatically accessible through NFC-enabled mobile devices as they tap marked areas on the books. As well as its intended use in libraries the SLIX 2 can also be used for ski ticketing, medical records management, document tracking and authorized service monitoring.
"As a long-standing development partner, Bibliotheca, is delighted to have been working with NXP on the specification for this new silicon which will provide technical advances to libraries globally. The improved memory and enhanced performance means that libraries can extract even more value from their initial label investments - a philosophy we embrace in all our products," said
"Partnering with companies like NXP help us continue to bring the latest advancements to libraries to help them better serve their communities," said
"More and more libraries worldwide are utilizing RFID to automate the issuance and return of media, and gain reliable, real-time visibility for their inventory. Having the new ICODE SLIX 2 in place, this high-performing chip will certainly broaden our HF tag portfolio in an ideal way," said
"The first tests with ICODE SLIX 2 and our new handheld inventory reader for library ID ISC.PRH200 showed promising results. We see about 50 per cent performance improvements in the inventory situations of typical library media," said
"With SLIX 2, the newest member in our ICODE SLI family, we continue the successful path of performance improvements in each generation. SLIX 2 smart labels propel libraries and archives into exciting, dynamic and new environments. Not only will the faster and larger read ranges increase operational efficiencies, the ability of the labels to interact with NFC-enabled devices ensures that customers also greatly benefit by having more valuable information at their fingertips," said
Key features of the ICODE SLIX 2 include:
The product is released and available for ordering.
About
Forward-looking Statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT: For further press information, please contact:NXP Semiconductors Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com