NUREMBERG, Germany,
| |||||
“Companies are now beginning to understand the importance of securing IoT devices and connections for future cloud applications and services, but they lack either the knowledge or the right security solution to integrate,” said Philippe Dubois, senior director and general manager IoT security at NXP. “The A71CH comes with all the technical collateral to accommodate a mass market need for security. It is designed to provide a Root of Trust with the needs and demands to grow and evolve the IoT market.”
Security-by-Design for the IoT
Unique to the chip, is its ‘Plug and Trust” approach supporting easy integration of security and cloud onboarding, e.g., through host libraries and a development kit compatible to different NXP microcontrollers (MCU and MPU) platforms such as Kinetis and i.MX. Also, example codes and various application notes are available to streamline the design process.
Thanks to the collaboration with Data I/O, a world's leading provider of security provisioning and device programming systems, customers further benefit from an easy personalization service on the A71CH for any quantities in addition to NXP’s trust provisioning service. Consequently, the new security IC gives developers, even with limited security expertise, freedom to innovate and deploy secure solutions.
The A71CH provides the following set of key features:
The new A71CH supports NXP’s vision to drive intelligent and secure implementations of edge computing applications. The device builds on the company’s market-proven identification portfolio, which has already seen much success in the authentication, payment, transit and access market.
NXP at Embedded World and IoT Edge Corridor Experience
The A71CH is designed for use in the smart home and industrial applications including sensor networks, gateways, IP cameras, smart cities and home appliances. NXP will showcase its latest solutions including the A71CH for mutual authentication and cloud onboarding, connected cars, and industrial systems at Embedded World 2018 at the NXP booth, #4A-220.
A highlight of the show will be the NXP IoT Edge Compute Experience, located at the entrance of hall 4A. To RSVP your personalized visit to the IoT Edge Compute Experience or schedule a meeting during Embedded World 2018, please contact pr@nxp.com.
To hear the latest news for NXP at the show visit the NXP Embedded World 2018 press room.
About NXP Semiconductors
NXP and the NXP logo are trademarks of
For more information, please contact:
| Americas | Europe | Greater China / Asia |
| Tate Tran | Martijn van der Linden | Esther Chang |
| Tel: +1 408-802-0602 | Tel: +31 6 10914896 | Tel: +886 2 8170 9990 |
| Email: tate.tran@nxp.com | Email: martijn.van.der.linden@nxp.com | Email: esther.chang@nxp.com |
A photo accompanying this announcement is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/e5d1a45b-8d15-4c5c-b6fa-88e66c9ed8c0