EINDHOVEN,
The SSDP is a set of hardware tools and software blocks that enable application developers to quickly start building apps that leverage the eSE in the PN66T. With the platform developers are able to test and validate their secure applications on a commercial phone. As well as providing real-world phone solutions, the development platform also contains example industry use-cases from companies such as Hyatt, 7Eleven and TransportKiosk. The SSDP can be used to create many different applications ranging from secure banking, transit, access control, authentication, automotive, and much more.
"The SSDP supports partners wanting to create new secure applications by removing the technical challenges they face in getting credentials on to the secure element in phones and wearable devices. Now, instead of taking months, new applications can be created and validated in a matter of weeks," said
Customer Quotes:
"NXP's SSDP makes the rock-solid trust of secure elements much easier for Sequent's Trusted Services products to manage and leverage in security-sensitive applications like payments, transit, access control, and identity. The SSDP complements Sequent's Open Wallet Platform, Digital Issuance, and Trust Authority products in dramatically reducing the complexity, time-to-market, and cost of enabling trusted services on connected, mobile devices," said
As a leading operator of Secure Mobile Wallet Platforms,
"MeaWallet is a leader in cloud based mobile solutions and has quickly developed a deep competence and understanding of the Secure Element through our work with the SSDP. Being able to validate our solutions on the development platform means that we can support our customers and partners in the enabling of next generation solutions for access, transit and ticketing, further expanding the use of smartphones instead of plastic cards," said
"We are integrating our SP TSM with NXP's SSDP loader service to enable all service providers - like banks and mass transit companies operating on the Cardtek SP TSM platform - to easily deploy NFC-based services on devices with NXP's new chip set. This new platform will not only simplify the technology adaptation for vendors like us but also will increase the interoperability and compatibility with smart devices like smart phones, tablets and wearable gadgets," said Ali Salcı, EVP of
About
Forward-looking Statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT: For further press information, please contact:NXP Semiconductors Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com