NTAG I²C and PN7462 designed for simple to sophisticated applications
NUREMBURG,
This Smart News Release features multimedia. View the full release here:http://www.businesswire.com/news/home/20160222006201/en/
NXP's PN7462 family is ideal for applications like corporate access, hospitality or home banking (Photo: Business Wire)
The company released its NTAG I²C plus, which extends the family of connected tag solutions that combines passive NFC with I²C interfaces well known for enabling NFC commissioning, simple “tap-to-connect” communications between smart devices to the home network. The new tags deliver four times higher data transfer performance, while adding new, advanced features for password protection, full memory-access configuration from both interfaces, and an ECC based originality signature for protection against cloning.
At Embedded World 2016, NXP also introduces the PN7462, a highly integrated family of single-chip solutions that combine low power ARM® Cortex®-M0 microcontroller core, USB, a contact and contactless interface with full NFC support and capabilities. The PN7462 family is specifically designed for applications like corporate access, hospitality or home banking as it integrates a myriad of technologies, supports the complete MIFARE product portfolio and comes with an
NTAG I²C plus and the PN7462 family combined with the recently launched PN5180 frontend, are an important part of NXP’s strategy to enable the industry to develop and deliver compelling NFC use cases for smarter and more secure connections.
As the inventor of MIFARE and co-creator of NFC, NXP is committed to driving new experiences throughout daily life with NFC technology from delivering the ease to connect to home appliances, personal devices and public systems. “NXP is fuelled by our customer’s excitement to explore the rich set of NFC use cases that can securely and conveniently connect devices,” said
“We are happy to team up with NXP, the market leader in contactless identification technologies, to address the fast growing leisure market and to jointly explore new market opportunities globally,” said
Demonstration
NXP’s NFC solutions will be demonstrated at Embedded World 2016 at the NXP booth# 4A-220.
NXP will also demonstrate the NFC-enabled NHS31XX solutions that marked NXP’s first move into the smart pharma sector for cold chain monitoring and therapy adherence.
Availability
NTAG I²C plus is released and fully available through all major NXP distributors. The PN7462 family is expected to be available for mass production at
Supporting Links
www.nxp.com/products/:NT3H2111_2211
About
NXP and the NXP logo are trademarks of
View source version on businesswire.com: http://www.businesswire.com/news/home/20160222006201/en/
Source:
NXP Global Technology PR
Tate Tran, +1-408-802-0602
tate.tran@nxp.com
or
NXP Global Technology PR
Jack Taylor, +1-512-560-7143
j.taylor@nxp.com
Tags: Industrial