The Jedsy X medical delivery drone expands medical access using UWB for precise location detection.
NXP Semiconductors today announced that its Trimension Ultra-Wideband (UWB) technology enables Jedsy X medical delivery drones . Jedsy is the first company in the world to dock directly at windows or balconies with delivery drones, allowing for quicker and easier dispatch of medical goods. Designed to rapidly bring essential medical supplies and life-saving medicines to urban or remote areas, Jedsy drones leverage NXP’s Trimension SR150 to detect the drone’s precise location, enabling more challenging maneuvers, such as landing at building windows.
Healthcare is often at the forefront of new technology, leveraging groundbreaking features in new ways to save lives. UWB technology enables many of these innovations, from precision drone landings on the side of a building, to fall detection in elder care settings.
“The precision, security and accuracy of UWB-based location or motion tracking offers a number of benefits in medical applications. Jedsy’s UWB-enabled drone makes it easier to deliver medical supplies directly where they are needed. In other settings, UWB could be used to monitor the patient’s vitals in real-time, without the need for intrusive cameras or equipment, or determine the location of an important piece of hospital equipment.”
Jerome Legros, Vice President, Secure Embedded Transactions, NXP
“Jedsy is dedicated to ensuring that life-saving treatments and essential medical supplies are able to reach those who need them. UWB technology has given the Jedsy X drone the precision required to be able to land where it’s needed – whether that’s in a rural field or on the side of a building in an urban city center.”
Christian Bredemeier, CEO, Jedsy
The Trimension SR150 is part of one of the industry’s broadest UWB portfolios, spanning automotive, mobile and IoT applications. The Trimension portfolio leverages short-range UWB radar, secure UWB ranging, angle-of-arrival data and more to enable precise location detection, as well as motion detection. This makes UWB suitable for a variety of healthcare applications, ranging from occupancy detection and patient monitoring to asset mapping, access control and more.
For more information about NXP’s reference designs for drones, please visit NXP.com/drone.
For more information about NXP’s Trimension UWB portfolio, please visit NXP.com/Trimension.
NXP Semiconductors N.V. (NASDAQ: NXPI) is the trusted partner for innovative solutions in the automotive, industrial & IoT, mobile, and communications infrastructure markets. NXP's "Brighter Together" approach combines leading-edge technology with pioneering people to develop system solutions that make the connected world better, safer, and more secure. The company has operations in more than 30 countries and posted revenue of $12.61 billion in 2024. Find out more at www.nxp.com.
NXP, Trimension and the NXP logo are trademarks of NXP B.V. All other product or service names are the property of their respective owners. All rights reserved. © 2025 NXP B.V
View this News Brief in German
Tags: Industrial