EINDHOVEN,
New Plug-and-Play Evaluation Tools Quickens Time to Market
Designed from the ground up to enable engineers with simple plug-and-play testing for RF energy applications, the NXP evaluation tools feature control and measurement functions efficiently viewable from one screen. It also saves development time by eliminating the need for low-level programming and enabling all possible algorithms be set and tested at once. To further shorten time to market, the evaluation kit allows developers to use LabVIEW codes as example codes for final programming. This added functionality allows design teams to test without interrupting lab design workflows.
Power Amplifier in ACP-3 package, BLC2425M9XS250
Delivering breakthrough thermal performance management with 30 percent improvement compared to existing products, NXP's new amplifier enables product designers to improve, simplify and reduce cost for RF designs by saving board space.
S-Band Radar Applications - Gen9 LDMOS RF power transistors, BLS9G2934LS400
NXP announced that its ninth generation (Gen9) LDMOS RF power transistors can achieve required power and efficiency levels in S-band radar applications. S-band radar applications is a fast growing sub-segment in RF power applications. S-band radar applications include weather radar, surface ship radar and some communications satellites.
About
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP's business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
CONTACT: For further press information, please contact:Europe :Martijn van der Linden +31 6 10914896 martijn.van.der.linden@nxp.comGreater China /Asia :Esther Chang +886 2 8170 9990 esther.chang@nxp.comAmericas :Hillary Cain +1 408 518 5227 hillary.cain@nxp.com