LAS VEGAS,
| |||
A photo accompanying this release is available at http://www.globenewswire.com/NewsRoom/AttachmentNg/366758c3-6ef0-400a-a8bd-d87af3b5e62a.
The NXP chip enables a new generation of radar sensor assemblies, roughly the size of a postage stamp, that can be integrated “invisibly” practically anywhere in the car – a great advantage for vehicle designers as the number of sensors steadily increases on the road towards automated driving. Its power consumption is 40 percent lower than conventional radar ICs. Key safety applications include emergency braking, adaptive cruise control, blind-spot monitoring, cross-traffic alert and automated-parking.
“Building the world’s smallest, fully integrated 77GHz chip will pave the way for self-driving cars and drive increased ADAS adoption in the volume market,” said Torsten Lehmann, senior vice president infotainment and driver assistance at NXP. “In self-driving cars, a ‘cocoon’ of radar sensors is required to provide a robust high-resolution, 360 degree view of the environment. This is a real challenge using traditional, bulky radar hardware. Manufacturers are also eager to replace existing ultra-sonic based park distance control systems with “invisible” radar sensors and avoid unattractive holes in the bumper while improving performance and features.”
Radar-based ADAS will have a steep penetration over the next years with
With the completion of its merger with Freescale Semiconductor on
Source: IHS, Advanced Driver Assistance Applications Semiconductor Market Tracker – H1 2015
Availability
Working prototypes are available to key customers.
Link
Complementing radar data with automotive vision systems, NXP's S32V vision microprocessor.
About NXP Semiconductors
Forward-looking Statements
This document includes forward-looking statements which include statements regarding NXP’s business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by the United States federal securities laws, NXP does not have any intention or obligation to publicly update or revise any forward-looking statements after NXP distributes this document, whether to reflect any future events or circumstances or otherwise. For a discussion of potential risks and uncertainties, please refer to the risk factors listed in NXP’s SEC filings. Copies of NXP’s SEC filings are available from the SEC website, www.sec.gov.
For more information, please contact:NXP Global Technology PRTate TranTel: +1 408-802-0602Email: tate.tran@nxp.comNXP Global Technology PRJack TaylorTel: +1 512-560-7143Email: j.taylor@nxp.comNXP Global Automotive PRBirgit AhlbornTel: +49 170 5746124Email: birgit.ahlborn@nxp.com
Tags: Automotive