EINDHOVEN, The Netherlands, May 19, 2020 (GLOBE NEWSWIRE) NXP Semiconductors N.V. (NASDAQ: NXPI) today announced that its most recent radio frequency front-end (RFFE) solution, designed with Wi-Fi 6 standards, is now designed into the Xiaomi Mi 10 5G smartphone.
NXP's radio frequency front-end (RFFE) solution, designed with Wi-Fi 6 standards
Advanced 5G devices make steep demands in terms of performance, integration, size and Wi-Fi 6 capability. NXP’s RFFE solution is highly integrated and tightly packed in a 3 mm x 4 mm package. It is designed with Wi-Fi 6 capability to support advanced portable computing devices, including premier 5G smartphones, and to enable 2x2 MIMO functionality with the highest performance. NXP’s compact high performance RFFE solution can reduce the design time and improve time to market significantly for original equipment manufacturers (OEMs).
“Xiaomi is very pleased to work with NXP in support of developing an RFFE with Wi-Fi 6 support for our flagship 5G smartphones,” said Lei Zhang, Vice President of Mi Smartphone and General Manager of Hardware R&D, Xiaomi. And offer excellent Wi-Fi 6 performance, which reduces design time for getting to market faster.”
NXP’s high performance WLAN11ax portfolio supports customers in fulfilling the ever-increasing need for more bandwidth by providing both the 2.4 GHz and the 5 GHz bands that fit the 802.11ax Wi-Fi 6 standard. NXP offers a flexible portfolio that scales across these specifications. NXP offers 2x2 multiple input multiple output (MIMO) support for IEEE802.11a/n/ac/ax applications.
“Xiaomi’s speedy adoption of this RFFE technology will enable them to meet the rapidly rising global demand for Wi-Fi 6 in 5G handsets,” said Paul Hart, Senior Vice President and General Manager of NXP’s Radio Power. “Designed with the latest Wi-Fi 6 standards, NXP’s highly integrated RFFE solutions have the right combination of performance for mobile applications such as Xiaomi’s.”
The new RF front-end modules are available now. For more information, contact your local NXP sales representative.
To learn more, visit our growing wireless local area network (WLAN) portfolio,
WLAN Front-End ICs and Modules
NXP Semiconductors N.V. enables secure connections for a smarter world, advancing solutions that make lives easier, better and safer. As the world leader in secure connectivity solutions for embedded applications, NXP is driving innovation in the automotive, industrial & IoT, mobile and communication infrastructure markets. Built on more than 60 years of combined experience and expertise, the company has approximately 29,000 employees in more than 30 countries and posted revenue of $8.88 billion in 2019. Find out more at NXP Semiconductors.
NXP, EdgeVerse and the NXP logo are trademarks of NXP B.V. All other products or service names are the property of their respective owners. All rights reserved. © 2020 NXP B.V.