EINDHOVEN,
“Our new agreement with NXP allows us to tap into the huge installed base of MIFARE® and provide a massive amount of card-based applications into mobile devices. It opens up opportunities for transit agencies, hotels and other organizations to effectively leverage mobile devices as the cards and keys of their customers,” said
Sequent’s Token Service Platform (TSP) supports hardware secure element security and other security appliances in connected devices. This enables them to offer more widely the use of MIFARE-based credentials, also on smartphones that do not have a native MIFARE implementation on the secure element. With this flexibility, Sequent can support more card types and emulation standards, making them available in the smartphone apps consumers already know and use and this greatly simplifies and fosters efficiencies in a wide variety of industries.
“NXP’s MIFARE DESFire and MIFARE Classic are widely used for many applications including transit and access control, with over 10 billion cards sold in more than 736 cities worldwide,” said
About
MIFARE, MIFARE4Mobile, MIFARE Classic and MIFARE DESFire are registered trademarks of
About Sequent
Sequent Platform brings cards to mobile and makes them useful for consumers. Sequent enables banks, transit agencies and any other issuer to securely digitize their credit, debit, transit, loyalty or ID cards and distribute them to their own application, and to any other application using the Sequent Platform. Sequent’s simple APIs empower the app developer community to bring cards to all apps on mobile, wearable, and other connected devices enabling consumers to make payments, redeem offers, open doors, and ride transit systems. Sequent Platform includes: Token Service Platform (TSP), Card and Wallet Management Platform, and Trust Authority. For more information, visit www.sequent.com, and follow us on Twitter @sequentsw.
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP’s business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by
For further press information, please contact:NXP Americas:Hillary Cain +1 408 518 5227hillary.cain@nxp.comSequent SystemsMarcelo Delima 1 650 776 7109marcelo.delima@sequent.com