NXP NFC Technology Enables Brand Authentication and TraceabilityEINDHOVEN, Netherlands, Oct. 29, 2015 (GLOBE NEWSWIRE) -- NXP Semiconductors N.V. (NASDAQ:NXPI), the world leader in near field communication (NFC) and radio frequency identification (RFID) technologies, today announced that its NFC smart security solutions will be included in the World Customs Organization’s (WCO) Interface Public Members (IPM) Connected anti-counterfeiting program. IPM is the WCO’s on-line tool to combat counterfeiting by providing customs officers with key operational product information to help them distinguish between genuine and fake products. Over the past year, the WCO has developed IPM Connected, a global network of security solution providers interfaced with IPM that enables customs officials to instantly verify the authenticity of a product. NXP’s full suite of high-performance NFC tag solutions, based on established standards that ensure maximum compatibility with NFC-enabled devices, will gradually interface into the IPM anti-counterfeiting platform providing a secure authentication service for brand owners.
Brand owners or rights holders can apply NFC tags to protect their products at the point of manufacture. These secure NFC tags provide an additional scaled layer of security and can be used to deliver details on the product only known by the brand owner or rights holder. Genuine products can be quickly and reliably verified at any point in the supply chain by an NFC-enabled device, such as a smartphone or a computer with a connected reader. As goods pass international borders customs officials using the WCO’s IPM web or mobile application will be able to dynamically spot-check the authenticity of the product by cross referencing real-time information provided by the brand owners. With many existing anti-counterfeiting technologies, such as bar codes and holograms, already being duplicated by counterfeiters NFC is quickly emerging as the next force in brand authentication and source-to-sale channel traceability.
“Being able to offer our secure and fully standardized NFC solutions to the WCO IPM program is a significant development and ensures that technology remains at the forefront of the fight against global counterfeiting,” said Matthias Poppel, general manager, secure mobility and retail, NXP Semiconductors. “Over 70 percent of all counterfeit seizures in the world are processed by customs officials on the front line. Having a simple, yet highly effective way to instantly verify the authenticity of a product, using NFC tags and a secure NFC-enabled smartphone for example, will help streamline the international customs process and provide a deterrent for would-be counterfeiters.”
According to the International Chamber of Commerce global financial losses from counterfeiting soared to $1 trillion in 2013 and losses are forecast to jump to $2.3 trillion by 2018. Global counterfeiting is accelerating rapidly at a double-digit rate and already impacts many industries such as fashion; food and beverages; FMCGs; electronics; and, pharmaceuticals.
The World Customs Organization (WCO) is an independent intergovernmental body whose mission is to enhance the effectiveness and efficiency of Customs administrations. The WCO represents 180 Customs administrations across the globe that collectively process approximately 98 percent of world trade. As the global center of Customs expertise, the WCO is the only international organization with competence in Customs matters, rightly calling itself the voice of the international Customs community. More information about the WCO IPM program can be found here.
About NXP Semiconductors
NXP Semiconductors N.V. (NASDAQ:NXPI) creates solutions that enable Secure Connections for a Smarter World. Building on its expertise in High Performance Mixed Signal electronics, NXP is driving innovation in the application areas Connected Car, Security, Portable & Wearable and Internet of Things. NXP has operations in more than 25 countries, and posted revenue of $5.65 billion in 2014. Find out more at nxp.com.
Forward-looking statements
This document includes forward-looking statements which include statements regarding NXP’s business strategy, financial condition, results of operations and market data, as well as other statements that are not historical facts. By their nature, forward-looking statements are subject to numerous factors, risks and uncertainties that could cause actual outcomes and results to be materially different from those projected. Readers are cautioned not to place undue reliance on these forward-looking statements. Except for any ongoing obligation to disclose material information as required by the United States federal securities laws, NXP does not have any intention or obligation to publicly update or revise any forward-looking statements after NXP distributes this document, whether to reflect any future events or circumstances or otherwise. For a discussion of potential risks and uncertainties, please refer to the risk factors listed in NXP’s SEC filings. Copies of NXP’s SEC filings are available from the SEC website, www.sec.gov.
For further press information, please contact:NXP SemiconductorsEurope: Martijn van der Linden+31 6 10914896martijn.van.der.linden@nxp.comGreater China / Asia: Esther Chang+886 2 8170 9990esther.chang@nxp.comAmericas: Hillary Cain+1 408 518 5227hillary.cain@nxp.com

NXP Semiconductors Netherlands B.V.